# Zed X One Calibration Board

**URL:** <https://community.stereolabs.com/t/zed-x-one-calibration-board/8048>\
**Category:** ZED X\
**Created:** [February 5, 2025, 2:59am UTC](https://community.stereolabs.com/t/zed-x-one-calibration-board/8048 "2025-02-05T02:59:23Z")\
**Posts on this page:** 5\
**Page:** 1

<div class="post-metadata">

**Author:** ![auc7us](https://community.stereolabs.com/user_avatar/community.stereolabs.com/auc7us/32/4156_2.png) [@auc7us](https://community.stereolabs.com/u/auc7us)\
**Post date:** [February 5, 2025, 2:59am UTC](https://community.stereolabs.com/t/zed-x-one-calibration-board/8048/1 "2025-02-05T02:59:23Z")

</div>

Hi,

I have two **Zed X Ones (2.2mm)** that I plan on using with a **baseline of 1.25m**

During my first trial calibration, I had them at 45cm baseline and used a A4 calibration pattern with square size 25mm, 9x6 internal edges. The one provided in the calibration readme in zedx-one-capture repository. I tried the calibration 4-6 times and noticed that the best baseline post calibration was reported at 51cm in the .conf file. Which was not really reassuring but I didn’t really mind that coz it was just a test.

Now for the final deployment, i want them to be at 1.25m like mentioned above. I have a calibration board that nearly an A2, with a square size of 105mm and 7x5 internal edges. (This board has no white borders around the outer edges of the chess board, not really sure if that matters). I noticed that the calibration script does not pick up the board at all, I tried this with the calibration board at 2m-5m away from the stereo rig. By this I mean, while the entire board is clearly visible in both the camera’s fov, I don’t see the multi colored lines that appear on the left camera to indicate it’s being detected.

I understand that a bigger board with a lot of squares would make the calibration more accurate. I’m planning on getting a new calibration board and would appreciate it if you could provide the optimal/ ideal parameters for the calibration pattern for my setup (1.25m baseline) (size of squares and number of edges + if I need the white border and how thick)

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [February 5, 2025, 10:56am UTC](https://community.stereolabs.com/t/zed-x-one-calibration-board/8048/2 "2025-02-05T10:56:16Z")

</div>

Hi @auc7us

> [@auc7us](#):
>
> I noticed that the calibration script does not pick up the board at all, I tried this with the calibration board at 2m-5m away from the stereo rig. By this I mean, while the entire board is clearly visible in both the camera’s fov, I don’t see the multi colored lines that appear on the left camera to indicate it’s being detected.

Can you send me a picture of this calibration board?

> [@auc7us](#):
>
> I understand that a bigger board with a lot of squares would make the calibration more accurate. I’m planning on getting a new calibration board and would appreciate it if you could provide the optimal/ ideal parameters for the calibration pattern for my setup (1.25m baseline) (size of squares and number of edges + if I need the white border and how thick)

An A2 board is good; you could use smaller squares to add more corners.

---

<div class="post-metadata">

**Author:** ![auc7us](https://community.stereolabs.com/user_avatar/community.stereolabs.com/auc7us/32/4156_2.png) [@auc7us](https://community.stereolabs.com/u/auc7us)\
**Post date:** [February 5, 2025, 4:18pm UTC](https://community.stereolabs.com/t/zed-x-one-calibration-board/8048/3 "2025-02-05T16:18:17Z")

</div>

![IMG_3727](https://community.stereolabs.com/uploads/default/original/2X/c/cc4495874265114c6d10a685c54213ada97ffe03.jpeg)

This is the board I used. This was picked up in couple of frames when then baseline was 45cm indoors but it struggled. With the baseline set to 125cm it wasn’t picked up for a single frame. We did this calibration outdoors with the board held in front of a wall by a person, I’m assuming overcast lighting would have no affect on calibration.

Could you also specify number of squares or the size and what’s a good distance to calibrate it from. I’m on a time crunch and can’t afford to print multiple boards to test what setup would me reliable results.

---

<div class="post-metadata">

**Author:** ![auc7us](https://community.stereolabs.com/user_avatar/community.stereolabs.com/auc7us/32/4156_2.png) [@auc7us](https://community.stereolabs.com/u/auc7us)\
**Post date:** [February 10, 2025, 7:15pm UTC](https://community.stereolabs.com/t/zed-x-one-calibration-board/8048/4 "2025-02-10T19:15:37Z")

</div>

Hey, I’d have to return the cameras if we can’t get the expected/ advertised range accurately. The return window is getting close. I’d really appreciate it if you could share the parameters I should use for calibrating the zed X ones wide with 1.2m baseline

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [February 11, 2025, 11:25am UTC](https://community.stereolabs.com/t/zed-x-one-calibration-board/8048/5 "2025-02-11T11:25:37Z")

</div>

> [@auc7us](#):
>
> ![IMG_3727](https://community.stereolabs.com/uploads/default/original/2X/c/cc4495874265114c6d10a685c54213ada97ffe03.jpeg)
> 
> This is the board I used. This was picked up in couple of frames when then baseline was 45cm indoors but it struggled. With the baseline set to 125cm it wasn’t picked up for a single frame. We did this calibration outdoors with the board held in front of a wall by a person, I’m assuming overcast lighting would have no affect on calibration.

You need with boarded for a better detection of the checker board.

> [@auc7us](#):
>
> Could you also specify number of squares or the size and what’s a good distance to calibrate it from. I’m on a time crunch and can’t afford to print multiple boards to test what setup would me reliable results.

This is a 7x5 board. I recommend you double the squares on both width and height.  
Concerning the distance, you must not use a fixed distance, you must move the board forward and backward being sure that it’s always detected in the field of view of both cameras