# ZED X not recognized by SDK - GMSLList empty, /dev/video7 hangs, ZED\_Explorer "Cannot find a valid camera"

**URL:** <https://community.stereolabs.com/t/zed-x-not-recognized-by-sdk-gmsllist-empty-dev-video7-hangs-zed-explorer-cannot-find-a-valid-camera/11091>\
**Category:** ZED X\
**Tags:** sdk, jetson, depth\
**Created:** [March 26, 2026, 8:14am UTC](https://community.stereolabs.com/t/zed-x-not-recognized-by-sdk-gmsllist-empty-dev-video7-hangs-zed-explorer-cannot-find-a-valid-camera/11091 "2026-03-26T08:14:30Z")\
**Posts on this page:** 5\
**Page:** 1

<div class="post-metadata">

**Author:** ![Ryan-Simpson](https://community.stereolabs.com/user_avatar/community.stereolabs.com/ryan-simpson/32/6007_2.png) [@Ryan-Simpson](https://community.stereolabs.com/u/Ryan-Simpson)\
**Post date:** [March 26, 2026, 8:14am UTC](https://community.stereolabs.com/t/zed-x-not-recognized-by-sdk-gmsllist-empty-dev-video7-hangs-zed-explorer-cannot-find-a-valid-camera/11091/1 "2026-03-26T08:14:30Z")

</div>

**Okay so  
My Platform / Environment**

- Jetson AGX Orin, JetPack 6.1 (L4T 36.4.7), kernel 5.15.148-tegra

- ZED SDK 5.2.0

- ZED Link Quad driver: [stereolabs](https://www.stereolabs.com/)-zedlink-quad 1.4.0-SL-MAX96712-L4T36.4.0

- DTB: kernel\_tegra234-p3737-0000+p3701-0005-nv.dtb with overlay tegra234-p3737-camera-zedlink-quad-sl-overlay.dtbo

- Dual ZED X camera setup left camera (S/N: 43779087) works normally; right camera (S/N: 47753729) is the affected unit

**Problem Description**

One of our two ZED X cameras (S/N: 47753729) is no longer recognized by the ZED SDK. ZED\_Explorer reports “Cannot find a valid camera.” The camera does enumerate at the driver level two /dev/video\* nodes appear but the SDK sees nothing.

**Observed Behavior**

Using v4l2-ctl:

- /dev/video6 streams successfully

- /dev/video7 hangs indefinitely, no frames returned

Both nodes report similar capabilities and EEPROM data via v4l2-ctl --all.

From the ZED Diagnostic Tool output:

- GMSLList is empty

- ZEDDetected, ZEDCount, ZEDs, Serial Number, and InternalDevicesCount (GMSL) are all empty

- Camera Test \> valid shows “Camera: ZED-X” (type identified, but no camera actually found)

- CUDA Operations, ZED SDK, AI Models, and GMSL Driver all pass

**Driver State**

All relevant kernel modules are loaded:

sl\_zedx 28672 2 sl\_max9295 16384 3 sl\_zedxhdr,sl\_zedxone\_uhd,sl\_zedx sl\_max96712 32768 4 sl\_zedxhdr,sl\_zedxone\_uhd,sl\_max9295,sl\_zedx tegra\_camera 217088 15 …sl\_zedx videodev 249856 10 …sl\_zedx

zed\_x\_daemon.service is active and running. GMSL driver package shows ii (fully installed) in dpkg.

Driver file status from diagnostic:

- sl\_max96712.ko → exists

- sl\_zedx.ko → exists

- max96712.ko → not found (non-SL variant, expected)

- sl\_max9296.ko → not found (expected, Quad uses MAX96712 not MAX9296)

**I2C Traces**

The mux channels show activity on i2c-8 (addresses 0x12, 0x29, 0x70) consistent with the ZED Link Quad and one camera. No addresses corresponding to the second camera’s serializer appear on any mux sub-channel, which suggests the affected camera’s MAX9295 serializer is not being seen on the I2C bus.

**Troubleshooting Already Performed**

- Replaced GMSL2 cable

- Full power cycle (unplugged from wall, not just reboot)

- Reseated camera connector

- Verified all kernel modules load correctly

- Verified zed\_x\_daemon is active and running

- Confirmed the other ZED X (S/N: 43779087) works normally on the same ZED Link Quad and software stack

**Question**

Given that:

1. The GMSL driver, SDK, and daemon are all healthy

2. The working camera (S/N: 43779087) shares the same software stack with no issues

3. The affected camera (S/N: 47753729) enumerates /dev/video\* nodes but /dev/video7 hangs and the SDK sees an empty GMSLList

4. I2C traces do not show the second camera’s serializer being addressed on any mux channel

Is the camera’s onboard GMSL serializer (MAX9295) likely damaged? Is this consistent with a hardware failure that would fall under warranty, or is there a further diagnostic step we should try before concluding it is a hardware fault?

Happy to run additional commands or capture more logs if helpful. Thank you.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [March 27, 2026, 12:02pm UTC](https://community.stereolabs.com/t/zed-x-not-recognized-by-sdk-gmsllist-empty-dev-video7-hangs-zed-explorer-cannot-find-a-valid-camera/11091/2 "2026-03-27T12:02:18Z")

</div>

Hi @Ryan-Simpson  
Welcome to the [Stereolabs](https://www.stereolabs.com/) community.

Please run `sudo ZED_Diagnostic --dmesg` and share the content of the `dmesg.log` file that it generates.

---

<div class="post-metadata">

**Author:** ![Ryan-Simpson](https://community.stereolabs.com/user_avatar/community.stereolabs.com/ryan-simpson/32/6007_2.png) [@Ryan-Simpson](https://community.stereolabs.com/u/Ryan-Simpson)\
**Post date:** [March 27, 2026, 7:20pm UTC](https://community.stereolabs.com/t/zed-x-not-recognized-by-sdk-gmsllist-empty-dev-video7-hangs-zed-explorer-cannot-find-a-valid-camera/11091/3 "2026-03-27T19:20:45Z")

</div>

Hi @Myzhar

Thanks for the reply.

I ran `sudo ZED_Diagnostic --dmesg`. On SDK 5.2.0 it outputs a JSON file instead of `dmesg.log`. Relevant dmesg lines:

sl\_max96712 9-0029: Camera connected to GMSL port 3  
sl\_max96712 9-0029: zedx camera connected to this port  
sl\_max9295 9-0062: Serializer for zedx detect success

zedx 9-0020: zedx\_probe: Serial Number : 47753729  
zedx 9-0020: zedx\_probe: success  
zedx 9-0028: zedx\_probe: Serial Number : 47753729  
zedx 9-0028: zedx\_probe: success

The camera is present in V4L2:

/dev/video0  
/dev/video1

But the SDK still shows:

GMSLList []

ZEDDetected []

ZED Explorer just stays on “waiting for camera”.

We tested multiple ZED X cameras on the same rig and setup. Other cameras work. This unit (S/N 47753729) is the only one that fails.

Does this match a known camera-side issue or should we try more diagnostics before RMA?

Happy to share the full JSON if needed.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [March 30, 2026, 1:54pm UTC](https://community.stereolabs.com/t/zed-x-not-recognized-by-sdk-gmsllist-empty-dev-video7-hangs-zed-explorer-cannot-find-a-valid-camera/11091/4 "2026-03-30T13:54:13Z")

</div>

> [@Ryan-Simpson](#):
>
> Relevant dmesg lines:

I need the full content of the file. Thank you

---

<div class="post-metadata">

**Author:** ![Bongiiii](https://community.stereolabs.com/user_avatar/community.stereolabs.com/bongiiii/32/6074_2.png) [@Bongiiii](https://community.stereolabs.com/u/Bongiiii)\
**Post date:** [April 15, 2026, 7:29am UTC](https://community.stereolabs.com/t/zed-x-not-recognized-by-sdk-gmsllist-empty-dev-video7-hangs-zed-explorer-cannot-find-a-valid-camera/11091/5 "2026-04-15T07:29:59Z")

</div>

Hey, I am having a similar issue. Here are my [diagnostic](https://drive.google.com/file/d/1X-9dRRt7_seis_Di9gIp7EtrA55FRGY4/view?usp=sharing) results. Please help.

> **[latesttttt.json](https://drive.google.com/file/d/1X-9dRRt7_seis_Di9gIp7EtrA55FRGY4/view?usp=sharing)**
>
> Google Drive file.