# ZED X grab stuck in FAILURE after Argus / ZED-X daemon failure

**URL:** <https://community.stereolabs.com/t/zed-x-grab-stuck-in-failure-after-argus-zed-x-daemon-failure/11590>\
**Category:** ZED X\
**Tags:** sdk, jetson, ros2\
**Created:** [July 28, 2026, 5:49pm UTC](https://community.stereolabs.com/t/zed-x-grab-stuck-in-failure-after-argus-zed-x-daemon-failure/11590 "2026-07-28T17:49:27Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![matialmar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/matialmar/32/4971_2.png) [@matialmar](https://community.stereolabs.com/u/matialmar)\
**Post date:** [July 28, 2026, 5:49pm UTC](https://community.stereolabs.com/t/zed-x-grab-stuck-in-failure-after-argus-zed-x-daemon-failure/11590/1 "2026-07-28T17:49:27Z")

</div>

Hi there!

We are currently developing a perception solution using the ZED X Camera and Orin NX. And currently facing the problems using the `zed-ros2-wrapper` with sporadic reboots and failures.

## The core problem

While a ZED X camera is streaming, if `nvargus-daemon` and/or `zed_x_daemon` are restarted (or otherwise disrupted), `sl::Camera::grab()` enters `CAMERA_REBOOTING`, then reports a critical Argus reboot failure and transitions to `FAILURE`. After that point, grab remains in `FAILURE` indefinitely; the SDK does not recover the session even with `async_grab_camera_recovery = true`.

The only reliable recovery we found is:

1. Kill the application / ROS node that holds the camera session

2. Restart `nvargus-daemon` + `zed_x_daemon`

3. Re-open the camera (`sl::Camera::open`)

This mechanism is used for both hotplug and unhandled reboots by the SDK.

* * *

### Environment

| Item | Value |
| --- | --- |
| Platform | NVIDIA Jetson Orin NX Engineering Reference Developer Kit |
| Host OS / L4T | Linux 5.15.185-tegra, **L4T R36.5.0** |
| ZED Link package | `stereolabs-zedlink-duo` **1.4.2-LI-MAX96712-L4T36.5.0** |
| Camera | **ZED X** , S/N **46817456** |
| Capture mode | HD1200@30, GMSL |
| Depth mode | NEURAL LIGHT |
| ZED SDK | **5.4.0** — Build `115927_a75bfaef_3175036` |
| CUDA (SDK) | 12.6 |
| Runtime | Docker image based on L4T 36.4.0 + ZED SDK 5.4.0 (`zed_ros2_l4t_36.4.0_sdk_5.4.0`) with NVIDIA runtime, privileged, `pid: host` |
| Application | ZED ROS 2 wrapper (Humble), `component_container_isolated` |
| Host daemons | `nvargus-daemon.service`, `zed_x_daemon.service` (`/usr/sbin/ZEDX_Daemon`) |

* * *

### How to reproduce

1. Open the ZED X camera and stream continuously (`grab()` loop / ROS wrapper publishing depth + RGB).

2. Confirm healthy streaming.

3. On the host, restart the GMSL/Argus stack while the session is still open:

```bash

sudo systemctl restart zed_x_daemon.service

sudo systemctl restart nvargus-daemon.service

```

1. Observe `grab()` status codes and ZED/Argus logs.

Also reproducible in our setup by any hard disruption of Argus while the camera is open (not only an intentional `systemctl restart`).

* * *

## 4. Observed behavior (timeline from 2026-07-28 test)

Approximate UTC times from container logs:

| Time (UTC) | Event |
| --- | --- |
| 18:54:50 | Host: `systemctl restart zed_x_daemon` + `nvargus-daemon` |
| 18:54:54 → 18:55:02 | `grab()` returns `CAMERA_REBOOTING` repeatedly |
| same window | Flood of Argus client errors (see below) |
| **18:55:03** | **`[ZED-Argus][Critical] Reboot has failed for CAM0 with current state=4`** |
| 18:55:03 | `grab()` returns `FAILURE` |
| after | `FAILURE` persists on every subsequent `grab()`; no return to `SUCCESS` without process kill + reopen |

#### 4.1 Critical ZED SDK / Argus messages

```plaintext

[ZED][INFO] CAMERA REBOOTING in sl::ERROR_CODE sl::Camera::grab(sl::RuntimeParameters)

(Argus) Error InvalidState: Receive thread is not running cannot send.

(in src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 96)

(Argus) Error InvalidState:

(propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)

[ZED][ERROR] [ZED-Argus][Critical] Reboot has failed for CAM0 with current state=4

[ZED][ERROR] FAILURE in sl::ERROR_CODE sl::Camera::grab(sl::RuntimeParameters)

```

#### 4.2 Host `nvargus-daemon` journal (around re-open after recovery)

After killing the process and restarting daemons, Argus still logged transient open errors before the new session succeeded:

```plaintext

NvPclStateControllerOpen: Failed ImagerGUID 13. (error 0xA000E)

NvPclOpen: PCL Open Failed. Error: 0xf

SCF: Error BadParameter: Sensor could not be opened.

(in src/services/capture/CaptureServiceDeviceSensor.cpp, function getSourceFromGuid(), line 725)

(Argus) Error AlreadyAllocated: Device 0 (of 1) is in use

(in src/api/CameraProviderImpl.cpp, function createCaptureSessionInternal(), line 286)

```

The camera eventually opened again after a full process restart + daemon restart.

* * *

## Questions

1. Is `Reboot has failed for CAM0 with current state=4` a known issue on ZED X + L4T 36.5 / SDK 5.4.0? What does `state=4` mean?

2. After this critical reboot failure, is `grab()` → `FAILURE` forever until `close()` (and possibly daemon restart) expected?

3. What is the recommended production recovery sequence when Argus reports `InvalidState: Receive thread is not running` mid-stream?

4. Should applications avoid restarting `nvargus-daemon` / `zed_x_daemon` while a session is open, or is the SDK supposed to handle reboots, failures and hotplug?

5. Is running SDK 5.4.0 inside an L4T 36.4-based container on a host with L4T 36.5 + ZED Link 36.5.0 a supported configuration?

6. Are there known issues with `AlreadyAllocated: Device 0 is in use` after a failed reboot / unclean session teardown?

7. Is there a known solution for this kind of issues?

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [July 28, 2026, 7:52pm UTC](https://community.stereolabs.com/t/zed-x-grab-stuck-in-failure-after-argus-zed-x-daemon-failure/11590/2 "2026-07-28T19:52:08Z")

</div>

Hi @matialmar  
please upgrade the ZED SDK to v5.4.1 and the ZED X Driver to v1.4.3 because they both introduces improvements to this behavior.

---

<div class="post-metadata">

**Author:** ![matialmar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/matialmar/32/4971_2.png) [@matialmar](https://community.stereolabs.com/u/matialmar)\
**Post date:** [July 30, 2026, 4:52pm UTC](https://community.stereolabs.com/t/zed-x-grab-stuck-in-failure-after-argus-zed-x-daemon-failure/11590/3 "2026-07-30T16:52:10Z")

</div>

Thank you @Myzhar. This version fixes almost all of the problems.

Just to mention, trying to break the docker I stopped the zed\_x\_daemon and restarted it and it caused an invalid state that could not be restored from restarting the zed\_x\_daemon along with nvargus daemon

Not even removing the docker, manually unplugging and plugging the ZED X, restarting the daemons and afterwards restarting the docker would restore the previous working state. Just a full reboot did the job.

Although I know this is not intended usage, it may be helpful to improve ZED X robustness.

A quick log in case it is usefull.

```auto
[component_container_isolated-2] [ERROR] [1785343391.723567985] [zed.zed_node]: Connection issue detected: CAMERA REBOOTING
[component_container_isolated-2] (Argus) Error FileOperationFailed: Failed socket read: Connection reset by peer (in src/rpc/socket/common/SocketUtils.cpp, function readSocket(), line 79)
[component_container_isolated-2] (Argus) Error FileOperationFailed: Unexpected error in reading socket (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 277)
[component_container_isolated-2] (Argus) Error FileOperationFailed: Receive worker failure, notifying 1 waiting threads (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 350)
[component_container_isolated-2] (Argus) Error InvalidState: Argus client is exiting with 1 outstanding client threads (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 366)
[component_container_isolated-2] (Argus) Error FileOperationFailed: Receiving thread terminated with error (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadWrapper(), line 379)
[component_container_isolated-2] (Argus) Error FileOperationFailed: Client thread received an error from socket (in src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 145)
[component_container_isolated-2] (Argus) Error FileOperationFailed: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
[component_container_isolated-2] (Argus) Error InvalidState: Receive thread is not running cannot send. (in src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 96)
[component_container_isolated-2] (Argus) Error InvalidState: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
[component_container_isolated-2] (Argus) Error InvalidState: Receive thread is not running cannot send. (in src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 96)
[component_container_isolated-2] (Argus) Error InvalidState: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)

```

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [August 4, 2026, 2:51pm UTC](https://community.stereolabs.com/t/zed-x-grab-stuck-in-failure-after-argus-zed-x-daemon-failure/11590/4 "2026-08-04T14:51:55Z")

</div>

> [@matialmar](#):
>
> Just to mention, trying to break the docker I stopped the zed\_x\_daemon and restarted it and it caused an invalid state that could not be restored from restarting the zed\_x\_daemon along with nvargus daemon

This is expected because by stopping the zed\_x\_daemon and restarting it, you’ve “unloaded” and “reloaded” the ZED X Driver, causing unexpected behaviors for the software that was using it.

> [@matialmar](#):
>
> Not even removing the docker, manually unplugging and plugging the ZED X, restarting the daemons and afterwards restarting the docker would restore the previous working state. Just a full reboot did the job.

This is not a recommended operation with GMSL2 cameras.  
GMSL2 is not plug-and-play. If you want to unplug and replug the cameras we recommend to turn off the host device and remove the power to the capture card before.