# ZED X drivers for TZTEK YS-X1-32G

**URL:** <https://community.stereolabs.com/t/zed-x-drivers-for-tztek-ys-x1-32g/11338>\
**Category:** ZED X\
**Tags:** jetson\
**Created:** [May 22, 2026, 6:38pm UTC](https://community.stereolabs.com/t/zed-x-drivers-for-tztek-ys-x1-32g/11338 "2026-05-22T18:38:50Z")\
**Posts on this page:** 3\
**Page:** 1

<div class="post-metadata">

**Author:** ![dbarinov](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/d/d26b3c/32.png) [@dbarinov](https://community.stereolabs.com/u/dbarinov)\
**Post date:** [May 22, 2026, 6:38pm UTC](https://community.stereolabs.com/t/zed-x-drivers-for-tztek-ys-x1-32g/11338/1 "2026-05-22T18:38:50Z")

</div>

Hello,

We are planning to use **[Stereolabs](https://www.stereolabs.com/) ZED X MINI and NANO GMSL2 cameras** on a **TZTEK YS-X1-32G / NVIDIA Jetson AGX Orin** platform.

Current system:

> L4T R36.4.3  
> Kernel: 5.15.148-tegra  
> SoC: NVIDIA Jetson AGX Orin / tegra234  
> Board compatible: nvidia,p3737-0000+p3701-0004  
> GMSL topology: 4x MAX9296, up to 8 camera ports

The current BSP uses an IMX185 camera stack:

> tztek\_camera\_driver  
> tztek\_max9296  
> max9296\_class  
> nv\_imx185

Could you please advise:

1. Is there a ready-to-use driver/BSP for **ZED X + TZTEK YS-X1-32G + L4T R36.4.3**?

2. Can you provide compatible versions of:

3. If no ready package is available, could you provide recommendations for adaptation, or source code/DKMS to build the drivers for kernel `5.15.148-tegra`?

Thank you.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [May 22, 2026, 6:42pm UTC](https://community.stereolabs.com/t/zed-x-drivers-for-tztek-ys-x1-32g/11338/2 "2026-05-22T18:42:28Z")

</div>

Hi @dbarinov  
Welcome to the [StereoLabs](https://www.stereolabs.com/) community.

> [@dbarinov](#):
>
> Is there a ready-to-use driver/BSP for **ZED X + TZTEK YS-X1-32G + L4T R36.4.3**?

Unfortunately, we only provide a driver for the GEACX2-64G model.

> [@dbarinov](#):
>
> Can you provide compatible versions of:
> 
> - `sl_zedx.ko`
> - `sl_max9296.ko`
> - DTB/DTBO for MAX9296/ZED X
> - `ZEDX_Daemon`
> - ISP file for AR0234

You can contact **TZTEK** to ask for a compatible driver for the YS-X1-32G model.

> [@dbarinov](#):
>
> If no ready package is available, could you provide recommendations for adaptation, or source code/DKMS to build the drivers for kernel `5.15.148-tegra`?

You can write to [support@stereolabs.com](mailto:support@stereolabs.com) to ask to sign the required NDA to be invited to the repository of the source code of the ZED X Driver and use the provided information to develop a custom driver.

---

<div class="post-metadata">

**Author:** ![dbarinov](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/d/d26b3c/32.png) [@dbarinov](https://community.stereolabs.com/u/dbarinov)\
**Post date:** [May 25, 2026, 8:09am UTC](https://community.stereolabs.com/t/zed-x-drivers-for-tztek-ys-x1-32g/11338/3 "2026-05-25T08:09:28Z")

</div>

Hi!

Thank you for your reply.

I will try both: TZTEK and [stereolabs](https://www.stereolabs.com/) support approaches.

Also I will respond here about final resolution.