# ZED X - capture card connection to SEED J4012 ( Orin NX 16GB)

**URL:** <https://community.stereolabs.com/t/zed-x-capture-card-connection-to-seed-j4012-orin-nx-16gb/6096>\
**Category:** ZED X\
**Created:** [May 22, 2024, 8:59am UTC](https://community.stereolabs.com/t/zed-x-capture-card-connection-to-seed-j4012-orin-nx-16gb/6096 "2024-05-22T08:59:27Z")\
**Posts on this page:** 5\
**Page:** 1

<div class="post-metadata">

**Author:** ![Vivio](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/v/ccd318/32.png) [@Vivio](https://community.stereolabs.com/u/Vivio)\
**Post date:** [May 22, 2024, 8:59am UTC](https://community.stereolabs.com/t/zed-x-capture-card-connection-to-seed-j4012-orin-nx-16gb/6096/1 "2024-05-22T08:59:28Z")

</div>

Hi there,

Finally I’ve bought an ZED X with capture card.  
I want to pair it to SEEED reComputer J4012-Edge NVIDIA Jetson Orin™ NX 16GB module.

J4012 has a carrier board called J401.  
Based on this **[documentation](https://files.seeedstudio.com/products/NVIDIA/User_Guide_GMSL_Compatibility_Seeed.pdf)** I’ve connected the capture card to the J401.

 ![image](https://community.stereolabs.com/uploads/default/original/2X/a/ad832919340950485827e744962fb6dba9c1a09e.jpeg)

The docs regarding capture card and J401 are a little bit unclear if the capture card MUST be powered up with 12-19V or it gets power though the CSI port as stated in the specification of the [Stereolabs](https://www.stereolabs.com/) capture card

> - Connects to and is powered by the CSI port of the Orin/Xavier Developer Kit.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [May 22, 2024, 1:33pm UTC](https://community.stereolabs.com/t/zed-x-capture-card-connection-to-seed-j4012-orin-nx-16gb/6096/2 "2024-05-22T13:33:39Z")

</div>

Hi @Vivio  
Welcome to the [Stereolabs](https://www.stereolabs.com/) community.

> [@Vivio](#):
>
> The docs regarding capture card and J401 are a little bit unclear if the capture card MUST be powered up with 12-19V or it gets power though the CSI port as stated in the specification of the [Stereolabs](https://www.stereolabs.com/) capture card

The 12-19V power is required. The flat cables cannot provide the required current to power the capture card.

---

<div class="post-metadata">

**Author:** ![Vivio](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/v/ccd318/32.png) [@Vivio](https://community.stereolabs.com/u/Vivio)\
**Post date:** [May 22, 2024, 3:59pm UTC](https://community.stereolabs.com/t/zed-x-capture-card-connection-to-seed-j4012-orin-nx-16gb/6096/3 "2024-05-22T15:59:45Z")

</div>

Thank you @Myzhar !

If I may, I want to put some follow up questions:

1. Is there a chance to powerup the capture card internally? I want to avoid using two power supplies.

2. What’s the power consumption of the Capture card? I’ve seen that the ZED box with Orin NX 16GB & capture card is shipped with 12V/5A power supply.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [May 22, 2024, 4:15pm UTC](https://community.stereolabs.com/t/zed-x-capture-card-connection-to-seed-j4012-orin-nx-16gb/6096/4 "2024-05-22T16:15:33Z")

</div>

> [@Vivio](#):
>
> Is there a chance to powerup the capture card internally? I want to avoid using two power supplies.

You could split the Jetson power cable, so you can use the same source.

> [@Vivio](#):
>
> What’s the power consumption of the Capture card? I’ve seen that the ZED box with Orin NX 16GB & capture card is shipped with 12V/5A power supply.

1A is the recommended minimum current to be provided to the capture card.

---

<div class="post-metadata">

**Author:** ![Vivio](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/v/ccd318/32.png) [@Vivio](https://community.stereolabs.com/u/Vivio)\
**Post date:** [May 22, 2024, 4:23pm UTC](https://community.stereolabs.com/t/zed-x-capture-card-connection-to-seed-j4012-orin-nx-16gb/6096/5 "2024-05-22T16:23:57Z")

</div>

I can split it, right!

Is there a more less visible solution like on the Zed Box?

The capture card has some headers. They cannot be used for power?

I guess that soldering on the pads of the barrel jack voids my warranty.

Is there a schematic of the caprure card?

Thank you for shooting the replies fast 😄