# ZED X camera - Error CAMERA REBOOTING, (Argus) Error FileOperationFailed, InvalidState

**URL:** <https://community.stereolabs.com/t/zed-x-camera-error-camera-rebooting-argus-error-fileoperationfailed-invalidstate/10558>\
**Category:** Software\
**Tags:** sdk, jetson\
**Created:** [December 29, 2025, 11:25am UTC](https://community.stereolabs.com/t/zed-x-camera-error-camera-rebooting-argus-error-fileoperationfailed-invalidstate/10558 "2025-12-29T11:25:20Z")\
**Posts on this page:** 12\
**Page:** 1

<div class="post-metadata">

**Author:** ![daniel.mirs](https://community.stereolabs.com/user_avatar/community.stereolabs.com/daniel.mirs/32/6439_2.png) [@daniel.mirs](https://community.stereolabs.com/u/daniel.mirs)\
**Post date:** [December 29, 2025, 11:25am UTC](https://community.stereolabs.com/t/zed-x-camera-error-camera-rebooting-argus-error-fileoperationfailed-invalidstate/10558/1 "2025-12-29T11:25:20Z")

</div>

Good afternoon,

Today I was scheduled to present an industrial robotics project to a client, and unfortunately, during the demonstration, errors appeared in the data reception from the ZED X camera. This situation was completely unexpected.

This problem had already occurred previously on other Jetson platforms using SDK 5.0. However, it is now recurring with SDK 5.1, which is particularly concerning. To reconnect the camera correctly, a complete Jetson reboot is required, which is impractical in an industrial environment and critical for the project’s continuity.

Because of this, this behavior calls into question the reliability of the ZED X camera for industrial applications, relegating it more to prototyping use.

My Jetson platform version and configuration are as follows:

_Software part of jetson-stats 4.3.2 - (c) 2024, Raffaello Bonghi  
Model: NVIDIA Jetson Orin NX Engineering Reference Developer Kit - Jetpack 6.2 [L4T 36.4.3]  
NV Power Mode[0]: MAXN  
Serial Number: [XXX Show with: jetson\_release -s XXX]  
Hardware:_

- _P-Number: p3767-0000_
- _Module: NVIDIA Jetson Orin NX (16GB ram)  
Platform:_
- _Distribution: Ubuntu 22.04 Jammy Jellyfish_
- _Release: 5.15.148-tegra  
jtop:_
- _Version: 4.3.2_
- _Service: Active  
Libraries:_
- _CUDA: 12.6.68_
- _cuDNN: 9.3.0.75_
- _TensorRT: 10.3.0.30_
- _VPI: 3.2.4_
- _Vulkan: 1.3.204_
- _OpenCV: 4.8.0 - with CUDA: NO_

I would appreciate it if you could inform me what is causing these errors and how they can be resolved.

I have attached the corresponding [error logs](https://mirsrobotics-my.sharepoint.com/:t:/p/daniel_mendez/IQCWJd9wCPVcTJ3_-lDHmyb-ATOQ1IouHgwTWZ2Mk-6pTdU?e=N5gixf) and the [dmesg.log](https://mirsrobotics-my.sharepoint.com/:u:/p/daniel_mendez/IQBWQG2d6T4KT5BBcDtmcTAVAY4Ebur6O7oJVYzblmhCrog?e=EZHTGY) file for your review.

_2025-12-22T12:14:57-0300 python[3617]: (Argus) Error FileOperationFailed: Failed socket read: Connection reset by peer (in src/rpc/socket/common/SocketUtils.cpp, function readSocket(), line 79)  
2025-12-22T12:14:57-0300 python[3617]: (Argus) Error InvalidState: Argus client is exiting with 1 outstanding client threads (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 366)  
2025-12-22T12:14:57-0300 python[3617]: 2025-12-22 12:14:57,784 - WARNING - Error en grab: CAMERA REBOOTING  
2025-12-22T12:14:57-0300 python[3617]: [2025-12-22 12:14:57 UTC][ZED][INFO] CAMERA REBOOTING in sl::ERROR\_CODE sl:📷:grab(sl::RuntimeParameters)_

I look forward to your comments.

Best regards,  
Daniel Méndez

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [December 29, 2025, 1:59pm UTC](https://community.stereolabs.com/t/zed-x-camera-error-camera-rebooting-argus-error-fileoperationfailed-invalidstate/10558/2 "2025-12-29T13:59:52Z")

</div>

Hi @daniel.mirs  
Welcome to the [Stereolabs](https://www.stereolabs.com/) community.

> [@daniel.mirs](#):
>
> To reconnect the camera correctly, a complete Jetson reboot is required, which is impractical in an industrial environment and critical for the project’s continuity.

Normally, this is not required. The command `sudo service zed_x_daemon restart` should be enough to recover a camera.

If it’s not working, it means that something weird is happening.

> [@daniel.mirs](#):
>
> Module: NVIDIA Jetson Orin NX (16GB ram)

What carrier board and GMSL2 capture card are you using?

---

<div class="post-metadata">

**Author:** ![daniel.mirs](https://community.stereolabs.com/user_avatar/community.stereolabs.com/daniel.mirs/32/6439_2.png) [@daniel.mirs](https://community.stereolabs.com/u/daniel.mirs)\
**Post date:** [January 12, 2026, 8:44pm UTC](https://community.stereolabs.com/t/zed-x-camera-error-camera-rebooting-argus-error-fileoperationfailed-invalidstate/10558/3 "2026-01-12T20:44:06Z")

</div>

Hi Myzhar, thanks for your reply.

Unfortunately, the commands `sudo service nvargus-daemon restart` and `sudo service zed_x_daemon restart` almost never work in my experience. Therefore, if this happens, it’s necessary to completely restart the Jetson (ZED Box) (approximately 1-2 minutes).

My industrial machine vision system must operate 24/7 without interruption; otherwise, the production line stops, which is critical for my client. If 24/7 operation cannot be guaranteed, I will no longer be able to use this camera model in future industrial projects.

I am currently using SDK 5.1.2 and the zedbox-mini\_1.3.2-SL-MAX9296 driver. However, several times a week, and in the worst cases once a day, the “Argus Error” associated with the NVIDIA driver appears. This problem occurs on all the ZED Boxes I have purchased and with the various ZED X cameras I use.

I suspect this is a GMSL driver issue, possibly due to NVIDIA resource blocking, such as nvbuf\_utils: dmabuf\_fd.

Have you tried connecting the ZED BOXES to ZED X cameras for a 24/7 period in continuous streaming or recording mode (30-minute recordings in a row)? I’d like to know if you’ve received any reports of this type of error associated with prolonged use.

Regarding my hardware, all my ZED BOXs are the Mini model, with a 16GB Orin NX graphics card.

I look forward to your reply.

Thank you very much.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [January 13, 2026, 11:12am UTC](https://community.stereolabs.com/t/zed-x-camera-error-camera-rebooting-argus-error-fileoperationfailed-invalidstate/10558/4 "2026-01-13T11:12:30Z")

</div>

Hi @daniel.mirs  
Can you provide a brief description of how the camera is used?  
If reloading the driver does not work, it’s possible that micro-disconnections can occur.

If this is the case, the ZED X Driver v1.4.0 promises to improve the behavior.  
The new driver is currently in the QA phase, and it’s expected to be released before the end of the month if no unexpected issues arise.

---

<div class="post-metadata">

**Author:** ![daniel.mirs](https://community.stereolabs.com/user_avatar/community.stereolabs.com/daniel.mirs/32/6439_2.png) [@daniel.mirs](https://community.stereolabs.com/u/daniel.mirs)\
**Post date:** [January 13, 2026, 2:54pm UTC](https://community.stereolabs.com/t/zed-x-camera-error-camera-rebooting-argus-error-fileoperationfailed-invalidstate/10558/5 "2026-01-13T14:54:49Z")

</div>

Hi Myzhar, thank you for your response.

I use the cameras in different ways, mainly mounted on gantries to measure the load of vehicles or conveyor belts. However, regarding the Argus Error disconnections I mentioned, I have also tested them under controlled conditions, with the cameras placed on my desk, without any movement or external noise.

Specifically, I tested a setup with a ZED BOX Mini with a 16 GB Orin NX, connected to a single ZED X 4 mm camera. In addition, I tested different GMSL cable lengths on my desk (10 m, 5 m, and 1.5 m). It is worth mentioning that the CPU and GPU temperatures remain between 38 and 42 °C, as reported in the console using the jtop command.

In all the scenarios described, when the cameras are used continuously, Argus Error disconnections always appear within approximately 6 to 48 hours after the Jetson Box is powered on. However, this error occurs consistently, regardless of the hardware configuration being used.

Regarding the new driver version, I am looking forward to it so I can test it and provide feedback on whether it improves the stability issues.

Thank you and best regards.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [January 13, 2026, 3:24pm UTC](https://community.stereolabs.com/t/zed-x-camera-error-camera-rebooting-argus-error-fileoperationfailed-invalidstate/10558/6 "2026-01-13T15:24:24Z")

</div>

> [@daniel.mirs](#):
>
> It is worth mentioning that the CPU and GPU temperatures remain between 38 and 42 °C, as reported in the console using the jtop command.

What power mode are you using? Try to use `MAXN` if you are not using it.

---

<div class="post-metadata">

**Author:** ![daniel.mirs](https://community.stereolabs.com/user_avatar/community.stereolabs.com/daniel.mirs/32/6439_2.png) [@daniel.mirs](https://community.stereolabs.com/u/daniel.mirs)\
**Post date:** [January 13, 2026, 6:03pm UTC](https://community.stereolabs.com/t/zed-x-camera-error-camera-rebooting-argus-error-fileoperationfailed-invalidstate/10558/7 "2026-01-13T18:03:06Z")

</div>

That’s right, I’m using that power mode (‘MAXN’). The CPU and GPU temperatures aren’t high because the workload only involves recording or streaming from a single camera. Therefore, it’s not putting a heavy load on the CPU or GPU.

---

<div class="post-metadata">

**Author:** ![JWhitleyWork](https://community.stereolabs.com/user_avatar/community.stereolabs.com/jwhitleywork/32/6011_2.png) [@JWhitleyWork](https://community.stereolabs.com/u/JWhitleyWork)\
**Post date:** [March 27, 2026, 8:35am UTC](https://community.stereolabs.com/t/zed-x-camera-error-camera-rebooting-argus-error-fileoperationfailed-invalidstate/10558/8 "2026-03-27T08:35:42Z")

</div>

We are seeing this issue as well and I have seen it at previous companies. We are specifically using ZedX cameras but I have seen it with ZedX 4KOne cameras as well. I ultimately had to create a monitoring script which would look for this error in the logs and force-restart both the `nvargus-daemon.service` and `zed_x_daemon.service` which would _usually_ fix the issue but now we are also using a Neousys IPC and that device does not use the `zed_x_daemon.service`. I am still testing to see whether only restarting the `nvargus-daemon.service` will solve the issue. We are happy to provide logs but we need a solution.

Our current configuration:

- Neousys NRU-230V-AWP-JAO64GB
- JetPack 6.2.1
- 2x or 4x ZedX Stereo cameras
- MAX\_N power mode
- `jetson_clocks` run at start-up
- Using ROS2 with [GitHub - stereolabs/zed-ros2-wrapper: ROS 2 wrapper for the ZED SDK · GitHub](https://github.com/stereolabs/zed-ros2-wrapper)

---

<div class="post-metadata">

**Author:** ![metalerk](https://community.stereolabs.com/user_avatar/community.stereolabs.com/metalerk/32/5516_2.png) [@metalerk](https://community.stereolabs.com/u/metalerk)\
**Post date:** [April 13, 2026, 5:16pm UTC](https://community.stereolabs.com/t/zed-x-camera-error-camera-rebooting-argus-error-fileoperationfailed-invalidstate/10558/9 "2026-04-13T17:16:17Z")

</div>

We’ve been having the same issue for a year now.

```auto
>>> sl.Camera.get_device_list()
[ZED X Mini (0) /dev/i2c-9 SN50998557 AVAILABLE, ZED X Mini (1) /dev/i2c-10 SN52927714 NOT AVAILABLE]
>>> sl.Camera.get_device_list()[1].camera_state
NOT AVAILABLE
>>> c = sl.Camera.get_device_list()[1]
>>> serial = c.serial_number
>>> cam = sl.Camera()
>>> init = sl.InitParameters()
>>> init.set_from_serial_number(serial)
>>> init.camera_resolution = sl.RESOLUTION.HD1200
>>> init.camera_fps = 30
>>> init.depth_mode = sl.DEPTH_MODE.NONE
>>> init.sdk_verbose = 1
>>> result = cam.open(init)
[2026-04-13 16:59:30 UTC][ZED][INFO] Logging level INFO
[2026-04-13 16:59:30 UTC][ZED][ERROR] CAMERA STREAM FAILED TO START in sl::ERROR_CODE sl:Camera:open(sl::InitParameters)
>>> result
CAMERA STREAM FAILED TO START
>>> sl.Camera.reboot(c.serial_number)
[2026-04-13 17:00:51 UTC][ZED][ERROR] INVALID FUNCTION CALL in static sl::ERROR_CODE sl:Camera:reboot(int, bool)
INVALID FUNCTION CALL

```

Restarting the daemon is not possible since we run this inside a container. And it seems that every time the daemon tries to self heal, something goes south again:

```auto
(Argus) Error Timeout: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
(Argus) Error Timeout: (propagating from src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 137)
(Argus) Error Timeout: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
(Argus) Error Timeout: (propagating from src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 137)
(Argus) Error Timeout: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
[produceDualV5] CAM1 No event is queue...Waiting C=1, status is 11 and queue size is (Argus) Error Timeout: (propagating from src/rpc/socket/client/ClientSocketManager.cpp,
 function send(), line 137)
(Argus) Error Timeout: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
0
[2026-04-13 16:45:05 UTC][ZED][ERROR] [ZED-Argus] Capture Error for CAM1 Err = 6||6
[2026-04-13 16:45:05 UTC][ZED][WARNING] [ZED-Argus]{produceDualV5} CAM 1 has timeout -- recovering...
(Argus) Error Timeout: (propagating from src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 137)
(Argus) Error Timeout: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
[ZED-Argus]{produceDualV5} CAM 1 has exited

```

We’ve tried with several different SDK versions, including the latest ones, but it remains the same.  
We’ve also tried with `set_from_serial_port` but the same thing happens.

---

<div class="post-metadata">

**Author:** ![Suveen](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/s/a9adbd/32.png) [@Suveen](https://community.stereolabs.com/u/Suveen)\
**Post date:** [April 22, 2026, 10:35am UTC](https://community.stereolabs.com/t/zed-x-camera-error-camera-rebooting-argus-error-fileoperationfailed-invalidstate/10558/10 "2026-04-22T10:35:21Z")

</div>

we’re hitting the same `Argus AlreadyAllocated: Device 0 (of 1) is in use` on a ZED Box Mini with two ZED X One GS cameras.

Basically when connecting 1 camera to the ZED box mini and ran the ZED explorer UI, it’s able to detect and stream the video feed.

But when both cameras are connected to the ZED box mini, the explorer UI couldn’t connect to the cameras and timed out with the errors shown in the screenshot.

 ![unnamed (2)](https://community.stereolabs.com/uploads/default/original/2X/7/7f88f90709d7b234708d51f49ecf8cd49fd64a0e.jpeg)

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [May 4, 2026, 4:09pm UTC](https://community.stereolabs.com/t/zed-x-camera-error-camera-rebooting-argus-error-fileoperationfailed-invalidstate/10558/11 "2026-05-04T16:09:40Z")

</div>

Hi @Suveen  
does this happen using the latest ZED X Driver v1.4.1 and the latest ZED SDK v5.3?

---

<div class="post-metadata">

**Author:** ![tiedvards](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/t/dc4da7/32.png) [@tiedvards](https://community.stereolabs.com/u/tiedvards)\
**Post date:** [May 5, 2026, 10:23am UTC](https://community.stereolabs.com/t/zed-x-camera-error-camera-rebooting-argus-error-fileoperationfailed-invalidstate/10558/12 "2026-05-05T10:23:50Z")

</div>

Hi @Myzhar,

We’re hitting a very similar pattern on our side — 4× ZED X on ZED Box Orin NX 16GB running 24/7 in an industrial recording station. We see random failures specifically around Camera.open() and Camera.close(), sometimes recoverable via `sudo systemctl restart zed_x_daemon`, sometimes only via full Jetson reboot. SDK 5.0, MAXN, depth NONE, HD1200 @ 30fps, H265 SVO2. Service runs in a Docker container (privileged, network=host), planning to update to ZED Link Driver 1.4.1.

Currently we open/close all 4 cameras per recording session (truck arrives \> open \> record ~50s \> stop \> close). Most failures we observe happen on the open/close transitions, not during streaming.

My direct question:

**Is it a good practice to keep all 4 cameras permanently open at service startup, and only toggle `enable_recording` / `disable_recording` per session — instead of open/close per session? Or is this discouraged for some reason?**

Intuitively it should reduce exposure to the flaky open/close paths, but we want to make sure we’re not trading one problem for another (sensor drift, resource leaks during long idle streaming, sync issues, anything unexpected on the SDK side).

Any official recommendation or experience from other 24/7 deployments would be very helpful. Thanks!