# ZED\_SVO\_Export Requires having the Camera that taken the records?

**URL:** <https://community.stereolabs.com/t/zed-svo-export-requires-having-the-camera-that-taken-the-records/11604>\
**Category:** Python\
**Tags:** svo, jetson\
**Created:** [August 4, 2026, 8:22am UTC](https://community.stereolabs.com/t/zed-svo-export-requires-having-the-camera-that-taken-the-records/11604 "2026-08-04T08:22:17Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![NivC](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/n/ecae2f/32.png) [@NivC](https://community.stereolabs.com/u/NivC)\
**Post date:** [August 4, 2026, 8:22am UTC](https://community.stereolabs.com/t/zed-svo-export-requires-having-the-camera-that-taken-the-records/11604/1 "2026-08-04T08:22:17Z")

</div>

Hi [Stereolabs](https://www.stereolabs.com/) team,

I am using a setup with three **ZED X One** cameras. Two of the cameras are configured as a stereo pair, while the third camera is used independently.

My hardware and software configuration is a Jetson Orin Nano Super Developer Kit running JetPack 6.2.1 with ZED SDK 5.2.3 and the [stereolabs](https://www.stereolabs.com/)-zedlink-duo driver version 1.4.2.

I am encountering an issue when trying to open or convert an **SVO2** file that was recorded by a camera that has already been delivered to a customer and is no longer available to me.

Since I need to review the customer’s recordings on my Jetson or Windows PC, I would like to convert the SVO2 recording into a standard video format, such as MP4 or another commonly supported format. I do have additional **ZED X One** cameras available, but they have different serial numbers than the camera that originally recorded the file.

When I try to use the `ZED_SVO_Export` sample located at `/usr/local/zed/samples/recording/export/svo/cpp/build/ZED_SVO_Export`, I receive the following error:

```auto
[2026-08-04 10:22:52 UTC][ZED][WARNING] MODULE NOT COMPATIBLE WITH SELECTED CAMERA
in sl::ERROR_CODE sl::CameraOneImpl::open(const sl::InitParametersOne&)

```

Is it possible to export an SVO2 file (for example, using `ZED_SVO_Export`) without opening or connecting any camera?

If a camera must be opened, can I use another **ZED X One** camera that I own, even though it is not the same physical camera that originally recorded the SVO2 file?

For reference, I tested `ZED_SVO_Export` with an SVO2 file recorded using one of my own cameras, and the export works correctly. The issue only occurs with the recording received from the customer’s camera.

Thank you for your help!

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [August 4, 2026, 7:00pm UTC](https://community.stereolabs.com/t/zed-svo-export-requires-having-the-camera-that-taken-the-records/11604/2 "2026-08-04T19:00:16Z")

</div>

Hi @NivC

> [@NivC](#):
>
> When I try to use the `ZED_SVO_Export` sample located at `/usr/local/zed/samples/recording/export/svo/cpp/build/ZED_SVO_Export`, I receive the following error:
> 
> ```auto
> [2026-08-04 10:22:52 UTC][ZED][WARNING] MODULE NOT COMPATIBLE WITH SELECTED CAMERA
> in sl::ERROR_CODE sl::CameraOneImpl::open(const sl::InitParametersOne&)
> 
> ```

What version of the ZED SDK are you using?  
Have you tried to open the SVO with the new [ZED SDK v5.4.1](https://www.stereolabs.com/en-it/developers/release)?