# ZED SDK v3.8 is out!

**URL:** <https://community.stereolabs.com/t/zed-sdk-v3-8-is-out/1667>\
**Category:** Announcement\
**Tags:** release, sdk\
**Created:** [October 18, 2022, 7:27am UTC](https://community.stereolabs.com/t/zed-sdk-v3-8-is-out/1667 "2022-10-18T07:27:48Z")\
**Posts on this page:** 5\
**Page:** 1

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [October 18, 2022, 7:27am UTC](https://community.stereolabs.com/t/zed-sdk-v3-8-is-out/1667/1 "2022-10-18T07:27:48Z")

</div>

[Download it now](https://www.stereolabs.com/developers/release)

## What’s New

2022-10-18

ZED SDK 3.8 is a major release that includes new features and performance improvements to depth sensing and body tracking. This update brings up to 50% performance improvement for Neural depth sensing. Human skeleton tracking has also been sped up by +40% on most platforms. The Linux installer size has been reduced by 50%.

A new plugin for Unreal Engine 5 is now available. The latest ROS2 LTS distribution Humble Hawksbill is also now supported.

Note: On Linux, the “zstd” package is now required to uncompress the installer (see details below).

## 3.8.0

### New Features

- Improved Neural depth runtime by up to 50%
  - Depth FPS now reaches 60FPS on platforms such as Jetson AGX Orin, and 30FPS for 2 cameras.
  - This speed-up is a combination of network optimization, pruning and improved usage of FP16 inference for supported configuration. It applied to all GPU.

- Added a new Camera::setRegionOfInterest function.
  - It defines a region of interest with a mask to focus on for all the SDK, discarding other parts.
  - It can be useful to filter out known objects that are irrelevant, such as vehicle hoods or drone propellers that can degrade positional tracking or depth estimation by adding noises. Two new samples are now available.

- Added a new ObjectDetectionParameters::allow\_reduced\_precision\_inference parameter.
  - This parameter enables AI inference with quantization to improve runtime while allowing a slight decrease in accuracy. By default all AI models are running in fp16 (half) with no accuracy difference when the GPU supports (requires a Jetson or Volta GPU and newer) it and fallback to fp32 otherwise. This mode allows int8 inference that provides x4 the throughput on supported operations compared to fp32 and decreases the memory usage.
  - The accuracy loss should not exceed 1-2% on the compatible models. For now, only HUMAN\_BODY\_xxxx models support it.

### Improvements

- Improved Depth Viewer rendering pipeline, especially on Jetson. It is now up to 50% faster.
- Improved sharpening behavior, the lowest setting now disables it. The processing has also been improved and no longer produces color artifacts.
- Added PositionalTrackingParameters::set\_gravity\_as\_origin parameter. It allows you to set the odometry world position using sensor data. For instance, if true (default), the initial\_world\_transform will be aligned with IMU gravity by keeping the user’s yaw.
- Added PositionalTrackingParameters::depth\_min\_range parameter to change the minimum range of the odometry. It may be useful if we want to remove some fixed objects in near range.
- Added ObjectDetectionParameters::prediction\_timeout\_s parameter to tune the prediction time when an object disappears. When an object is not detected anymore, the SDK will predict its positions for a short period of time before its state switches to SEARCHING. This parameter prevents the jittering of the object state when there is a short misdetection
- Improved floor plane detection stability
- Introduced a new sl::POSITIONAL\_TRACKING\_STATE::SEARCHING\_FLOOR\_PLANE, when you use the sl::PositionalTrackingParameter::set\_floor\_as\_origin, to know if the positional tracking is started or not
- sl::Mat class has been improved to allow faster transfers. The updateGPUfromCPU and updateCPUfromGPU, as well as copyTo, now include a cudaStream\_t parameter to asynchronously retrieve the data when using GPU memory.
- Added a support function, sl::convertImage, to convert image format from sl::MAT\_TYPE::U8C4 to sl::MAT\_TYPE::S8C4, mainly for Unreal Engine.
- On Linux, the installers now use zstandard as the default compression (previously gzip). They are now half the size and twice faster to extract. The zstd package must be installed (sudo apt install zstd) to use the ZED SDK installer.

### Bug Fixes

- Fixed a slight drift in sl::Pose from the Camera::getPosition function when using sl::REFERENCE\_FRAME::CAMERA. The cumulative pose from this local pose could introduce a huge drift compared to the sl::Pose from sl::REFERENCE\_FRAME::WORLD when loop closure is disabled

### Integrations

#### Python

- Improve installation script with better python package folder detection (reported by Github user @GER-Jani).

#### Unreal

- Release of a new plugin compatible with Unreal Engine 5

#### [Unity](https://github.com/stereolabs/zed-unity)

- Add the option to open the camera by its serial number.

#### [ROS 2](https://github.com/stereolabs/zed-ros2-wrapper)

- Added support for ROS2 Humble Hawksbill. Thx @nakai-omer. The two ROS2 LTS releases are now supported simultaneously.
- Fixed a wrong behavior of the set\_pose service. Now the initial odometry is coherent with the new starting point value used as a parameter.
- Added Plane Detection feature. [Read more](https://www.stereolabs.com/docs/ros2/plane-detection).
- Added a sub-set of parameters for debugging with new parameters debug\_mode and debug\_sensors.
- Fixed the “NO DEPTH” mode. By setting depth.quality to 0 now the depth extraction and all the sub-modules depending on it are correctly disabled.
- Set read\_only flag in the parameter descriptor for non-dynamic parameters. Thx @bjsowa.
- Enabled Intra Process Communication (IPC). The ZED node no longer publishes topics with TRANSIENT LOCAL durability.
- Added TF broadcasting diagnostic.
- Fixed data grabbing frame rate when publishing is set to a lower value.
- Improved IMU/Left Camera TF broadcasting at IMU frequency.
- Improved TF broadcasting at grabbing frequency.
- Fixed random errors when closing the node.
- New data thread configuration to maximize data publishing frequency.
- Sensor data publishing moved from timer to thread.
- RGB/Depth data publishing moved from timer to thread.
- Moved Sensor Parameters from cameras configuration files to common.yaml.
- Moved Object Detection parameters from cameras configuration files to common.yaml.
- The parameter general.sdk\_verbose is now an integer accepting different SDK verbose levels.
- Added a new benchmarking tool in the zed-ros2-examples repository to get frequency and bandwidth information from a subscribed topic and plot data.

#### [ROS](https://github.com/stereolabs/zed-ros-wrapper)

- Fixed TF timestamp issue in SVO mode.
- Added Plane Detection. [Read more](https://www.stereolabs.com/docs/ros/plane_detection).
- Fixed wrong TF broadcasting when calling the set\_pose, reset\_tracking, and reset\_odometry services. Now the initial odometry is coherent with the new starting point.
- Added parameter sensors/max\_pub\_rate to set the maximum publishing frequency of sensors data
- Improved Sensors thread.
- Fixed the frame links of barometer, magnetometer, and temperature sensors for ZED2i.

### Deprecations

- CUDA 10.0 installers are no longer supported with this release. Users are encouraged to migrate to the latest CUDA 11.X.
- While CUDA 10.2 is still supported, users are strongly encouraged to migrate to CUDA 11.X, which provides a performance improvement between 20 to 40% with the same hardware.
- Jetson users are encouraged to move the latest L4T 35.1 when using a Xavier and Orin, and L4T 32.7 for Nano and TX2. The L4T 32.3, 32.4, 32.5, 32.6 are now deprecated.

---

<div class="post-metadata">

**Author:** ![salsus](https://community.stereolabs.com/user_avatar/community.stereolabs.com/salsus/32/793_2.png) [@salsus](https://community.stereolabs.com/u/salsus)\
**Post date:** [October 24, 2022, 5:06am UTC](https://community.stereolabs.com/t/zed-sdk-v3-8-is-out/1667/2 "2022-10-24T05:06:14Z")

</div>

Thankyou so much to the team for all your hard work!

Ive been using the UE 4.21 custom engine for a project passing the ZED camera feed to the engine for a MR app, and have been keenly watching for this update - I can see the LiveLink repo has been updated to 5 but not the UE plugin repo, was this 3.8 SDK UE update only to the LiveLink plugin or are there plans to port the base plugin over too?

---

<div class="post-metadata">

**Author:** ![BenjaminV](https://community.stereolabs.com/user_avatar/community.stereolabs.com/benjaminv/32/3863_2.png) [@BenjaminV](https://community.stereolabs.com/u/BenjaminV)\
**Post date:** [October 24, 2022, 11:35am UTC](https://community.stereolabs.com/t/zed-sdk-v3-8-is-out/1667/3 "2022-10-24T11:35:39Z")

</div>

Hi,

Are you currently using the V3.7 version of the plugin ?  
If so, you should just need to change the Minor version here ([zed-unreal-plugin/Stereolabs.Build.cs at UE4.21\_ZedSdk3.7 · stereolabs/zed-unreal-plugin · GitHub](https://github.com/stereolabs/zed-unreal-plugin/blob/UE4.21_ZedSdk3.7/Stereolabs/Source/Stereolabs/Stereolabs.Build.cs#L91)) to “8” and it should compile with the ZED SDK 3.8.

Best,  
Benjamin Vallon

---

<div class="post-metadata">

**Author:** ![salsus](https://community.stereolabs.com/user_avatar/community.stereolabs.com/salsus/32/793_2.png) [@salsus](https://community.stereolabs.com/u/salsus)\
**Post date:** [October 26, 2022, 4:29am UTC](https://community.stereolabs.com/t/zed-sdk-v3-8-is-out/1667/4 "2022-10-26T04:29:10Z")

</div>

@BenjaminV Thankyou very much for the quick response!

Were there any docs on getting the ZED UE Plugin working in 5 under the new SDK ver? (This repo [GitHub - stereolabs/zed-unreal-plugin: Stereolabs ZED - UE4 Plugin](https://github.com/stereolabs/zed-unreal-plugin) )

---

<div class="post-metadata">

**Author:** ![BenjaminV](https://community.stereolabs.com/user_avatar/community.stereolabs.com/benjaminv/32/3863_2.png) [@BenjaminV](https://community.stereolabs.com/u/BenjaminV)\
**Post date:** [October 26, 2022, 7:22am UTC](https://community.stereolabs.com/t/zed-sdk-v3-8-is-out/1667/5 "2022-10-26T07:22:22Z")

</div>

As you know, this plugin requires a custom version of the engine to work, which makes it difficult to use for you and difficult to maintain for us.

That’s why we decided to make a new version of the plugin which will be compatible with standard UE5.  
Some features won’t be available for the moment (mostly VR headset compatibility, MR lightning/shading).

Best,  
Benjamin Vallon