# ZED SDK v3.7.4 is out!

**URL:** <https://community.stereolabs.com/t/zed-sdk-v3-7-4-is-out/1163>\
**Category:** Announcement\
**Created:** [May 20, 2022, 10:52am UTC](https://community.stereolabs.com/t/zed-sdk-v3-7-4-is-out/1163 "2022-05-20T10:52:22Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [May 20, 2022, 10:52am UTC](https://community.stereolabs.com/t/zed-sdk-v3-7-4-is-out/1163/1 "2022-05-20T10:52:22Z")

</div>

The new ZED SDK patch version 3.7.4 includes also the enhancements introduced with the v3.7.3 released a few days ago:

# 3.7.4

## Security Fixes

- Fixed security issue on Linux: the installed udev rules, to open the IMU without root access, were incorrect and could allow privilege escalation.

## Improvements

- Removed warning verbose of deprecated functions during compilation

# 3.7.3

## Improvements

- Added AI model download and optimization progress bars

## Bug Fixes

- Fixed possible crash in Reid model optimization
- Fixed spatial mapping invalid behavior when using multiple camera simultaneously
- Fixed Custom object detector random infinite loops
- Fixed self-calibration undeterministic behavior when reading the same SVO multiple times.

## Tools

- Fixed regression ZED Explorer streaming input

## Samples

- Added support for YOLOv5 v6 in the custom detector cpp sample
- Improved sample cmakes

## Integrations

### Python

- Improved numpy conversion in get\_data() function by removing the deep copy by default (up to 30% faster samples)
- Fixed missing timestamp attribute for Mat class

Download page: [https://www.stereolabs.com/developers/release/](https://www.stereolabs.com/developers/release/)