# ZED SDK Installation Fails in Docker on JetPack 6.1 (nvargus-daemon Error)

**URL:** <https://community.stereolabs.com/t/zed-sdk-installation-fails-in-docker-on-jetpack-6-1-nvargus-daemon-error/7856>\
**Category:** Docker\
**Tags:** jetson\
**Created:** [January 9, 2025, 6:05pm UTC](https://community.stereolabs.com/t/zed-sdk-installation-fails-in-docker-on-jetpack-6-1-nvargus-daemon-error/7856 "2025-01-09T18:05:20Z")\
**Posts on this page:** 7\
**Page:** 1

<div class="post-metadata">

**Author:** ![ba2sakal](https://community.stereolabs.com/user_avatar/community.stereolabs.com/ba2sakal/32/4031_2.png) [@ba2sakal](https://community.stereolabs.com/u/ba2sakal)\
**Post date:** [January 9, 2025, 6:05pm UTC](https://community.stereolabs.com/t/zed-sdk-installation-fails-in-docker-on-jetpack-6-1-nvargus-daemon-error/7856/1 "2025-01-09T18:05:20Z")

</div>

I am attempting to install the ZED SDK on my Jetson device running JetPack 6.1 in a Docker container, but the installation fails with the following error:

```auto
sed: can't read /etc/systemd/system/nvargus-daemon.service: No such file or directory

```

While this service exists on my host system, it seems to be inaccessible or missing inside the Docker container. Despite the script displaying `ZED SDK installation complete!`, the SDK is not installed, and I cannot proceed.

#### System Information:

- **JetPack Version:** 6.1 (L4T 36.4)
- **CUDA Version:** 12.6
- **SDK Version:** ZED SDK 4.2
- **Base OS (Host):** Ubuntu 22.04 (arm64)
- **Container Base Image:** NVIDIA L4T Base Image (arm64)

#### Installation Steps:

1. Installed all dependencies inside the Docker container using `apt-get`.
2. Downloaded the ZED SDK installation file (`ZED_SDK_Linux.run`) to `/tmp` in the container.
3. Ran the installation command inside the Docker container:

```auto
sudo -u admin ./ZED_SDK_Linux.run silent skip_od_module skip_python skip_drivers

```

1. Encountered the error about the missing `nvargus-daemon.service`.

#### Observations:

- The file `/etc/systemd/system/nvargus-daemon.service` exists on the host system but is not available inside the Docker container.
- This may be causing the ZED SDK installation script to fail.

#### Questions:

1. How can I resolve the `nvargus-daemon.service` issue in the Docker environment?
2. Do I need to mount additional host files or services into the container to make this work?

#### Additional Context:

I followed the Docker setup guidelines provided in the NVIDIA Isaac ROS documentation and included the following steps in the Dockerfile:

I install from ISAAC ROS Repo with

```auto
# Based on https://github.com/stereolabs/zed-docker

# Download dependencies for zed SDK installation RUN file
sudo apt-get update -y || true
sudo apt-get install --no-install-recommends lsb-release wget less zstd udev sudo apt-transport-https -y

# Download zed SDK installation RUN file to /tmp directory
cd /tmp

wget -q --no-check-certificate -O ZED_SDK_Linux.run +wget -q --no-check-certificate -O ZED_SDK_Linux.run https://download.stereolabs.com/zedsdk/4.2/l4t36.4/jetsons
sudo chmod 777 ./ZED_SDK_Linux.run
sudo -u admin ./ZED_SDK_Linux.run silent skip_od_module skip_python skip_drivers
# Symlink required to use the streaming features on Jetson inside a container, based on
# https://github.com/stereolabs/zed-docker/blob/fd514606174d8bb09f21a229f1099205b284ecb6/4.X/l4t/devel/Dockerfile#L27C5-L27C95
sudo ln -sf /usr/lib/aarch64-linux-gnu/tegra/libv4l2.so.0 /usr/lib/aarch64-linux-gnu/libv4l2.so

# Cleanup
sudo rm -rf /usr/local/zed/resources/*
rm -rf ZED_SDK_Linux.run
sudo rm -rf /var/lib/apt/lists/*

```

```auto
:/workspaces/isaac_ros-dev$ sudo chmod +x ${ISAAC_ROS_WS}/src/isaac_ros_common/docker/scripts/install-zed-aarch64.sh && \
${ISAAC_ROS_WS}/src/isaac_ros_common/docker/scripts/install-zed-aarch64.sh
Hit:1 http://ports.ubuntu.com/ubuntu-ports jammy InRelease
Get:2 http://ports.ubuntu.com/ubuntu-ports jammy-updates InRelease [128 kB]                                                                 
Hit:3 https://repo.download.nvidia.com/jetson/common r36.4 InRelease                                                                        
Hit:4 http://packages.ros.org/ros2/ubuntu jammy InRelease                                                                                   
Hit:5 https://isaac.download.nvidia.com/isaac-ros/release-3 jammy InRelease                                                                 
Hit:6 http://ports.ubuntu.com/ubuntu-ports jammy-backports InRelease                                                                        
Hit:7 https://deb.nodesource.com/node_18.x nodistro InRelease                                                                               
Hit:8 https://dl.yarnpkg.com/debian stable InRelease                                                                                        
Get:9 http://ports.ubuntu.com/ubuntu-ports jammy-security InRelease [129 kB]                                    
Hit:10 https://developer.download.nvidia.com/compute/cuda/repos/ubuntu2204/arm64 InRelease         
Hit:11 https://repo.download.nvidia.com/jetson/t234 r36.4 InRelease                                 
Hit:12 https://ppa.launchpadcontent.net/mosquitto-dev/mosquitto-ppa/ubuntu jammy InRelease
Get:13 http://ports.ubuntu.com/ubuntu-ports jammy-security/restricted arm64 Packages [2,805 kB]
Get:14 http://ports.ubuntu.com/ubuntu-ports jammy-security/multiverse arm64 Packages [24.2 kB]
Get:15 http://ports.ubuntu.com/ubuntu-ports jammy-security/main arm64 Packages [2,227 kB]
Fetched 5,313 kB in 6s (903 kB/s)                            
Reading package lists... Done
W: https://repo.download.nvidia.com/jetson/common/dists/r36.4/InRelease: Key is stored in legacy trusted.gpg keyring (/etc/apt/trusted.gpg), see the DEPRECATION section in apt-key(8) for details.
W: https://isaac.download.nvidia.com/isaac-ros/release-3/dists/jammy/InRelease: Key is stored in legacy trusted.gpg keyring (/etc/apt/trusted.gpg), see the DEPRECATION section in apt-key(8) for details.
W: https://dl.yarnpkg.com/debian/dists/stable/InRelease: Key is stored in legacy trusted.gpg keyring (/etc/apt/trusted.gpg), see the DEPRECATION section in apt-key(8) for details.
W: https://repo.download.nvidia.com/jetson/t234/dists/r36.4/InRelease: Key is stored in legacy trusted.gpg keyring (/etc/apt/trusted.gpg), see the DEPRECATION section in apt-key(8) for details.
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
lsb-release is already the newest version (11.1.0ubuntu4).
zstd is already the newest version (1.4.8+dfsg-3build1).
zstd set to manually installed.
less is already the newest version (590-1ubuntu0.22.04.3).
less set to manually installed.
sudo is already the newest version (1.9.9-1ubuntu2.4).
udev is already the newest version (249.11-0ubuntu3.12).
wget is already the newest version (1.21.2-2ubuntu1.1).
apt-transport-https is already the newest version (2.4.13).
0 upgraded, 0 newly installed, 0 to remove and 42 not upgraded.
Verifying archive integrity... 100% MD5 checksums are OK. All good.
Uncompressing 'ZED camera SDK by Stereolabs (Use 'sudo apt install zstd' if zstd is not found)' 100%  
WARNING: unknown parameter "skip_drivers" (ignored)
USAGE: 
        -h --help
        --silent
        --runtime_only
        --skip_tools
        --skip_cuda
        --skip_od_module
        --skip_python
        --skip_hub

L4T version 36.4 detected. OK
Installation path: /usr/local/zed
Checking CUDA version...
OK: Found CUDA 12.6
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
libjpeg-turbo8 is already the newest version (2.1.2-0ubuntu1).
libjpeg-turbo8 set to manually installed.
libpng-dev is already the newest version (1.6.37-3build5).
libpng-dev set to manually installed.
libv4l-0 is already the newest version (1.22.1-2build1).
freeglut3-dev is already the newest version (2.8.1-6).
libglew-dev is already the newest version (2.2.0-4).
libglew-dev set to manually installed.
libopenblas-dev is already the newest version (0.3.20+ds-1).
libqt5svg5 is already the newest version (5.15.3-1).
libqt5svg5 set to manually installed.
libturbojpeg is already the newest version (2.1.2-0ubuntu1).
qtchooser is already the newest version (66-2build1).
qtchooser set to manually installed.
curl is already the newest version (7.81.0-1ubuntu1.20).
libarchive-dev is already the newest version (3.6.0-1ubuntu1.3).
libusb-1.0-0 is already the newest version (2:1.0.25-1ubuntu2).
libusb-1.0-0 set to manually installed.
libusb-1.0-0-dev is already the newest version (2:1.0.25-1ubuntu2).
libusb-1.0-0-dev set to manually installed.
unzip is already the newest version (6.0-26ubuntu3.2).
zlib1g is already the newest version (1:1.2.11.dfsg-2ubuntu9.2).
libqt5opengl5 is already the newest version (5.15.3+dfsg-2ubuntu0.2).
libqt5opengl5 set to manually installed.
qt5-qmake is already the newest version (5.15.3+dfsg-2ubuntu0.2).
qt5-qmake set to manually installed.
qtbase5-dev is already the newest version (5.15.3+dfsg-2ubuntu0.2).
qtbase5-dev set to manually installed.
qtbase5-dev-tools is already the newest version (5.15.3+dfsg-2ubuntu0.2).
qtbase5-dev-tools set to manually installed.
The following additional packages will be installed:
  mesa-utils-bin
The following NEW packages will be installed:
  mesa-utils mesa-utils-bin
0 upgraded, 2 newly installed, 0 to remove and 42 not upgraded.
Need to get 1,117 kB of archives.
After this operation, 2,418 kB of additional disk space will be used.
Get:1 http://ports.ubuntu.com/ubuntu-ports jammy/universe arm64 mesa-utils-bin arm64 8.4.0-1ubuntu1 [52.2 kB]
Get:2 http://ports.ubuntu.com/ubuntu-ports jammy/universe arm64 mesa-utils arm64 8.4.0-1ubuntu1 [1,065 kB]
Fetched 1,117 kB in 1s (1,729 kB/s)   
debconf: unable to initialize frontend: Dialog
debconf: (No usable dialog-like program is installed, so the dialog based frontend cannot be used. at /usr/share/perl5/Debconf/FrontEnd/Dialog.pm line 78, <> line 2.)
debconf: falling back to frontend: Readline
Selecting previously unselected package mesa-utils-bin:arm64.
(Reading database ... 168386 files and directories currently installed.)
Preparing to unpack .../mesa-utils-bin_8.4.0-1ubuntu1_arm64.deb ...
Unpacking mesa-utils-bin:arm64 (8.4.0-1ubuntu1) ...
Selecting previously unselected package mesa-utils.
Preparing to unpack .../mesa-utils_8.4.0-1ubuntu1_arm64.deb ...
Unpacking mesa-utils (8.4.0-1ubuntu1) ...
Setting up mesa-utils-bin:arm64 (8.4.0-1ubuntu1) ...
Setting up mesa-utils (8.4.0-1ubuntu1) ...
Processing triggers for man-db (2.10.2-1) ...
W: --force-yes is deprecated, use one of the options starting with --allow instead.
Running in chroot, ignoring request.
Running in chroot, ignoring request.
sed: can't read /etc/systemd/system/nvargus-daemon.service: No such file or directory

ZED SDK installation complete !

```

Any assistance or insights on resolving this issue would be greatly appreciated!

---

<div class="post-metadata">

**Author:** ![beniaminopozzan](https://community.stereolabs.com/user_avatar/community.stereolabs.com/beniaminopozzan/32/3586_2.png) [@beniaminopozzan](https://community.stereolabs.com/u/beniaminopozzan)\
**Post date:** [January 10, 2025, 1:49pm UTC](https://community.stereolabs.com/t/zed-sdk-installation-fails-in-docker-on-jetpack-6-1-nvargus-daemon-error/7856/2 "2025-01-10T13:49:12Z")

</div>

Hi @ba2sakal , I’m having the _exact_ same issue.  
However, the SDK seems to be installed properly afterwards: I see the `ZED_*` utility commands and the ROS2 ZED packages can find the ZED SDK and I can compile them.

---

<div class="post-metadata">

**Author:** ![adujardin](https://community.stereolabs.com/user_avatar/community.stereolabs.com/adujardin/32/4125_2.png) [@adujardin](https://community.stereolabs.com/u/adujardin)\
**Post date:** [January 10, 2025, 5:03pm UTC](https://community.stereolabs.com/t/zed-sdk-installation-fails-in-docker-on-jetpack-6-1-nvargus-daemon-error/7856/3 "2025-01-10T17:03:20Z")

</div>

Hi,

The ZED SDK installer is misleading, the _skip\_driver_ option was missing and the installer tries to set up the driver in the container and doesn’t find the expected resources. This will be addressed in a future patch. The error messages can be ignored.

Here’s a doc page that should clarify the situation: [How to use ZED X with Docker - Stereolabs](https://www.stereolabs.com/docs/get-started-with-zed-x/zed-x-and-docker)

→ The driver must be installed on the host, only  
 → The container requires several volumes to be mounted to have a working ZED X from docker

---

<div class="post-metadata">

**Author:** ![beniaminopozzan](https://community.stereolabs.com/user_avatar/community.stereolabs.com/beniaminopozzan/32/3586_2.png) [@beniaminopozzan](https://community.stereolabs.com/u/beniaminopozzan)\
**Post date:** [January 10, 2025, 7:39pm UTC](https://community.stereolabs.com/t/zed-sdk-installation-fails-in-docker-on-jetpack-6-1-nvargus-daemon-error/7856/5 "2025-01-10T19:39:01Z")

</div>

@adujardin thanks! That’s nice to know it is that error can be ignored! I hope the patch will be released soon!

@ba2sakal , I think we are using the same setup (only one camera on my side though and no display connected to the Jetson) I’m struggling a lot at trying to get the `zed_camera.launch.py` running as `admin` and I get it working only as `root`. Are you able to run the lauchfile as `admin`?

---

<div class="post-metadata">

**Author:** ![ba2sakal](https://community.stereolabs.com/user_avatar/community.stereolabs.com/ba2sakal/32/4031_2.png) [@ba2sakal](https://community.stereolabs.com/u/ba2sakal)\
**Post date:** [January 11, 2025, 10:17am UTC](https://community.stereolabs.com/t/zed-sdk-installation-fails-in-docker-on-jetpack-6-1-nvargus-daemon-error/7856/6 "2025-01-11T10:17:27Z")

</div>

@beniaminopozzan  
Yes, from the Docker container, if I don’t execute the launch file with `sudo` or use Docker as the `root` user, I can’t initialize the cameras either. I believe the issue is that the `zedx_daemon.service` runs as `root`, and the cameras can’t access it without the necessary permissions. I haven’t been able to get it working with an admin user either.

For my setup, I also don’t usually use a screen, but for testing and diagnosing problems, you’ll need to, as many issues can’t be resolved through SSH alone.

By the way, are you experiencing the same bad-quality image problem that I am?

---

<div class="post-metadata">

**Author:** ![beniaminopozzan](https://community.stereolabs.com/user_avatar/community.stereolabs.com/beniaminopozzan/32/3586_2.png) [@beniaminopozzan](https://community.stereolabs.com/u/beniaminopozzan)\
**Post date:** [January 11, 2025, 11:02am UTC](https://community.stereolabs.com/t/zed-sdk-installation-fails-in-docker-on-jetpack-6-1-nvargus-daemon-error/7856/7 "2025-01-11T11:02:30Z")

</div>

“glad” it is not an isolated issue then.

I don’t think that’s the entire reason though: I don’t need sudo if I run it outside docker.

No, the image quality is good, I’m using a single ZED X One GS

---

<div class="post-metadata">

**Author:** ![ba2sakal](https://community.stereolabs.com/user_avatar/community.stereolabs.com/ba2sakal/32/4031_2.png) [@ba2sakal](https://community.stereolabs.com/u/ba2sakal)\
**Post date:** [January 11, 2025, 12:35pm UTC](https://community.stereolabs.com/t/zed-sdk-installation-fails-in-docker-on-jetpack-6-1-nvargus-daemon-error/7856/8 "2025-01-11T12:35:41Z")

</div>

I believe it is due to Admin access capabilities. I use the container directly as root as I understand it shouldn’t create a problem.