# ZED SDK 3.4.0 Release Candidate

**URL:** <https://community.stereolabs.com/t/zed-sdk-3-4-0-release-candidate/58>\
**Category:** Announcement\
**Created:** [December 15, 2020, 9:33am UTC](https://community.stereolabs.com/t/zed-sdk-3-4-0-release-candidate/58 "2020-12-15T09:33:49Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![adujardin](https://community.stereolabs.com/user_avatar/community.stereolabs.com/adujardin/32/4125_2.png) [@adujardin](https://community.stereolabs.com/u/adujardin)\
**Post date:** [December 15, 2020, 9:33am UTC](https://community.stereolabs.com/t/zed-sdk-3-4-0-release-candidate/58/1 "2020-12-15T09:33:49Z")

</div>

We are pleased to announce the **ZED SDK 3.4.0 RC1** , a new Release Candidate version of the ZED SDK.

Please note that “RC” means that this release is not yet finalized and fully stable. This shouldn’t be used in production as the final QA is still in progress. If you notice a bug, feel free to report it on this topic, thanks!

Here are the release notes:

# Release notes

## SDK

### New Features

#### API

- Added depth map format (`MEASURE::DEPTH_U16_MM` and `MEASURE::DEPTH_U16_MM_RIGHT`) as unsigned short (`MAT_TYPE::U16_C1`) to store it in millimeters, useful for many integrations
- Added depth max range for Detection module using `ObjectDetectionParameters::max_range`
- Added skeletons keypoints confidence (`ObjectData::keypoint_confidence`)
- Added a way to import OpenCV calibration using `InitParameters::optional_opencv_calibration_file`
- Added `Camera::updateSelfCalibration()` function to update the camera self calibration at runtime

#### Tools

- Added an offline mode for SVOs in ZEDfu to better handle positional tracking loop closures
- Calibration Tool can now be used with a ZED2
- Added a calibration procedure for magnetometer in Sensors Viewer

### Bug Fixes

- Fixed the magnetometer data coordinate frame
- Fixed an issue with Tegra encoder limiting the number of calls to the recording module

### General Improvements

- Positional tracking with area memory performs faster and more accurate relocalization, leading to better global accuracy

* * *

The links are below :

# SDK Downloads

## Standard installer

#### CUDA 11.1

- [ZED SDK for Windows 10](https://download.stereolabs.com/zedsdk/3.4/cu111/win) 3.4.0 RC1
- [ZED SDK for Ubuntu 20](https://download.stereolabs.com/zedsdk/3.4/cu111/ubuntu20) 3.4.0 RC1
- [ZED SDK for Ubuntu 18](https://download.stereolabs.com/zedsdk/3.4/cu111/ubuntu18) 3.4.0 RC1
- [ZED SDK for Ubuntu 16](https://download.stereolabs.com/zedsdk/3.4/cu111/ubuntu16) 3.4.0 RC1

#### CUDA 11.0

- [ZED SDK for Windows 10](https://download.stereolabs.com/zedsdk/3.4/cu110/win) 3.4.0 RC1
- [ZED SDK for Ubuntu 20](https://download.stereolabs.com/zedsdk/3.4/cu110/ubuntu20) 3.4.0 RC1
- [ZED SDK for Ubuntu 18](https://download.stereolabs.com/zedsdk/3.4/cu110/ubuntu18) 3.4.0 RC1
- [ZED SDK for Ubuntu 16](https://download.stereolabs.com/zedsdk/3.4/cu110/ubuntu16) 3.4.0 RC1

#### CUDA 10.2

- [ZED SDK for Windows 10](https://download.stereolabs.com/zedsdk/3.4/cu102/win) 3.4.0 RC1
- [ZED SDK for Ubuntu 18](https://download.stereolabs.com/zedsdk/3.4/cu102/ubuntu18) 3.4.0 RC1
- [ZED SDK for Ubuntu 16](https://download.stereolabs.com/zedsdk/3.4/cu102/ubuntu16) 3.4.0 RC1

#### CUDA 10.0

- [ZED SDK for Windows 10](https://download.stereolabs.com/zedsdk/3.4/cu100/win) 3.4.0 RC1
- [ZED SDK for Ubuntu 18](https://download.stereolabs.com/zedsdk/3.4/cu100/ubuntu18) 3.4.0 RC1
- [ZED SDK for Ubuntu 16](https://download.stereolabs.com/zedsdk/3.4/cu100/ubuntu16) 3.4.0 RC1

#### NVIDIA Jetson

- [ZED SDK for Jetpack 4.4](https://download.stereolabs.com/zedsdk/3.4/jp44/jetsons) 3.4.0 RC1 (Jetson Nano, NX, TX2, Xavier, CUDA 10.2)
- [ZED SDK for Jetpack 4.3](https://download.stereolabs.com/zedsdk/3.4/jp43/jetsons) 3.4.0 RC1 (Jetson Nano, TX2, Xavier, CUDA 10)

## Full installer

#### CUDA 11.1

- [ZED SDK Full installer for Ubuntu 20](https://download.stereolabs.com/zedsdk/3.4/cu111/ubuntu20_full) 3.4.0 RC1
- [ZED SDK Full installer for Ubuntu 18](https://download.stereolabs.com/zedsdk/3.4/cu111/ubuntu18_full) 3.4.0 RC1
- [ZED SDK Full installer for Ubuntu 16](https://download.stereolabs.com/zedsdk/3.4/cu111/ubuntu16_full) 3.4.0 RC1

#### CUDA 11.0

- [ZED SDK Full installer for Ubuntu 20](https://download.stereolabs.com/zedsdk/3.4/cu110/ubuntu20_full) 3.4.0 RC1
- [ZED SDK Full installer for Ubuntu 18](https://download.stereolabs.com/zedsdk/3.4/cu110/ubuntu18_full) 3.4.0 RC1
- [ZED SDK Full installer for Ubuntu 16](https://download.stereolabs.com/zedsdk/3.4/cu110/ubuntu16_full) 3.4.0 RC1

#### CUDA 10.2

- [ZED SDK Full installer for Ubuntu 18](https://download.stereolabs.com/zedsdk/3.4/cu102/ubuntu18_full) 3.4.0 RC1
- [ZED SDK Full installer for Ubuntu 16](https://download.stereolabs.com/zedsdk/3.4/cu102/ubuntu16_full) 3.4.0 RC1

#### CUDA 10.0

- [ZED SDK Full installer for Ubuntu 18](https://download.stereolabs.com/zedsdk/3.4/cu100/ubuntu18_full) 3.4.0 RC1
- [ZED SDK Full installer for Ubuntu 16](https://download.stereolabs.com/zedsdk/3.4/cu100/ubuntu16_full) 3.4.0 RC1

#### NVIDIA Jetson

- [ZED SDK Full installer for Jetpack 4.3](https://download.stereolabs.com/zedsdk/3.4/jp43/jetsons_full) 3.4.0 RC1 (Jetson Nano, TX2, Xavier, CUDA 10)