# ZED ROS2 wrapper: restarting one camera changes FPS of all cameras on Jetson

**URL:** <https://community.stereolabs.com/t/zed-ros2-wrapper-restarting-one-camera-changes-fps-of-all-cameras-on-jetson/11284>\
**Category:** Software\
**Tags:** jetson, ros2\
**Created:** [May 8, 2026, 12:46pm UTC](https://community.stereolabs.com/t/zed-ros2-wrapper-restarting-one-camera-changes-fps-of-all-cameras-on-jetson/11284 "2026-05-08T12:46:55Z")\
**Posts on this page:** 3\
**Page:** 1

<div class="post-metadata">

**Author:** ![vietlh](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/v/7ba0ec/32.png) [@vietlh](https://community.stereolabs.com/u/vietlh)\
**Post date:** [May 8, 2026, 12:46pm UTC](https://community.stereolabs.com/t/zed-ros2-wrapper-restarting-one-camera-changes-fps-of-all-cameras-on-jetson/11284/1 "2026-05-08T12:46:55Z")

</div>

Hi,

I have problem when using zed\_ros2\_wrapper with 3 zed x mini camera.

Environment:

- Jetson Orin AGX

- ZED link duo with 1.4.1 driver

- ROS2

- zed-ros2-wrapper run in docker with zedsdk 5.2.3

- Multiple ZED cameras

- Each camera runs with a separate `ros2 launch` command in separate `ros2 container` with separate config file

- Each camera uses its own ROS2 launch process

Issue:

When I restart one camera with a lower FPS configuration, the FPS of the other running cameras also decreases automatically.

Example:

- Camera A: 30 FPS

- Camera B: 30 FPS

- Camera C: 30 FPS

If I restart Camera C with 15 FPS:

- Camera A also drops close to 15 FPS

- Camera B also drops close to 15 FPS

Questions:

1. Does the ZED SDK synchronize FPS globally across cameras on Jetson?

2. Could this be related to USB bandwidth renegotiation or shared GPU/CUDA resources?

3. Is there a recommended way to isolate FPS/resource scheduling between multiple ZED cameras?

4. Are there known limitations for multi-camera setups with separate configs on Jetson platforms?

Thank you so much

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [May 8, 2026, 2:49pm UTC](https://community.stereolabs.com/t/zed-ros2-wrapper-restarting-one-camera-changes-fps-of-all-cameras-on-jetson/11284/2 "2026-05-08T14:49:47Z")

</div>

Hi @vietlh  
In a multicamera setup, the cameras of the same block share the same frame rate.  
Read more here:

> **[Multi-camera configurations - ZED Link Duo on AGX Orin - Stereolabs](https://www.stereolabs.com/docs/embedded/zed-link/dual-jetson-orin-agx-devkit-setup#multi-camera-configurations)**
>
> This tutorial will help you set up the ZED Link Duo GMSL2 capture card, and use the Stereolabs GMSL2 cameras with the NVIDIA® Jetson™ AGX Orin Developer Kit.

If you want to run a node with a different rate, you can:

- set the same value of the parameter [general.grab\_frame\_rate](https://github.com/stereolabs/zed-ros2-wrapper/blob/master/zed_wrapper/config/zedxm.yaml#L10) in all the node
- set a specific value of [general.grab\_compute\_capping\_fps](https://github.com/stereolabs/zed-ros2-wrapper/blob/master/zed_wrapper/config/common_stereo.yaml#L31) for each single node that must have a frame rate lower than the grab rate

You can also dynamically change the publishing rate of the topics.

I recommend you read this section of the documentation for all the details:

> **[Node Frequency Tuning - Stereolabs](https://www.stereolabs.com/docs/ros2/frequency-tuning)**
>
> 📌 Note: This guide applies only to the stereolabs::ZedCamera component for stereo cameras. The stereolabs::ZedCameraOne component for monocular cameras does not provide the behaviors described in this …

---

<div class="post-metadata">

**Author:** ![vietlh](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/v/7ba0ec/32.png) [@vietlh](https://community.stereolabs.com/u/vietlh)\
**Post date:** [May 9, 2026, 3:15am UTC](https://community.stereolabs.com/t/zed-ros2-wrapper-restarting-one-camera-changes-fps-of-all-cameras-on-jetson/11284/3 "2026-05-09T03:15:54Z")

</div>

Thank you so much, @Myzhar

It is very helpful for me.