# zed-ros2-wrapper build errors for Jetson Orin with ROS Foxy

**URL:** <https://community.stereolabs.com/t/zed-ros2-wrapper-build-errors-for-jetson-orin-with-ros-foxy/9635>\
**Category:** ROS2\
**Tags:** sdk, ros, jetson\
**Created:** [August 7, 2025, 7:42am UTC](https://community.stereolabs.com/t/zed-ros2-wrapper-build-errors-for-jetson-orin-with-ros-foxy/9635 "2025-08-07T07:42:50Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![SaanviM](https://community.stereolabs.com/user_avatar/community.stereolabs.com/saanvim/32/4852_2.png) [@SaanviM](https://community.stereolabs.com/u/SaanviM)\
**Post date:** [August 7, 2025, 7:42am UTC](https://community.stereolabs.com/t/zed-ros2-wrapper-build-errors-for-jetson-orin-with-ros-foxy/9635/1 "2025-08-07T07:42:50Z")

</div>

### Description

I have a Jetson Orin that has CUDA 11 and Foxy running. Since its CUDA 11, i installed the SDK version as below

[ZED SDK for JetPack 5.1.1 (L4T 35.3)](https://download.stereolabs.com/zedsdk/5.0/l4t35.3/jetsons) 5.0 (Jetson Xavier, Orin AGX/NX/Nano, CUDA 11.4)

I have the master branch checked out for the zed2-ros-wrapper. When i build the package as per the steps mentioned here [https://github.com/stereolabs/zed-ros2-wrapper/](https://github.com/stereolabs/zed-ros2-wrapper/) , the C++ code throws errors as below

```auto
zed_ws/src/zed-ros2-wrapper/zed_components/src/zed_camera/src/zed_camera_one_component.cpp: In member function ‘void stereolabs::ZedCameraOne::init()’:
zed_ws/src/zed-ros2-wrapper/zed_components/src/zed_camera/src/zed_camera_one_component.cpp:680:33: error: ‘using element_type = class rclcpp::contexts::DefaultContext’ {aka ‘class rclcpp::contexts::DefaultContext’} has no member named ‘add_pre_shutdown_callback’; did you mean ‘get_on_shutdown_callbacks’?
  680 | get_global_default_context()->add_pre_shutdown_callback(
      | ^ ~~~~~~~~~~~~~~~~~~~~~~~~
      | get_on_shutdown_callbacks

zed_ws/src/zed-ros2-wrapper/zed_components/src/zed_camera/src/zed_camera_component_main.cpp: In member function ‘void stereolabs::ZedCamera::initPublishers()’:
zed_ws/src/zed-ros2-wrapper/zed_components/src/zed_camera/src/zed_camera_component_main.cpp:1995:32: error: ‘ClockQoS’ is not a member of ‘rclcpp’; did you mean ‘Clock’?
 1995 | auto clock_qos = rclcpp::ClockQoS();
ed_ws/src/zed-ros2-wrapper/zed_components/src/zed_camera/src/zed_camera_component_main.cpp:1996:37: error: ‘rclcpp::ReliabilityPolicy’ has not been declared
 1996 | clock_qos.reliability(rclcpp::ReliabilityPolicy::Reliable); // REQUIRED

```

Any suggestions on an alternate SDK version or how to get the package installed for Foxy?

### Steps to Reproduce

1. Install [ZED SDK for JetPack 5.1.1 (L4T 35.3)](https://download.stereolabs.com/zedsdk/5.0/l4t35.3/jetsons) 5.0 (Jetson Xavier, Orin AGX/NX/Nano, CUDA 11.4)  
2.Checkout zed-ros2-wrapper and zed-ros2-interfaces

2. Follow build steps as mentioned in [https://github.com/stereolabs/zed-ros2-wrapper/](https://github.com/stereolabs/zed-ros2-wrapper/)  
…

### Expected Result

Package is installed successfully

### Actual Result

Failed \<\<\< zed\_components [35.6s, exited with code 2]

Summary: 1 package finished [1min 17s]  
1 package failed: zed\_components  
1 package had stderr output: zed\_components

### Environment

```auto
OS: Ubuntu 22
GPU : Nvidia Jetson Orin
SDK version : [ZED SDK for JetPack 5.1.1 (L4T 35.3)](https://download.stereolabs.com/zedsdk/5.0/l4t35.3/jetsons) 5.0 (Jetson Xavier, Orin AGX/NX/Nano, CUDA 11.4)
ROS: Foxy

```

---

<div class="post-metadata">

**Author:** ![mattrouss](https://community.stereolabs.com/user_avatar/community.stereolabs.com/mattrouss/32/2452_2.png) [@mattrouss](https://community.stereolabs.com/u/mattrouss)\
**Post date:** [August 11, 2025, 5:06pm UTC](https://community.stereolabs.com/t/zed-ros2-wrapper-build-errors-for-jetson-orin-with-ros-foxy/9635/2 "2025-08-11T17:06:28Z")

</div>

Hi @SaanviM,

This looks like a Foxy compatibility issue, this should not happen, I will log this internally so we can look into this.

If possible, you can compile the wrapper for Humble or Jazzy in the meantime