# Zed robot integration and visualising using the camera in isaac sim

**URL:** <https://community.stereolabs.com/t/zed-robot-integration-and-visualising-using-the-camera-in-isaac-sim/7818>\
**Category:** ROS2\
**Created:** [January 3, 2025, 2:49pm UTC](https://community.stereolabs.com/t/zed-robot-integration-and-visualising-using-the-camera-in-isaac-sim/7818 "2025-01-03T14:49:44Z")\
**Posts on this page:** 8\
**Page:** 1

<div class="post-metadata">

**Author:** ![Anirudhgudi](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/54ee81/32.png) [@Anirudhgudi](https://community.stereolabs.com/u/Anirudhgudi)\
**Post date:** [January 3, 2025, 2:49pm UTC](https://community.stereolabs.com/t/zed-robot-integration-and-visualising-using-the-camera-in-isaac-sim/7818/1 "2025-01-03T14:49:44Z")

</div>

I have integrated zedx camera into robot using the documentation provided in this link [ZED integration on a Robot - Stereolabs](https://www.stereolabs.com/docs/ros2/140_ros2-robot-integration#visualize-the-model)

When i try to import the urdf into isaac sim and try to stream the data using that camera, i am only getting a top plane view from the origin of the enviroment the camera is in,. The camera view stays there even if the robot moves.  
I am adding the zed\_camera\_link into the zed camera streamer in the camera prim while building action graph.

 ![Screenshot from 2025-01-03 20-17-54](https://community.stereolabs.com/uploads/default/original/2X/7/79676cfff08e28b08ea44a12abc5e65d1dfc7fa9.png)

---

<div class="post-metadata">

**Author:** ![mattrouss](https://community.stereolabs.com/user_avatar/community.stereolabs.com/mattrouss/32/2452_2.png) [@mattrouss](https://community.stereolabs.com/u/mattrouss)\
**Post date:** [January 6, 2025, 1:32pm UTC](https://community.stereolabs.com/t/zed-robot-integration-and-visualising-using-the-camera-in-isaac-sim/7818/2 "2025-01-06T13:32:38Z")

</div>

Hi @Anirudhgudi,

Once you’ve imported the URDF into Isaac Sim, have you included the ZED Camera extension using this guide in our documentation? [Setting up ZED Camera in Isaac Sim - Stereolabs](https://www.stereolabs.com/docs/isaac-sim/setting_up_zed_isaac_sim)

Are you able to stream the ZED camera data to our other tools such as ZED\_Explorer or ZED\_Depth\_Viewer?

---

<div class="post-metadata">

**Author:** ![Anirudhgudi](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/54ee81/32.png) [@Anirudhgudi](https://community.stereolabs.com/u/Anirudhgudi)\
**Post date:** [January 16, 2025, 6:58am UTC](https://community.stereolabs.com/t/zed-robot-integration-and-visualising-using-the-camera-in-isaac-sim/7818/3 "2025-01-16T06:58:35Z")

</div>

Hi sorry for the delay… yes i can stream the data… the image is the same as i attached in my previous post. Once i do the integration of robot in the urdf as per documentation, the cameras get added with individual prims and its visible this way in isaac sim ( image ). which prim should i add in the zed streamer node in omnigraph?

 ![image](https://community.stereolabs.com/uploads/default/original/2X/9/9e1d50c87c9e2be3d0e9e3b319d8a20023cfbac0.png)

---

<div class="post-metadata">

**Author:** ![mattrouss](https://community.stereolabs.com/user_avatar/community.stereolabs.com/mattrouss/32/2452_2.png) [@mattrouss](https://community.stereolabs.com/u/mattrouss)\
**Post date:** [January 16, 2025, 9:29am UTC](https://community.stereolabs.com/t/zed-robot-integration-and-visualising-using-the-camera-in-isaac-sim/7818/4 "2025-01-16T09:29:35Z")

</div>

Hi @Anirudhgudi,

Currently, we do not support importing the zed camera directly from an urdf file, the ZED X model still requires to be imported as described here: [Setting up ZED Camera in Isaac Sim - Stereolabs](https://www.stereolabs.com/docs/isaac-sim/setting_up_zed_isaac_sim#add-the-model-to-the-stage)

I would recommend placing the ZED\_X USD model under the `zed_back_camera_link` prim, and then following the tutorial to add the streamer node.

---

<div class="post-metadata">

**Author:** ![Anirudhgudi](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/54ee81/32.png) [@Anirudhgudi](https://community.stereolabs.com/u/Anirudhgudi)\
**Post date:** [January 16, 2025, 9:56am UTC](https://community.stereolabs.com/t/zed-robot-integration-and-visualising-using-the-camera-in-isaac-sim/7818/5 "2025-01-16T09:56:32Z")

</div>

Got it. Thank you for the support!

---

<div class="post-metadata">

**Author:** ![Anirudhgudi](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/54ee81/32.png) [@Anirudhgudi](https://community.stereolabs.com/u/Anirudhgudi)\
**Post date:** [January 20, 2025, 9:48am UTC](https://community.stereolabs.com/t/zed-robot-integration-and-visualising-using-the-camera-in-isaac-sim/7818/6 "2025-01-20T09:48:02Z")

</div>

Hi @mattrouss ,  
I configured both of the zed cameras in my isaac sim using the zed camera extension using two different action graphs. I have specified two different serial numbers in the zed camera streamer but i am not able to stream data from even one camera. As soon as hit the play sim button, i get this error “2025-01-20 09:43:55 [Error] [sl.sensor.camera.ogn.nodes.SlCameraStreamer] Failed to initialize the ZED SDK streamer with serial number 40976320.”  
Any suggestions on how to configure two cameras in isaac sim?

---

<div class="post-metadata">

**Author:** ![Anirudhgudi](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/54ee81/32.png) [@Anirudhgudi](https://community.stereolabs.com/u/Anirudhgudi)\
**Post date:** [January 20, 2025, 11:01am UTC](https://community.stereolabs.com/t/zed-robot-integration-and-visualising-using-the-camera-in-isaac-sim/7818/7 "2025-01-20T11:01:30Z")

</div>

Hi @mattrouss ,

I was able to rectify the error by keeping the serial number same and different sim ports in the zed cam streamer action graph.

Thank you!

---

<div class="post-metadata">

**Author:** ![robinvetsch](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/r/47e85d/32.png) [@robinvetsch](https://community.stereolabs.com/u/robinvetsch)\
**Post date:** [November 18, 2025, 7:24am UTC](https://community.stereolabs.com/t/zed-robot-integration-and-visualising-using-the-camera-in-isaac-sim/7818/8 "2025-11-18T07:24:22Z")

</div>

Hi @Anirudhgudi

I have a similar issue… We have in total four ZED X cameras. When creating one ActionGraph for only one camera, it works and I can see the camera stream on port 30000.

When creating a separate ActionGraph for each of the other cameras, with a different serial number (one of the proposed number) and a different streaming port (e.g. 30002, 30004, 30006), I can’t see the stream of the others in the ZED\_Depth\_Viewer.

I’m using Isaac Sim 4.5 and ZED SDK 4.2.5.

How did you manage to see the different cameras in the ZED viewer?

> Many thanks for your help.
> 
> [2025-11-18 07:24:29 UTC][ZED][INFO] Logging level INFO  
> [2025-11-18 07:24:37 UTC][ZED][INFO] Logging level INFO  
> [Streaming] Warning : receiving port 30000 is not available (already used)… switching to port 30002. Retrying…  
> [Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.  
> [Streaming] Metadata timeout. the size is equal to 196 instead of 21960. Skipping.  
> [Streaming] No backward compatibility required.  
> [2025-11-18 07:24:38 UTC][ZED][INFO] [Init] Depth mode: ULTRA  
> [2025-11-18 07:24:38 UTC][ZED][INFO] [Init] Serial Number: S/N 40976320  
> [2025-11-18 07:24:38 UTC][ZED][WARNING] Simulated ZED camera used.  
> [2025-11-18 07:24:38 UTC][ZED][WARNING] [Init] Invalid calibration file. On Linux, call export LC\_ALL=“C” and restart your application.  
> [2025-11-18 07:24:38 UTC][ZED][WARNING] Self Calibration Disabled.  
> [Streaming] Metadata timeout. the size is equal to -1 instead of 21960. Skipping.  
> [2025-11-18 07:24:50 UTC][ZED][INFO] Logging level INFO  
> [Streaming] Warning: Failed to retrieve camera settings from sender  
> [Streaming] Error: Stream Opening returned TIMEOUT (350)  
> [Streaming] Metadata timeout. the size is equal to -1 instead of 21960. Skipping.  
> [2025-11-18 07:25:01 UTC][ZED][WARNING] FAILURE in sl::ERROR\_CODE sl:📷:open(sl::InitParameters)