# ZED Mini IMU calibration lost - Reason?

**URL:** <https://community.stereolabs.com/t/zed-mini-imu-calibration-lost-reason/7674>\
**Category:** ZED Mini\
**Tags:** imu, unity\
**Created:** [December 11, 2024, 8:19am UTC](https://community.stereolabs.com/t/zed-mini-imu-calibration-lost-reason/7674 "2024-12-11T08:19:43Z")\
**Posts on this page:** 1\
**Showing post:** 8

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [October 8, 2026, 1:43pm UTC](https://community.stereolabs.com/t/zed-mini-imu-calibration-lost-reason/7674/8 "2026-10-08T13:43:30Z")

</div>

> [@marti](#):
>
> Not sure which procedure you mean…

The one linked in my first reply:

> [@Something's wrong with my Zed Mini IMU](https://community.stereolabs.com/t/somethings-wrong-with-my-zed-mini-imu/206/3):
>
> When you see the camera “spinning” in the “ZED Sensor Viewer” tool, that means that for some reason it lost the IMU calibration parameters. You can easily restore the IMU calibration running the “ZED Calibration” tool from the command line, adding the flag --cimu or --calib\_imu. Before running the calibration process please be sure that the camera is completely steady and placed on a horizontal surface. The re-calibration process is fast and fully automated, you can test if it worked correctl…

> [@marti](#):
>
> The problem with the IMU recalibration is that the systems do not have a monitor / mouse / keyboard attached. They are remotely controlled via a web interface.

You need at least an ssh session to run it.

Have you tested a recent version of the ZED SDK? Is the problem still present with v5.5?

---

_[View the full topic](https://community.stereolabs.com/t/zed-mini-imu-calibration-lost-reason/7674)._