#  ZED Link Duo camera limit clarification - Do ZED X Minis count as 2 cameras each?

**URL:** <https://community.stereolabs.com/t/zed-link-duo-camera-limit-clarification-do-zed-x-minis-count-as-2-cameras-each/10833>\
**Category:** ZED X\
**Tags:** sdk, jetson\
**Created:** [February 19, 2026, 3:18pm UTC](https://community.stereolabs.com/t/zed-link-duo-camera-limit-clarification-do-zed-x-minis-count-as-2-cameras-each/10833 "2026-02-19T15:18:52Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![marcel123](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/m/4491bb/32.png) [@marcel123](https://community.stereolabs.com/u/marcel123)\
**Post date:** [February 19, 2026, 3:18pm UTC](https://community.stereolabs.com/t/zed-link-duo-camera-limit-clarification-do-zed-x-minis-count-as-2-cameras-each/10833/1 "2026-02-19T15:18:52Z")

</div>

Hello,

I have been testing a setup with a Jetson Orin Nano Dev Kit, ZED Link Duo capture card, and a mix of ZED X Mini and ZED X One S cameras (not the 4K variant).

The [datasheet](https://www.stereolabs.com/assets/datasheets/zed-link-capture-card-duo-datasheet.pdf) states that the Duo capture card “ **supports up to 4 ZED X GS / ZED X Mini GS / ZED X One GS and up to 2 ZED One 4K** ”. However, during my testing I encountered unexpected behavior that suggests ZED X Mini cameras may count as **two cameras** toward this limit rather than one.

**my setup:**

- ZED X Mini cameras

- ZED X One S cameras

- x1 ZED Link Duo capture card (zed-link-duo driver v1.4.0)

- x1 Jetson Orin Nano Dev Kit (running Jetpack 6.1 L4T36.4)

- x1 GMSL2 Fakra 1-to-4 M-F Cable

- x2 MIPI cables connecting Jetson to capture card

- Using ZED SDK 4.2.5 with Python (pyzed)

**I observed the following:**

- With only x2 ZED X Mini’s connected, I can successfully open all camera streams (L/R of each)

- With only x4 ZED X One S cameras connected, I can successfully open all streams.

- With x2 ZED X Mini’s and x2 ZED X One S cameras connected, I get _CAMERA\_NOT\_DETECTED_ for the monocular cameras, and the X Mini will _sometimes_ work but usually not.

**My main question is does each ZED X Mini count as 2 cameras toward the 4-camera limit of the duo capture card since it’s stereo?** Are there any ways around this that allow us to consider a ZED X Mini as a single camera and capture both feeds? My goal is to have multiple camera streams running as ROS topics at once but I want to be clear on the limitations of the duo capture card.

Thank you!

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [February 19, 2026, 3:38pm UTC](https://community.stereolabs.com/t/zed-link-duo-camera-limit-clarification-do-zed-x-minis-count-as-2-cameras-each/10833/2 "2026-02-19T15:38:48Z")

</div>

Hi @marcel123  
Welcome to the [Stereolabs](https://www.stereolabs.com/) community.

> [@marcel123](#):
>
> **My main question is does each ZED X Mini count as 2 cameras toward the 4-camera limit of the duo capture card since it’s stereo?**

No, it doesn’t. Each Stereo camera counts as a single connected device.

I recommend you check the supported multi-camera combination and be sure that you connected the devices in the correct way:

> **[Multi-camera configurations - ZED Link Duo on Orin Nano - Stereolabs](https://www.stereolabs.com/docs/embedded/zed-link/dual-jetson-orin-nano-devkit-setup#multi-camera-configurations)**
>
> This tutorial will help you set up the ZED Link Duo GMSL2 capture card, and use the Stereolabs GMSL2 cameras with the NVIDIA® Jetson™ Orin Nano Developer Kits.