# Zed Gstreamer Local network UDP

**URL:** <https://community.stereolabs.com/t/zed-gstreamer-local-network-udp/9597>\
**Category:** Software\
**Tags:** zed-gstreamer\
**Created:** [August 4, 2025, 12:32pm UTC](https://community.stereolabs.com/t/zed-gstreamer-local-network-udp/9597 "2025-08-04T12:32:17Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![hatoktas](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/h/ba9def/32.png) [@hatoktas](https://community.stereolabs.com/u/hatoktas)\
**Post date:** [August 4, 2025, 12:32pm UTC](https://community.stereolabs.com/t/zed-gstreamer-local-network-udp/9597/1 "2025-08-04T12:32:17Z")

</div>

```auto
gst-launch-1.0 zedsrc ! timeoverlay ! tee name=split has-chain=true ! \
 queue ! autovideoconvert ! fpsdisplaysink \
 split. ! queue max-size-time=0 max-size-bytes=0 max-size-buffers=0 ! autovideoconvert ! \
 x264enc byte-stream=true tune=zerolatency speed-preset=ultrafast bitrate=3000 ! \
 h264parse ! rtph264pay config-interval=-1 pt=96 ! queue ! \
 udpsink clients=192.168.1.169:5000 max-bitrate=3000000 sync=false async=false

```

I can’t use this command with … zedsrc camera-resolution=3 camera-fps=60 stream-type=1 … sink.

It says failed to open camera , INVALID RESOLUTION. Is there anything for publishing 1920x1200 stream in 60 fps.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [August 4, 2025, 12:41pm UTC](https://community.stereolabs.com/t/zed-gstreamer-local-network-udp/9597/2 "2025-08-04T12:41:09Z")

</div>

Hi @hatoktas  
What camera model are you using?

`camera-resolution=3 camera-fps=60` is for HD720, you must use `camera-resolution=2 camera-fps=60`

```auto
  camera-resolution : Camera Resolution
                        flags: readable, writable
                        Enum "GstZedSrcRes" Default: 6, "Default value for the camera model"
                           (0): HD2K (USB3) - 2208x1242
                           (1): HD1080 (USB3/GMSL2) - 1920x1080
                           (2): HD1200 (GMSL2) - 1920x1200
                           (3): HD720 (USB3) - 1280x720
                           (4): SVGA (GMSL2) - 960x600
                           (5): VGA (USB3) - 672x376
                           (6): Default value for the camera model - Automatic

```

---

<div class="post-metadata">

**Author:** ![hatoktas](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/h/ba9def/32.png) [@hatoktas](https://community.stereolabs.com/u/hatoktas)\
**Post date:** [August 4, 2025, 5:59pm UTC](https://community.stereolabs.com/t/zed-gstreamer-local-network-udp/9597/3 "2025-08-04T17:59:56Z")

</div>

Hi Walter,

```auto
  camera-resolution : Camera Resolution
                        flags: readable, writable
                        Enum "GstZedsrcResolution" Default: 7, "Default value for the camera model"
                           (1): HD2K (USB3) - 2208x1242
                           (3): HD1200 (GMSL2) - 1920x1200
                           (2): HD1080 (USB3/GMSL2) - 1920x1080
                           (4): HD720 (USB3) - 1280x720
                           (5): SVGA (GMSL2) - 960x600
                           (6): VGA (USB3) - 672x376
                           (7): Default value for the camera model - Automatic

```

[GStreamer - ZED Camera Source - Stereolabs](https://www.stereolabs.com/docs/gstreamer/zed-camera-source#h264-streaming-over-udp-on-the-local-network). In this link, it is different. So I tried with camera-resolution=2 it worked but fps is to low. 2 fps. I wanted 60 fps. I think there is something wrong.

And also it is utilizing CPU I guess, is there any deep stream support for GPU utilization for encoding part in Gstreamer pipeline…

Camera model Zed X , zed box mini orin nx 16

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [August 5, 2025, 8:21am UTC](https://community.stereolabs.com/t/zed-gstreamer-local-network-udp/9597/4 "2025-08-05T08:21:52Z")

</div>

> [@hatoktas](#):
>
> [GStreamer - ZED Camera Source - Stereolabs](https://www.stereolabs.com/docs/gstreamer/zed-camera-source#h264-streaming-over-udp-on-the-local-network). In this link, it is different. So I tried with camera-resolution=2 it worked but fps is to low. 2 fps. I wanted 60 fps. I think there is something wrong.

Thank you for reporting. I’ve just updated the documentation with the new information from the command `gst-inspect-1.0 zedsrc` that is always the best way to check the allowed values for each property.

> [@hatoktas](#):
>
> And also it is utilizing CPU I guess, is there any deep stream support for GPU utilization for encoding part in Gstreamer pipeline…

You must create a pipeline that sends the data to the GPU memory.  
We have no ready examples for this.