# Zed cameras withdrawing power

**URL:** <https://community.stereolabs.com/t/zed-cameras-withdrawing-power/11166>\
**Category:** ZED X\
**Created:** [April 10, 2026, 3:19pm UTC](https://community.stereolabs.com/t/zed-cameras-withdrawing-power/11166 "2026-04-10T15:19:15Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![Hussein](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/h/9de053/32.png) [@Hussein](https://community.stereolabs.com/u/Hussein)\
**Post date:** [April 10, 2026, 3:19pm UTC](https://community.stereolabs.com/t/zed-cameras-withdrawing-power/11166/1 "2026-04-10T15:19:15Z")

</div>

Hi [Stereolabs](https://www.stereolabs.com/) community,

We are experiencing an issue with our ZED Box Mini where GPIO\_12 (line offset 85, pin #04) remains HIGH after system shutdown, but only when GMSL2 cameras are connected.

Setup:

- ZED Box Mini.

- One ZED X and one ZED X Mini connected via GMSL2 ports.

- GPIO\_11 (line 106) configured as input with pull-up resistor ,used as an ignition-off signal.

- GPIO\_12 (line 85) configured as output with pull-down resistor ,used to control a relay.

- libgpiod C++ application running as a systemd service

Expected behavior:

- On boot: GPIO\_12 is driven HIGH → relay closes

- On shutdown (GPIO\_11 goes LOW for 10 seconds) → system powers off → GPIO\_12 turns low (by default)→ relay releases.

Actual behavior:

- Without cameras connected: Works perfectly. GPIO\_12 goes LOW after shutdown, relay releases, power draw drops to 0.

- With cameras connected: After shutdown, GPIO\_12 remains HIGH. Multimeter confirms 2.6V on the pin. The relay does not release. The system draws approximately 100mA from the power supply even after shutdown despite having the blue LEDs on the Zed Box turned off.

What I’ve tried:

1. Using ‘systemctl poweroff’ instead of ‘shutdown -h now’

2. Using ‘systemctl --force poweroff’

3. Stopping the cameras before shutdown (sl.close()) .

4. Stopping zed\_x\_daemon.service and unloading the max9296 driver (modprobe -r) before shutdown

None of these resolved the issue. The 100mA draw and GPIO\_12 staying HIGH only occurs when cameras are physically connected to the GMSL2 ports.

---

<div class="post-metadata">

**Author:** ![Aldric](https://community.stereolabs.com/user_avatar/community.stereolabs.com/aldric/32/3863_2.png) [@Aldric](https://community.stereolabs.com/u/Aldric)\
**Post date:** [April 21, 2026, 12:48pm UTC](https://community.stereolabs.com/t/zed-cameras-withdrawing-power/11166/2 "2026-04-21T12:48:19Z")

</div>

Hi,

We’ll be reproducing this behavior internally to see if a solution can be applied

Best,

Aldric

[Stereolabs](https://www.stereolabs.com/) Support