# ZED Cameras w/o Lens not Working

**URL:** <https://community.stereolabs.com/t/zed-cameras-w-o-lens-not-working/11647>\
**Category:** ZED X\
**Created:** [August 21, 2026, 2:46pm UTC](https://community.stereolabs.com/t/zed-cameras-w-o-lens-not-working/11647 "2026-08-21T14:46:10Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![adeep.das](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/13edae/32.png) [@adeep.das](https://community.stereolabs.com/u/adeep.das)\
**Post date:** [August 21, 2026, 2:46pm UTC](https://community.stereolabs.com/t/zed-cameras-w-o-lens-not-working/11647/1 "2026-08-21T14:46:10Z")

</div>

I recently bought a ZED XOne S Camera without Lens and a ZED XOne GS Camera without Lens. I first mounted on a lens on the camera. Then, I wanted to preview it on ZED Studio but it wouldn’t work because of invalid calibration file. Then I tried to use your ZED OpenCV Calibration tool but then the GUI wouldn’t pop up. I have attached the things I was seeing, but overall I was hoping to get help regarding how to see a preview of my camera view. Thanks!

Terminal Output after trying to run OpenCV Calibration:

./zed\_mono\_calibration  
\*\*\* Monocular Camera Calibration Tool (ZED X One) \*\*\*

The calibration process requires a checkerboard of known characteristics.

- Expected checkerboard features:

- Lens distortion model: Radial-Tangential

- Camera Model: Unknown

- Camera Serial Number: 0

- Camera Resolution: 0 x 0

- Using prior calibration: No

DMesg Logs from ZED Diagnostic:

Created: Wed Aug 12 2026

###########################################  
############ ZED SDK VERSION #############  
###########################################

ZED SDK Version (Diag): 5.2.3  
ZED SDK Version (RT): 5.2.3

###########################################  
############ Linux Uname #############  
###########################################

Linux GTW-ONX1-C1GSIAXP 5.15.148-tegra #1 SMP PREEMPT Mon Jun 16 08:24:48 PDT 2025 aarch64 aarch64 aarch64 GNU/Linux

###########################################  
############ DMESG [ZEDX] LOG #############  
###########################################

[4.032789] i2c i2c-9: of\_i2c: modalias failure on /bus@0/i2c@3180000/tca9546@70/i2c@0/zedxone\_uhd\_ser@44  
[4.032803] i2c i2c-9: Failed to create I2C device for /bus@0/i2c@3180000/tca9546@70/i2c@0/zedxone\_uhd\_ser@44  
[4.032810] i2c i2c-9: of\_i2c: modalias failure on /bus@0/i2c@3180000/tca9546@70/i2c@0/zedxone\_uhd@1a  
[4.032814] i2c i2c-9: Failed to create I2C device for /bus@0/i2c@3180000/tca9546@70/i2c@0/zedxone\_uhd@1a  
[5715.637328] zedx 9-0010: Driver Version : v1.4.1  
[5715.637628] zedx 9-0010: tegracam sensor driver:video4\_v2.0.6  
[5715.966326] tegra-camrtc-capture-vi tegra-capture-vi: subdev zedx 9-0010 bound  
[5716.025774] zedx 9-0010: ZED-X sensor initialisation done  
[5716.025786] zedx 9-0010: zedx\_probe: Serial Number : 303579811  
[5716.031162] zedx 9-0010: zedx\_probe: success

###########################################  
############ DMESG [MAX9x] LOG #############  
###########################################

[17.660211] sl\_max96712 9-0029: Driver Version : v1.4.1  
[17.775795] sl\_max96712 9-0029: slow\_reset\_Dser: Setup Deser as 2 lanes output  
[19.498767] sl\_max96712 9-0029: sl\_max96712\_gmsl\_pipeline\_setup: Active GMSL ports : 0  
[19.767202] sl\_max96712 9-0029: sl\_max96712\_gmsl\_pipeline\_setup: No camera connected to GMSL port 0  
[20.199163] sl\_max96712 9-0029: sl\_max96712\_gmsl\_pipeline\_setup: No camera connected to GMSL port 1  
[20.635130] sl\_max96712 9-0029: sl\_max96712\_gmsl\_pipeline\_setup: No camera connected to GMSL port 2  
[21.067113] sl\_max96712 9-0029: sl\_max96712\_gmsl\_pipeline\_setup: No camera connected to GMSL port 3  
[21.451111] sl\_max96712 9-0029: sl\_max96712\_probe: No Camera connected to this deserializer  
[21.451121] sl\_max96712 9-0029: sl\_max96712\_probe: success  
[5711.187302] sl\_max96712 9-0029: sl\_max96712\_remove: success  
[5711.215808] sl\_max96712 9-0029: Driver Version : v1.4.1  
[5711.334168] sl\_max96712 9-0029: slow\_reset\_Dser: Setup Deser as 2 lanes output  
[5712.731426] sl\_max96712 9-0029: sl\_max96712\_gmsl\_pipeline\_setup: Active GMSL ports : 1  
[5712.999829] sl\_max96712 9-0029: sl\_max96712\_gmsl\_pipeline\_setup: No camera connected to GMSL port 0  
[5713.427994] sl\_max96712 9-0029: sl\_max96712\_gmsl\_pipeline\_setup: No camera connected to GMSL port 1  
[5713.695860] sl\_max96712 9-0029: sl\_max96712\_gmsl\_pipeline\_setup: Camera connected to GMSL port 2  
[5714.727762] sl\_max96712 9-0029: sl\_max96712\_get\_camera\_model: zedonegs camera connected to this port  
[5714.742144] sl\_max96712 9-0029: sl\_max96712\_pipes\_setup: camera pipeline operational  
[5714.742153] sl\_max96712 9-0029: sl\_max96712\_gmsl\_pipeline\_setup: GMSL #2 : Link Camera zedonegs (id: 4) to port-index 0  
[5715.011744] sl\_max96712 9-0029: sl\_max96712\_gmsl\_pipeline\_setup: No camera connected to GMSL port 3  
[5715.387730] sl\_max96712 9-0029: sl\_max96712\_probe: success  
[5715.397511] sl\_max9295 9-0066: Driver Version : v1.4.1  
[5715.611304] sl\_max9295 9-0066: probe\_serializer: Serializer pipeline operational  
[5715.612970] sl\_max9295 9-0066: probe\_serializer: Serializer for zedonegs detect success

###########################################  
############ DMESG [PCA] LOG #############  
###########################################

[4.036149] pca954x 2-0070: registered 4 multiplexed busses for I2C switch pca9546

###########################################  
############ DMESG [DTS] LOG #############  
###########################################

###########################################  
############ DTB list original ###########  
###########################################

/boot/dtb/kernel\_tegra234-p3768-0000+p3767-0000-nv.dtb

###########################################  
############ DTB list SLabs ###########  
###########################################

board.py  
extlinux.py  
fio.py  
Headers  
Jetson  
Linux  
**pycache**  
Utils  
zlconfig

###########################################  
############ EXTlinux file ###########  
###########################################

TIMEOUT 30  
DEFAULT [Stereolabs](https://www.stereolabs.com/)

MENU TITLE L4T boot options

LABEL primary  
MENU LABEL primary kernel  
LINUX /boot/Image  
INITRD /boot/initrd  
APPEND ${cbootargs} root=PARTUUID=a33f7d34-756b-4668-b73e-38e9a9ff0400 rw rootwait rootfstype=ext4 mminit\_loglevel=4 console=ttyTCU0,115200 firmware\_class.path=/etc/firmware fbcon=map:0 video=efifb:off console=tty0

# When testing a custom kernel, it is recommended that you create a backup of

# the original kernel and add a new entry to this file so that the device can

# fallback to the original kernel. To do this:

# 

# 1, Make a backup of the original kernel

# sudo cp /boot/Image /boot/Image.backup

# 

# 2, Copy your custom kernel into /boot/Image

# 

# 3, Uncomment below menu setting lines for the original kernel

# 

# 4, Reboot

# LABEL backup

# MENU LABEL backup kernel

# LINUX /boot/Image.backup

# INITRD /boot/initrd

# APPEND ${cbootargs}

LABEL [Stereolabs](https://www.stereolabs.com/)  
MENU LABEL [Stereolabs](https://www.stereolabs.com/) kernel  
LINUX /boot/Image  
FDT /boot/dtb/kernel\_tegra234-p3768-0000+p3767-0000-nv.dtb  
INITRD /boot/initrd  
APPEND ${cbootargs} root=PARTUUID=a33f7d34-756b-4668-b73e-38e9a9ff0400 rw rootwait rootfstype=ext4 mminit\_loglevel=4 console=ttyTCU0,115200 firmware\_class.path=/etc/firmware fbcon=map:0 video=efifb:off console=tty0  
OVERLAYS /boot/tegra234-p3768-camera-zedbox-duo-sl-overlay.dtbo

###########################################  
############ Jetpack ###########  
###########################################

# R36 (release), REVISION: 4.4, GCID: 41062509, BOARD: generic, EABI: aarch64, DATE: Mon Jun 16 16:07:13 UTC 2025

# KERNEL\_VARIANT: oot

TARGET\_USERSPACE\_LIB\_DIR=nvidia  
TARGET\_USERSPACE\_LIB\_DIR\_PATH=usr/lib/aarch64-linux-gnu/nvidia

###########################################  
############ Dpkg list ###########  
###########################################

ii [stereolabs](https://www.stereolabs.com/)-zedbox-duo 1.4.1-LI-MAX96712-ZEDBOX-L4T36.4.0 arm64 NVIDIA Kernel DTB Modified Package by [Stereolabs](https://www.stereolabs.com/)

####################################  
############ Driver list ###########  
####################################

/usr/lib/modules/5.15.148-tegra/kernel/drivers/[stereolabs](https://www.stereolabs.com/)/max96712/sl\_max96712.ko==\> exists  
/usr/lib/modules/5.15.148-tegra/kernel/drivers/[stereolabs](https://www.stereolabs.com/)/zedx/sl\_zedx.ko==\> exists  
/usr/lib/modules/5.15.148-tegra/kernel/drivers/[stereolabs](https://www.stereolabs.com/)/zedone4k/sl\_zedxone\_uhd.ko==\> exists  
/usr/lib/modules/5.15.148-tegra/kernel/drivers/[stereolabs](https://www.stereolabs.com/)/max9295/sl\_max9295.ko==\> exists

################################################  
############ ZEDX Daemon Status LS #############  
################################################

● zed\_x\_daemon.service - ZED-X Daemon service  
Loaded: loaded (/etc/systemd/system/zed\_x\_daemon.service; enabled; vendor preset: enabled)  
Active: active (running) since Wed 2026-08-12 19:23:55 UTC; 5min ago  
Main PID: 9289 (ZEDX\_Daemon)  
Tasks: 5 (limit: 18451)  
Memory: 620.0K  
CPU: 454ms  
CGroup: /system.slice/zed\_x\_daemon.service  
└─9289 /usr/sbin/ZEDX\_Daemon

Aug 12 19:23:55 GTW-ONX1-C1GSIAXP systemd[1]: Started ZED-X Daemon service.

################################################  
############ ZEDX Driver State #############  
################################################

Note : If the following drivers has a id-state \<0, reboot is required

sl\_zedxone\_uhd 36864 0  
sl\_zedx 28672 0  
sl\_zedxhdr 20480 0  
sl\_max9295 16384 3 sl\_zedxhdr,sl\_zedxone\_uhd,sl\_zedx  
sl\_max96712 32768 4 sl\_zedxhdr,sl\_zedxone\_uhd,sl\_max9295,sl\_zedx  
tegra\_camera 217088 9 nvhost\_isp5,nvhost\_nvcsi\_t194,sl\_zedxhdr,sl\_zedxone\_uhd,nv\_hawk\_owl,nvhost\_vi5,sl\_zedx  
videodev 249856 7 v4l2\_async,sl\_zedxhdr,videobuf2\_v4l2,tegra\_camera,sl\_zedxone\_uhd,videobuf2\_common,sl\_zedx

################################################  
############ I2C Trace [-l] #############  
################################################

i2c-0 i2c 3160000.i2c I2C adapter  
i2c-1 i2c c240000.i2c I2C adapter  
i2c-2 i2c 3180000.i2c I2C adapter  
i2c-4 i2c Tegra BPMP I2C adapter I2C adapter  
i2c-5 i2c 31b0000.i2c I2C adapter  
i2c-7 i2c c250000.i2c I2C adapter  
i2c-9 i2c i2c-2-mux (chan\_id 0) I2C adapter  
i2c-10 i2c i2c-2-mux (chan\_id 1) I2C adapter  
i2c-11 i2c i2c-2-mux (chan\_id 2) I2C adapter  
i2c-12 i2c i2c-2-mux (chan\_id 3) I2C adapter

################################################  
############ I2C Trace /dev/i2C-0 #############  
################################################

```auto
 0 1 2 3 4 5 6 7 8 9 a b c d e f

```

00: – – – – – – – –  
10: – – – – – – – – – – – – – – – –  
20: – – – – – – – – – – – – – – – –  
30: – – – – – – – – – – – – – – – –  
40: – – – – – – – – – – – – – – – –  
50: UU – – – – – – – – – – – – – – –  
60: – – – – – – – – – – – – – – – –  
70: – – – – – – – –

################################################  
############ I2C Trace /dev/i2C-1 #############  
################################################

```auto
 0 1 2 3 4 5 6 7 8 9 a b c d e f

```

00: – – – – – – – –  
10: – – – – – – – – – – – – – – – –  
20: – – – – – – – – – – – – – – – –  
30: – – – – – – – – – – – – – – – –  
40: UU – – – – – – – – – – – – – – –  
50: – – – – – – – – – – – – – – – –  
60: – – – – – – – – – – – – – – – –  
70: – – – – – – – –

################################################  
############ I2C Trace /dev/i2C-2 #############  
################################################

```auto
 0 1 2 3 4 5 6 7 8 9 a b c d e f

```

00: – – – – – – – –  
10: UU – – – – – – – – – – – – – – –  
20: – – – – – – – – – UU – – – – – –  
30: – – – – – – – – – – – UU – – – –  
40: – – – – – – – – – – – – – – – –  
50: – – – – – – – – – – – – – – – –  
60: – – – – – – UU – – – – – – – – –  
70: UU – – – – – – –

> > No bus available at index 3  
> > No bus available at index 6  
> > ################################################  
> > ############ I2C Trace /dev/i2C-7 #############  
> > ################################################

```auto
 0 1 2 3 4 5 6 7 8 9 a b c d e f

```

00: – – – – – – – –  
10: – – – – – – – – – – – – – – – –  
20: – – – – – – – – – – – – – – – –  
30: – – – – – – – – – – – – – – – –  
40: – – – – – – – – – – – – – – – –  
50: 50 – – – – – – – – – – – – – – –  
60: – – – – – – – – – – – – – – – –  
70: – – – – – – – –

> > No bus available at index 8  
> > ################################################  
> > ############ I2C Trace /dev/i2C-9 #############  
> > ################################################

```auto
 0 1 2 3 4 5 6 7 8 9 a b c d e f

```

00: – – – – – – – –  
10: UU – – – – – – – 18 – – – – – – –  
20: – – – – – – – – – UU – – – – – –  
30: – – – – – – – – – – – UU 3c – – –  
40: – – – – – – – – – – – – – – – –  
50: – – – – – – 56 57 – – – – – – – –  
60: – – – – – – UU – 68 – – – – – – –  
70: UU – – – – – – –

################################################  
############ I2C Trace /dev/i2C-10 #############  
################################################

```auto
 0 1 2 3 4 5 6 7 8 9 a b c d e f

```

00: – – – – – – – –  
10: – – – – – – – – – – – – – – – –  
20: – – – – – – – – – 29 – – – – – –  
30: – – – – – – – – – – – – – – – –  
40: – – – – – – – – – – – – – – – –  
50: – – – – – – – – – – – – – – – –  
60: – – – – – – – – – – – – – – – –  
70: UU – – – – – – –

################################################  
############ I2C Trace /dev/i2C-11 #############  
################################################

```auto
 0 1 2 3 4 5 6 7 8 9 a b c d e f

```

00: – – – – – – – –  
10: – – – – – – – – – – – – – – – –  
20: – – – – – – – – – – – – – – – –  
30: – – – – – – – – – – – – – – – –  
40: – – – – – – – – – – – – – – – –  
50: – – – – – – – – – – – – – – – –  
60: – – – – – – – – – – – – – – – –  
70: UU – – – – – – –

################################################  
############ I2C Trace /dev/i2C-12 #############  
################################################

```auto
 0 1 2 3 4 5 6 7 8 9 a b c d e f

```

00: – – – – – – – –  
10: – – – – – – – – – – – – – – – –  
20: – – – – – – – – – – – – – – – –  
30: – – – – – – – – – – – – – – – –  
40: – – – – – – – – – – – – – – – –  
50: – – – – – – – – – – – – – – – –  
60: – – – – – – – – – – – – – – – –  
70: UU – – – – – – –

> > No bus available at index 13  
> > No bus available at index 14  
> > No bus available at index 15  
> > No bus available at index 16  
> > No bus available at index 30  
> > No bus available at index 31  
> > No bus available at index 32  
> > No bus available at index 33  
> > No bus available at index 34  
> > No bus available at index 35  
> > No bus available at index 36  
> > No bus available at index 37  
> > No bus available at index 38  
> > No bus available at index 39  
> > No bus available at index 40

---

<div class="post-metadata">

**Author:** ![mattrouss](https://community.stereolabs.com/user_avatar/community.stereolabs.com/mattrouss/32/2452_2.png) [@mattrouss](https://community.stereolabs.com/u/mattrouss)\
**Post date:** [August 22, 2026, 12:19am UTC](https://community.stereolabs.com/t/zed-cameras-w-o-lens-not-working/11647/2 "2026-08-22T00:19:39Z")

</div>

Hi @adeep.das , welcome to the forums 👋

Can you confirm that after connecting the camera to the ZED Box, you have run this command:

```auto
sudo systemctl restart zed_x_daemon

```

And the camera is listed with this command?

```auto
ZED_Explorer --all

```