# ZED Camera Launch (ZED2i and ZEDXOneGS) - Component degraded, and USB camera crashing every few days

**URL:** <https://community.stereolabs.com/t/zed-camera-launch-zed2i-and-zedxonegs-component-degraded-and-usb-camera-crashing-every-few-days/10678>\
**Category:** ZED2\
**Tags:** ros, sdk, jetson\
**Created:** [January 23, 2026, 3:33am UTC](https://community.stereolabs.com/t/zed-camera-launch-zed2i-and-zedxonegs-component-degraded-and-usb-camera-crashing-every-few-days/10678 "2026-01-23T03:33:27Z")\
**Posts on this page:** 6\
**Page:** 1

<div class="post-metadata">

**Author:** ![Jumana](https://community.stereolabs.com/user_avatar/community.stereolabs.com/jumana/32/5657_2.png) [@Jumana](https://community.stereolabs.com/u/Jumana)\
**Post date:** [January 23, 2026, 3:33am UTC](https://community.stereolabs.com/t/zed-camera-launch-zed2i-and-zedxonegs-component-degraded-and-usb-camera-crashing-every-few-days/10678/1 "2026-01-23T03:33:27Z")

</div>

I am seeing the following error when launching mono/stereocameras through ROS2:

[component\_container\_isolated-2] [2026-01-22 22:27:48 UTC][ZED][WARNING] Frames may be corrupted or degraded  
[component\_container\_isolated-2] [2026-01-22 22:27:48 UTC][ZED][INFO] CORRUPTED FRAME in sl::ERROR\_CODE sl:📷:grab(sl::RuntimeParameters)  
[component\_container\_isolated-2] [WARN] [1769138868.619621462] [zed.zed\_node]: Grab status degraded: CORRUPTED FRAME

I launch cameras using the ros 2 command: `ros2 launch zed_wrapper zed_camera.launch.py camera_model:=zed2i`

However, when I launch in python using `zed.open()`, the camera opens and shows SUCCESS. There seem to be no errors in `get_health_status()`, `ZED_Explorer`, etc.

What might be causing this? Could this be due to low lighting (I noticed this at night time)? The health status low light check returns False, so it doesn’t seem to be because of this.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [January 23, 2026, 8:08am UTC](https://community.stereolabs.com/t/zed-camera-launch-zed2i-and-zedxonegs-component-degraded-and-usb-camera-crashing-every-few-days/10678/2 "2026-01-23T08:08:11Z")

</div>

Hi @Jumana

> [@Jumana](#):
>
> [component\_container\_isolated-2] [2026-01-22 22:27:48 UTC][ZED][WARNING] Frames may be corrupted or degraded  
> [component\_container\_isolated-2] [2026-01-22 22:27:48 UTC][ZED][INFO] CORRUPTED FRAME in sl::ERROR\_CODE sl:📷:grab(sl::RuntimeParameters)  
> [component\_container\_isolated-2] [WARN] [1769138868.619621462] [zed.zed\_node]: Grab status degraded: CORRUPTED FRAME

This is a warning notifying you that the ZED SDK has detected bad image conditions.  
You can get information about the status by subscribing to the `~/status/health` topic.  
You can read more about the available topics in the ROS 2 Wrapper documentation:

> **[ROS 2 - ZED Stereo Node - Stereolabs](https://www.stereolabs.com/docs/ros2/zed-node)**
>
> The easiest way to start a ZED ROS 2 node for a stereo camera is by using the command line:

You can also disable this feature by setting the `general.enable_image_validity_check` parameter to `false`:

> <https://github.com/stereolabs/zed-ros2-wrapper/blob/master/zed_wrapper/config/common_stereo.yaml#L31>

---

<div class="post-metadata">

**Author:** ![Jumana](https://community.stereolabs.com/user_avatar/community.stereolabs.com/jumana/32/5657_2.png) [@Jumana](https://community.stereolabs.com/u/Jumana)\
**Post date:** [January 23, 2026, 4:57pm UTC](https://community.stereolabs.com/t/zed-camera-launch-zed2i-and-zedxonegs-component-degraded-and-usb-camera-crashing-every-few-days/10678/3 "2026-01-23T16:57:15Z")

</div>

Thanks, that’s super helpful!

I can open another discussion question for this, but I am also seeing some issues with the ZED2i camera (USB connected) when running the camera for a long time (and killing it while testing using CTRL-C).

Every few days, my jetson is unable to detect the camera (`ZED_Explorer -all` does not see the camera, and `sl.Camera.get_device_list()` does not return the camera). Note that this doesn’t seem to happen to the GMSL cameras. Is there a way to make the USB camera connection more stable so that it does not “crash” as often?

(Note that I edited the title to accomodate the two separate questions in this thread thus far 🙂 )

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [January 26, 2026, 2:50pm UTC](https://community.stereolabs.com/t/zed-camera-launch-zed2i-and-zedxonegs-component-degraded-and-usb-camera-crashing-every-few-days/10678/4 "2026-01-26T14:50:46Z")

</div>

Please check that the Jetson is not suspending the USB3 ports to reduce the amount of power.

In any case, normally you can recover the camera by using the command

`ZED_Explorer --reboot`  
or if you have more connected cameras:  
`ZED_Explorer --reboot <serial_number>`

---

<div class="post-metadata">

**Author:** ![Jumana](https://community.stereolabs.com/user_avatar/community.stereolabs.com/jumana/32/5657_2.png) [@Jumana](https://community.stereolabs.com/u/Jumana)\
**Post date:** [January 26, 2026, 4:28pm UTC](https://community.stereolabs.com/t/zed-camera-launch-zed2i-and-zedxonegs-component-degraded-and-usb-camera-crashing-every-few-days/10678/5 "2026-01-26T16:28:56Z")

</div>

Thanks, it seems like the USB camera sometimes shows up on ZED\_Explorer, and sometimes doesn’t (doesn’t seem consistent). Is there any way to make the USB connection more consistent in terms of readout from this command (or from `sl.Camera().get_device_list()`?

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [January 29, 2026, 11:13am UTC](https://community.stereolabs.com/t/zed-camera-launch-zed2i-and-zedxonegs-component-degraded-and-usb-camera-crashing-every-few-days/10678/6 "2026-01-29T11:13:15Z")

</div>

This is a clear clue of poor USB3 connection.  
I recommend you check the cables and the USB ports to be sure that they are not damaged.