# ZED Box 2 – Internal Synchronization (sync\_mode=1): Supported Trigger Frequencies and Configuration

**URL:** <https://community.stereolabs.com/t/zed-box-2-internal-synchronization-sync-mode-1-supported-trigger-frequencies-and-configuration/11853>\
**Category:** ZED Box\
**Created:** [November 17, 2026, 6:12pm UTC](https://community.stereolabs.com/t/zed-box-2-internal-synchronization-sync-mode-1-supported-trigger-frequencies-and-configuration/11853 "2026-11-17T18:12:29Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![athanasios](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/779978/32.png) [@athanasios](https://community.stereolabs.com/u/athanasios)\
**Post date:** [November 17, 2026, 6:12pm UTC](https://community.stereolabs.com/t/zed-box-2-internal-synchronization-sync-mode-1-supported-trigger-frequencies-and-configuration/11853/1 "2026-11-17T18:12:29Z")

</div>

Hi [Stereolabs](https://www.stereolabs.com/) team,

According to the [ZED Box 2 – Using GMSL documentation](https://docs.stereolabs.com/docs/products/embedded/zed-box-series/zed-box-2/using-gmsl), setting `sync_mode=1` enables internal hardware synchronization across all eight GMSL2 ports.

However, the [documentation only explains how to enable internal synchronization](https://docs.stereolabs.com/docs/products/embedded/zed-box-series/zed-box-2/using-gmsl#multi-camera-configurations), without specifying its supported frequencies or how to configure them.

We also found the [ZED Link Quad – GPIO Triggering documentation](https://docs.stereolabs.com/docs/products/embedded/zed-link-capture-card/gmsl2/zed-link-quad/zed-link-quad-gpio-triggering), which describes internally generated trigger frequencies of 15, 30, 60, and 120 Hz, depending on the camera frame rate.

We would like to clarify two points specifically for **ZED Box 2 internal synchronization (`sync_mode=1`)**:

1. **What internal synchronization frequencies are supported?** Are they limited to 15, 30, 60, and 120 Hz, or are other frequencies possible? What determines these limitations?

2. **How can we configure the internal synchronization frequency?** We have only found instructions for enabling `sync_mode=1`. Does the frequency automatically follow the camera FPS configured through the ZED SDK, or is there a separate setting?

To clarify, this question concerns **internal hardware synchronization only** , without using the Sync + IO connector or an external trigger.

Thanks!

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [November 17, 2026, 6:51pm UTC](https://community.stereolabs.com/t/zed-box-2-internal-synchronization-sync-mode-1-supported-trigger-frequencies-and-configuration/11853/2 "2026-11-17T18:51:32Z")

</div>

Hi @athanasios,

> **Supported frequencies:** Are they limited to 15, 30, 60, and 120 Hz, and what determines those limits?

Yes. With `sync_mode=1` the internally generated trigger frequency is always one of the native frame rates of the [StereoLabs](https://www.stereolabs.com/) GMSL2 cameras: 15, 30, 60, or 120 Hz. The maximum value you can use depends on the camera model, the resolution, and the number of cameras on each Quad FAKRA-Z connector. For example, 120 Hz is only available in SVGA mode, and with four stereo cameras on the same connector the limit is HD1200@30 or SVGA@60. All the combinations are in the [Multi-camera configurations](https://docs.stereolabs.com/docs/products/embedded/zed-box-2/using-gmsl#multi-camera-configurations) table.

> **Configuration:** Does the sync frequency follow the camera FPS set through the ZED SDK, or is there a separate setting?

It follows the camera FPS; there is no separate setting. The trigger frequency is the frame rate you set with [`InitParameters::camera_fps`](https://www.stereolabs.com/docs/api/structsl_1_1InitParameters.html) when you open the cameras, so all the synchronized cameras must be opened with the same frame rate.

You can find more details in the [Camera synchronization](https://docs.stereolabs.com/docs/products/embedded/zed-box-2/using-gmsl#camera-synchronization) section of the ZED Box 2 documentation.