# Zed 2i - SDK 5.2 - ZED360 calibration, floor estimation

**URL:** <https://community.stereolabs.com/t/zed-2i-sdk-5-2-zed360-calibration-floor-estimation/10991>\
**Category:** Software\
**Tags:** python, calibration, sdk\
**Created:** [March 9, 2026, 2:22pm UTC](https://community.stereolabs.com/t/zed-2i-sdk-5-2-zed360-calibration-floor-estimation/10991 "2026-03-09T14:22:32Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![lemzr](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/l/9fc348/32.png) [@lemzr](https://community.stereolabs.com/u/lemzr)\
**Post date:** [March 9, 2026, 2:22pm UTC](https://community.stereolabs.com/t/zed-2i-sdk-5-2-zed360-calibration-floor-estimation/10991/1 "2026-03-09T14:22:32Z")

</div>

I’m planning to use ZED 360 to calibrate a setup of 6 ZED 2i cameras in my master’s project and I have a few questions.

The doc mentions that floor level is estimated when the ankles are visible. Are both ankles used? And how is H calculated ? averaged over multiple frames?  
Second, our cameras are positioned to capture a seated subject, meaning a standing/walking person might not be fully visible in the field of view. Can the calibration work with a seated person with feet roughly at floor level, moving slowly in place instead of walking?  
Third, regarding _overwrite\_gravity_, is it possible to use this parameter directly within ZED360, or does it require writing a custom fusion pipeline?

Thanks

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [March 11, 2026, 3:33pm UTC](https://community.stereolabs.com/t/zed-2i-sdk-5-2-zed360-calibration-floor-estimation/10991/2 "2026-03-11T15:33:00Z")

</div>

Hi @lemzr  
Welcome to the [StereoLabs](https://www.stereolabs.com/) community.

> [@lemzr](#):
>
> The doc mentions that floor level is estimated when the ankles are visible. Are both ankles used?

If both ankles are visible, the detection is more accurate.

> [@lemzr](#):
>
> And how is H calculated ? averaged over multiple frames?

This is not public information.

> [@lemzr](#):
>
> Second, our cameras are positioned to capture a seated subject, meaning a standing/walking person might not be fully visible in the field of view. Can the calibration work with a seated person with feet roughly at floor level, moving slowly in place instead of walking?

We have not tested it in similar conditions, but it should work correctly.

> [@lemzr](#):
>
> Third, regarding _overwrite\_gravity_, is it possible to use this parameter directly within ZED360, or does it require writing a custom fusion pipeline?

Where have you found this parameter?