# ZED 2i Low Topic Frequency with ROS2 Wrapper

**URL:** <https://community.stereolabs.com/t/zed-2i-low-topic-frequency-with-ros2-wrapper/9761>\
**Category:** Software\
**Tags:** ros2\
**Created:** [August 28, 2025, 8:07am UTC](https://community.stereolabs.com/t/zed-2i-low-topic-frequency-with-ros2-wrapper/9761 "2025-08-28T08:07:54Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![h228zhou](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/h/85f322/32.png) [@h228zhou](https://community.stereolabs.com/u/h228zhou)\
**Post date:** [August 28, 2025, 8:07am UTC](https://community.stereolabs.com/t/zed-2i-low-topic-frequency-with-ros2-wrapper/9761/1 "2025-08-28T08:07:54Z")

</div>

Hello,

I am using a ZED 2i camera on Ubuntu 24.04 with ROS 2 Jazzy and the `zed_wrapper`. I configured the camera to run at **HD720 @ 30 FPS** with depth disabled and publishing only raw images + camera\_info.

The node starts correctly and the logs confirm:

- Grab resolution: **1280×720**

- Publishing resolution: **1280×720**

- Publish framerate: **30 Hz**

- GPU ID: **0**

However, when I check the actual image topics with ros2 topic hz, the measured rate is much lower (around 5–7 Hz instead of 30 Hz). CPU usage is very low (≈3%), the GPU is detected, and the camera is connected via USB 3.1 (lsusb confirms 5000M bandwidth).

```auto
average rate: 5.675
        min: 0.031s max: 12.867s std dev: 0.58325s window: 4003
average rate: 5.685
        min: 0.031s max: 12.867s std dev: 0.58223s window: 4018
average rate: 5.706
        min: 0.031s max: 12.867s std dev: 0.58079s window: 4039
average rate: 5.715
        min: 0.031s max: 12.867s std dev: 0.57997s window: 4051
average rate: 5.712
        min: 0.031s max: 12.867s std dev: 0.57968s window: 4056
average rate: 5.741
        min: 0.031s max: 12.867s std dev: 0.57787s window: 4083
average rate: 5.762
        min: 0.031s max: 12.867s std dev: 0.57647s window: 4104
average rate: 5.767
        min: 0.031s max: 12.867s std dev: 0.57569s window: 4117
average rate: 5.789
        min: 0.031s max: 12.867s std dev: 0.57424s window: 4139
average rate: 5.811
        min: 0.031s max: 12.867s std dev: 0.57287s window: 4160
average rate: 5.802
        min: 0.031s max: 12.867s std dev: 0.57300s window: 4171
average rate: 5.793
        min: 0.031s max: 12.867s std dev: 0.57332s window: 4176
average rate: 5.775
        min: 0.031s max: 12.867s std dev: 0.57429s window: 4177
average rate: 5.729
        min: 0.031s max: 12.867s std dev: 0.58188s window: 4181
average rate: 5.722
        min: 0.031s max: 12.867s std dev: 0.58197s window: 4182
average rate: 5.706
        min: 0.031s max: 12.867s std dev: 0.58283s window: 4183

```

Here are my configs:

```yaml
# config/common_stereo.yaml
# Common parameters to Stereolabs ZED Stereo cameras

---
/**:
    ros__parameters:
        use_sim_time: false # Set to `true` only if there is a publisher for the simulated clock to the `/clock` topic. Normally used in simulation mode.

        simulation:
            sim_enabled: false # Set to `true` to enable the simulation mode and connect to a simulation server
            sim_address: '127.0.0.1' # The connection address of the simulation server. See the documentation of the supported simulation plugins for more information.
            sim_port: 30000 # The connection port of the simulation server. See the documentation of the supported simulation plugins for more information.

        svo:
            use_svo_timestamps: true # Use the SVO timestamps to publish data. If false, data will be published at the system time.
            publish_svo_clock: false # [overwritten by launch file options] When use_svo_timestamps is true allows to publish the SVO clock to the `/clock` topic. This is useful for synchronous rosbag playback.
            svo_loop: false # Enable loop mode when using an SVO as input source. NOTE: ignored if SVO timestamping is used
            svo_realtime: false # if true the SVO will be played trying to respect the original framerate eventually skipping frames, otherwise every frame will be processed respecting the `pub_frame_rate` setting
            play_from_frame: 0 # Start playing the SVO from a specific frame
            replay_rate: 1.0 # Replay rate for the SVO when not used in realtime mode (between [0.10-5.0])

        general:
            camera_timeout_sec: 5
            camera_max_reconnect: 5
            camera_flip: false
            self_calib: true # Enable the self-calibration process at camera opening. See https://www.stereolabs.com/docs/api/structsl_1_1InitParameters.html#affeaa06cfc1d849e311e484ceb8edcc5
            serial_number: 0 # overwritten by launch file
            pub_resolution: 'NATIVE' # The resolution used for image and depth map publishing. 'NATIVE' to use the same `general.grab_resolution` - `CUSTOM` to apply the `general.pub_downscale_factor` downscale factory to reduce bandwidth in transmission
            pub_downscale_factor: 1.0 # rescale factor used to rescale image before publishing when 'pub_resolution' is 'CUSTOM'
            pub_frame_rate: 30.0 # [DYNAMIC] Frequency of publishing of visual images and depth data (not the Point Cloud, see 'depth.point_cloud_freq'). This value must be equal or less than the camera framerate.
            enable_image_validity_check: 1 # [SDK5 required] Sets the image validity check. If set to 1, the SDK will check if the frames are valid before processing.
            gpu_id: 0
            optional_opencv_calibration_file: '' # Optional path where the ZED SDK can find a file containing the calibration information of the camera computed by OpenCV. Read the ZED SDK documentation for more information: https://www.stereolabs.com/docs/api/structsl_1_1InitParameters.html#a9eab2753374ef3baec1d31960859ba19
            async_image_retrieval: false # If set to true will camera image retrieve at a framerate different from \ref grab() application framerate. This is useful for recording SVO or sending camera stream at different rate than application.
            # Other parameters are defined, according to the camera model, in the 'zed.yaml', 'zedm.yaml', 'zed2.yaml', 'zed2i.yaml'
            # 'zedx.yaml', 'zedxmini.yaml', 'virtual.yaml' files

        video:
            saturation: 4 # [DYNAMIC]
            sharpness: 4 # [DYNAMIC]
            gamma: 8 # [DYNAMIC]
            auto_exposure_gain: true # [DYNAMIC]
            exposure: 80 # [DYNAMIC]
            gain: 80 # [DYNAMIC]
            auto_whitebalance: true # [DYNAMIC]
            whitebalance_temperature: 42 # [DYNAMIC] - [28,65] x100 - works only if `auto_whitebalance` is false
            # Other parameters are defined, according to the camera model, in the 'zed.yaml', 'zedm.yaml', 'zed2.yaml', 'zed2i.yaml'
            # 'zedx.yaml', 'zedxmini.yaml', 'virtual.yaml' files

        sensors:
            publish_imu_tf: false # [overwritten by launch file options] enable/disable the IMU TF broadcasting
            sensors_image_sync: false # Synchronize Sensors messages with latest published video/depth message
            sensors_pub_rate: 100. # frequency of publishing of sensors data. MAX: 400. - MIN: grab rate

        region_of_interest:
            automatic_roi: false # Enable the automatic ROI generation to automatically detect part of the robot in the FoV and remove them from the processing. Note: if enabled the value of `manual_polygon` is ignored
            depth_far_threshold_meters: 2.5 # Filtering how far object in the ROI should be considered, this is useful for a vehicle for instance
            image_height_ratio_cutoff: 0.5 # By default consider only the lower half of the image, can be useful to filter out the sky
            #manual_polygon: '[]' # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
            #manual_polygon: '[[0.25,0.33],[0.75,0.33],[0.75,0.5],[0.5,0.75],[0.25,0.5]]' # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
            #manual_polygon: '[[0.25,0.25],[0.75,0.25],[0.75,0.75],[0.25,0.75]]' # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
            #manual_polygon: '[[0.5,0.25],[0.75,0.5],[0.5,0.75],[0.25,0.5]]' # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
            apply_to_depth: true # Apply ROI to depth processing
            apply_to_positional_tracking: true # Apply ROI to positional tracking processing
            apply_to_object_detection: true # Apply ROI to object detection processing
            apply_to_body_tracking: true # Apply ROI to body tracking processing
            apply_to_spatial_mapping: true # Apply ROI to spatial mapping processing

        depth:
            depth_mode: 'NONE' # Matches the ZED SDK setting: 'NONE', 'PERFORMANCE', 'QUALITY', 'ULTRA', 'NEURAL', 'NEURAL_PLUS' - Note: if 'NONE' all the modules that requires depth extraction are disabled by default (Pos. Tracking, Obj. Detection, Mapping, ...)
            depth_stabilization: 30 # Forces positional tracking to start if major than 0 - Range: [0,100]
            openni_depth_mode: false # 'false': 32bit float [meters], 'true': 16bit unsigned int [millimeters]
            point_cloud_freq: 0.0 # [DYNAMIC] Frequency of the pointcloud publishing. This value must be equal or less than the camera framerate.
            point_cloud_res: 'COMPACT' # The resolution used for point cloud publishing - 'COMPACT'-Standard resolution. Optimizes processing and bandwidth, 'REDUCED'-Half resolution. Low processing and bandwidth requirements
            depth_confidence: 95 # [DYNAMIC]
            depth_texture_conf: 100 # [DYNAMIC]
            remove_saturated_areas: true # [DYNAMIC]
            # Other parameters are defined, according to the camera model, in the 'zed.yaml', 'zedm.yaml', 'zed2.yaml', 'zed2i.yaml'
            # 'zedx.yaml', 'zedxmini.yaml', 'virtual.yaml' files

        pos_tracking:
            pos_tracking_enabled: false # True to enable positional tracking from start
            pos_tracking_mode: 'GEN_1' # Matches the ZED SDK setting: 'GEN_1', 'GEN_2', 'GEN_3'
            imu_fusion: true # enable/disable IMU fusion. When set to false, only the optical odometry will be used.
            publish_tf: true # [overwritten by launch file options] publish `odom -> camera_link` TF
            publish_map_tf: true # [overwritten by launch file options] publish `map -> odom` TF
            map_frame: 'map'
            odometry_frame: 'odom'
            area_memory: true # Enable to detect loop closure
            area_file_path: '~/test_area_memory.area' # Path to the area memory file for relocalization and loop closure in a previously explored environment. 
            save_area_memory_on_closing: true # Save Area memory before closing the camera if `area_file_path` is not empty. You can also use the `save_area_memory` service to save the area memory at any time.
            reset_odom_with_loop_closure: true # Re-initialize odometry to the last valid pose when loop closure happens (reset camera odometry drift)
            depth_min_range: 0.0 # Set this value for removing fixed zones of the robot in the FoV of the camerafrom the visual odometry evaluation
            set_as_static: false # If 'true' the camera will be static and not move in the environment
            set_gravity_as_origin: true # If 'true' align the positional tracking world to imu gravity measurement. Keep the yaw from the user initial pose.
            floor_alignment: false # Enable to automatically calculate camera/floor offset
            initial_base_pose: [0.0, 0.0, 0.0, 0.0, 0.0, 0.0] # Initial position of the `camera_link` frame in the map -> [X, Y, Z, R, P, Y]
            path_pub_rate: 2.0 # [DYNAMIC] - Camera trajectory publishing frequency
            path_max_count: -1 # use '-1' for unlimited path size
            two_d_mode: false # Force navigation on a plane. If true the Z value will be fixed to 'fixed_z_value', roll and pitch to zero
            fixed_z_value: 0.0 # Value to be used for Z coordinate if `two_d_mode` is true
            transform_time_offset: 0.0 # The value added to the timestamp of `map->odom` and `odom->camera_link` transform being generated
            reset_pose_with_svo_loop: true # Reset the camera pose the `initial_base_pose` when the SVO loop is enabled and the SVO playback reaches the end of the file.

        gnss_fusion:
            gnss_fusion_enabled: false # fuse 'sensor_msg/NavSatFix' message information into pose data
            gnss_fix_topic: '/fix' # Name of the GNSS topic of type NavSatFix to subscribe [Default: '/gps/fix']
            gnss_zero_altitude: false # Set to `true` to ignore GNSS altitude information
            h_covariance_mul: 1.0 # Multiplier factor to be applied to horizontal covariance of the received fix (plane X/Y)
            v_covariance_mul: 1.0 # Multiplier factor to be applied to vertical covariance of the received fix (Z axis)
            publish_utm_tf: true # Publish `utm` -> `map` TF
            broadcast_utm_transform_as_parent_frame: false # if 'true' publish `utm` -> `map` TF, otherwise `map` -> `utm`
            enable_reinitialization: false # determines whether reinitialization should be performed between GNSS and VIO fusion when a significant disparity is detected between GNSS data and the current fusion data. It becomes particularly crucial during prolonged GNSS signal loss scenarios.
            enable_rolling_calibration: true # If this parameter is set to true, the fusion algorithm will used a rough VIO / GNSS calibration at first and then refine it. This allow you to quickly get a fused position.
            enable_translation_uncertainty_target: false # When this parameter is enabled (set to true), the calibration process between GNSS and VIO accounts for the uncertainty in the determined translation, thereby facilitating the calibration termination. The maximum allowable uncertainty is controlled by the 'target_translation_uncertainty' parameter.
            gnss_vio_reinit_threshold: 5.0 # determines the threshold for GNSS/VIO reinitialization. If the fused position deviates beyond out of the region defined by the product of the GNSS covariance and the gnss_vio_reinit_threshold, a reinitialization will be triggered.
            target_translation_uncertainty: 0.1 # defines the target translation uncertainty at which the calibration process between GNSS and VIO concludes. By default, the threshold is set at 10 centimeters.
            target_yaw_uncertainty: 0.1 # defines the target yaw uncertainty at which the calibration process between GNSS and VIO concludes. The unit of this parameter is in radian. By default, the threshold is set at 0.1 radians.

        mapping:
            mapping_enabled: false # True to enable mapping and fused point cloud pubblication
            resolution: 0.05 # maps resolution in meters [min: 0.01f - max: 0.2f]
            max_mapping_range: 5.0 # maximum depth range while mapping in meters (-1 for automatic calculation) [2.0, 20.0]
            fused_pointcloud_freq: 1.0 # frequency of the publishing of the fused colored point cloud
            clicked_point_topic: '/clicked_point' # Topic published by Rviz when a point of the cloud is clicked. Used for plane detection
            pd_max_distance_threshold: 0.15 # Plane detection: controls the spread of plane by checking the position difference.
            pd_normal_similarity_threshold: 15.0 # Plane detection: controls the spread of plane by checking the angle difference.

        object_detection:
            od_enabled: false # True to enable Object Detection
            enable_tracking: true # Whether the object detection system includes object tracking capabilities across a sequence of images.
            detection_model: 'MULTI_CLASS_BOX_FAST' # 'MULTI_CLASS_BOX_FAST', 'MULTI_CLASS_BOX_MEDIUM', 'MULTI_CLASS_BOX_ACCURATE', 'PERSON_HEAD_BOX_FAST', 'PERSON_HEAD_BOX_ACCURATE', 'CUSTOM_YOLOLIKE_BOX_OBJECTS'
            max_range: 20.0 # [m] Upper depth range for detections.The value cannot be greater than 'depth.max_depth'
            filtering_mode: 'NMS3D' # Filtering mode that should be applied to raw detections: 'NONE', 'NMS3D', 'NMS3D_PER_CLASS'
            prediction_timeout: 2.0 # During this time [sec], the object will have OK state even if it is not detected. Set this parameter to 0 to disable SDK predictions
            allow_reduced_precision_inference: false # Allow inference to run at a lower precision to improve runtime and memory usage
            # Other parameters are defined in the 'object_detection.yaml' and 'custom_object_detection.yaml' files

        body_tracking:
            bt_enabled: false # True to enable Body Tracking
            model: 'HUMAN_BODY_MEDIUM' # 'HUMAN_BODY_FAST', 'HUMAN_BODY_MEDIUM', 'HUMAN_BODY_ACCURATE'
            body_format: 'BODY_38' # 'BODY_18','BODY_34','BODY_38'
            allow_reduced_precision_inference: false # Allow inference to run at a lower precision to improve runtime and memory usage
            max_range: 15.0 # [m] Defines a upper depth range for detections
            body_kp_selection: 'FULL' # 'FULL', 'UPPER_BODY'
            enable_body_fitting: false # Defines if the body fitting will be applied
            enable_tracking: true # Defines if the object detection will track objects across images flow
            prediction_timeout_s: 0.5 # During this time [sec], the skeleton will have OK state even if it is not detected. Set this parameter to 0 to disable SDK predictions
            confidence_threshold: 50.0 # [DYNAMIC] - Minimum value of the detection confidence of skeleton key points [0,99]
            minimum_keypoints_threshold: 5 # [DYNAMIC] - Minimum number of skeleton key points to be detected for a valid skeleton

        stream_server:
            stream_enabled: false # enable the streaming server when the camera is open
            codec: 'H264' # different encoding types for image streaming: 'H264', 'H265'
            port: 30000 # Port used for streaming. Port must be an even number. Any odd number will be rejected.
            bitrate: 12500 # [1000 - 60000] Streaming bitrate (in Kbits/s) used for streaming. See https://www.stereolabs.com/docs/api/structsl_1_1StreamingParameters.html#a873ba9440e3e9786eb1476a3bfa536d0
            gop_size: -1 # [max 256] The GOP size determines the maximum distance between IDR/I-frames. Very high GOP size will result in slightly more efficient compression, especially on static scenes. But latency will increase.
            adaptative_bitrate: false # Bitrate will be adjusted depending the number of packet dropped during streaming. If activated, the bitrate can vary between [bitrate/4, bitrate].
            chunk_size: 16084 # [1024 - 65000] Stream buffers are divided into X number of chunks where each chunk is chunk_size bytes long. You can lower chunk_size value if network generates a lot of packet lost: this will generates more chunk for a single image, but each chunk sent will be lighter to avoid inside-chunk corruption. Increasing this value can decrease latency.
            target_framerate: 0 # Framerate for the streaming output. This framerate must be below or equal to the camera framerate. Allowed framerates are 15, 30, 60 or 100 if possible. Any other values will be discarded and camera FPS will be taken.

        advanced: # WARNING: do not modify unless you are confident of what you are doing
            # Reference documentation: https://man7.org/linux/man-pages/man7/sched.7.html
            thread_sched_policy: 'SCHED_BATCH' # 'SCHED_OTHER', 'SCHED_BATCH', 'SCHED_FIFO', 'SCHED_RR' - NOTE: 'SCHED_FIFO' and 'SCHED_RR' require 'sudo'
            thread_grab_priority: 50 # ONLY with 'SCHED_FIFO' and 'SCHED_RR' - [1 (LOW) z-> 99 (HIGH)] - NOTE: 'sudo' required
            thread_sensor_priority: 70 # ONLY with 'SCHED_FIFO' and 'SCHED_RR' - [1 (LOW) z-> 99 (HIGH)] - NOTE: 'sudo' required
            thread_pointcloud_priority: 60 # ONLY with 'SCHED_FIFO' and 'SCHED_RR' - [1 (LOW) z-> 99 (HIGH)] - NOTE: 'sudo' required

        debug:
            sdk_verbose: 1 # Set the verbose level of the ZED SDK
            sdk_verbose_log_file: '' # Path to the file where the ZED SDK will log its messages. If empty, no file will be created. The log level can be set using the `sdk_verbose` parameter.
            debug_common: false
            debug_sim: false
            debug_video_depth: false
            debug_camera_controls: false
            debug_point_cloud: false
            debug_positional_tracking: false
            debug_gnss: false
            debug_sensors: false
            debug_mapping: false
            debug_terrain_mapping: false
            debug_object_detection: false
            debug_body_tracking: false
            debug_roi: false
            debug_streaming: false
            debug_advanced: false

```

Here are the rqt debug info:

 ![image](https://community.stereolabs.com/uploads/default/original/2X/b/b95a9c84f8c73adb4969e961e25bbb67152d5810.png)

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [August 28, 2025, 9:55am UTC](https://community.stereolabs.com/t/zed-2i-low-topic-frequency-with-ros2-wrapper/9761/2 "2025-08-28T09:55:56Z")

</div>

Hi @h228zhou

Welcome to the [Stereolabs](https://www.stereolabs.com/) community.

The node is running at the maximum speed, the communication middleware is not configured to provide the best performance.

I recommend you read this guide: [DDS Middleware and Network tuning - Stereolabs](https://www.stereolabs.com/docs/ros2/dds_and_network_tuning)