# Zed 2i in WSL ubuntu20.04

**URL:** <https://community.stereolabs.com/t/zed-2i-in-wsl-ubuntu20-04/2852>\
**Category:** Software\
**Tags:** windows\
**Created:** [June 19, 2023, 8:55am UTC](https://community.stereolabs.com/t/zed-2i-in-wsl-ubuntu20-04/2852 "2023-06-19T08:55:39Z")\
**Posts on this page:** 1\
**Showing post:** 3

<div class="post-metadata">

**Author:** ![zed\_for\_sam](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/z/a698b9/32.png) [@zed\_for\_sam](https://community.stereolabs.com/u/zed_for_sam)\
**Post date:** [June 20, 2023, 7:33am UTC](https://community.stereolabs.com/t/zed-2i-in-wsl-ubuntu20-04/2852/3 "2023-06-20T07:33:42Z")

</div>

I read the report file, it says the camera is not connected to computer.  
I follow the tips provide by microsoft that how can connect the usb device from window to WSL ubuntu(the link is [连接 USB 设备 | Microsoft Learn](https://learn.microsoft.com/zh-cn/windows/wsl/connect-usb)), but it seems not work.  
This is the report file:

```auto
{
    "AI Models": {
        "info": [
            "MULTI CLASS DETECTION is not optimized",
            "MULTI CLASS MEDIUM DETECTION is not optimized",
            "MULTI CLASS ACCURATE DETECTION is not optimized",
            "HUMAN BODY FAST DETECTION is not optimized",
            "HUMAN BODY MEDIUM DETECTION is not optimized",
            "HUMAN BODY ACCURATE DETECTION is not optimized",
            "HUMAN BODY 38 FAST DETECTION is not optimized",
            "HUMAN BODY 38 MEDIUM DETECTION is not optimized",
            "HUMAN BODY 38 ACCURATE DETECTION is not optimized",
            "HUMAN BODY 70 FAST DETECTION is not optimized",
            "HUMAN BODY 70 MEDIUM DETECTION is not optimized",
            "HUMAN BODY 70 ACCURATE DETECTION is not optimized",
            "PERSON HEAD DETECTION is not optimized",
            "PERSON HEAD ACCURATE DETECTION is not optimized",
            "REID ASSOCIATION is not optimized",
            "NEURAL DEPTH is not optimized"
        ]
    },
    "Camera Test": {
        "InternalDevicesCount": 1,
        "ZEDCount": 0,
        "error": [
            "<b>Camera not detected</b> <br/> Make sure the camera is plugged in or try another USB 3.0 port."
        ]
    },
    "Devices": {
        "CorruptedFirmware": false,
        "USBList": [
            {
                "USBMode": 3,
                "USB_path": "/1",
                "bDescriptorType": 1,
                "bDeviceProtocol": 1,
                "bLength": 18,
                "bMaxPacketSize0": 9,
                "bNumConfigurations": 1,
                "bcdDevice": "1.0",
                "bcdUSB": "3.0",
                "bcdUSBClass": 239,
                "bcdUSBSubClass": 2,
                "busNumber": 2,
                "device": "ZED2i",
                "iManufacturer": 1,
                "iProduct": 2,
                "iSerial": 4,
                "idProduct": "0xf880",
                "idVendor": "0x2b03"
            }
        ],
        "USBMode": 3,
        "ZED Camera Module Detected": 63616,
        "ZEDDetected": true,
        "notTested": [
            "Please connect a camera to test the USB connection."
        ]
    },
    "Graphics Card": {
        "deviceCount": 1,
        "deviceDriverVersion": 11080,
        "devices": [
            {
                "arch": "Ampere",
                "computeCapability": "8.6",
                "cores": 6144,
                "name": "NVIDIA GeForce RTX 3080 Laptop GPU",
                "totalMemoryBytes": "17179344896",
                "totalMemoryMB": 16383.5
            }
        ],
        "initResult": 0,
        "valid": [
            "<b>Graphics card: </b> NVIDIA GeForce RTX 3080 Laptop GPU"
        ]
    },
    "Processor": {
        "OS": "Ubuntu 20.04.6 LTS ",
        "avxSupported": true,
        "coreCount": "16",
        "cpu": " AMD Ryzen 9 5900HX with Radeon Graphics",
        "datetime": "2023-06-20 03:26:38 PM",
        "hyperThreading": "1",
        "motherboard": ", ",
        "ramCapacity": "16.695714",
        "ramUsage": "",
        "ramUsed": "3.714306",
        "threadCount": "32",
        "valid": [
            "<b>Processor: </b> AMD Ryzen 9 5900HX with Radeon Graphics"
        ]
    },
    "ZED SDK": {
        "CUDA Toolkit version": "V11.8.89 -->located in /usr/local/cuda-11.8/bin/nvcc",
        "CUDA loading": false,
        "GPU Driver Version": "Driver Version : 522.25",
        "GPU Performance": " Performance State : P8",
        "ZED SDK Version (Diag)": "4.0.3",
        "ZED SDK Version (RT)": "4.0.3",
        "ai": {
            "checkAI": true,
            "cudaVersion": 11080,
            "cudnnCudartVersion": 11080,
            "cudnnVersion": 8600,
            "cudnnVersionExpected": 8600,
            "tensorVersion": 8501
        },
        "binFiles": [
            "libsl_ai.so",
            "libsl_zed.so",
            "libsl_zed_static.a"
        ],
        "resourcesFiles": [
        ],
        "resourcesFilesExpected": [
            "objects_performance_3.0"
        ],
        "valid": [
            "<b>ZED SDK version:</b> 4.0.3",
            "<b>CUDA version:</b> V11.8.89"
        ]
    }
}

```

---

_[View the full topic](https://community.stereolabs.com/t/zed-2i-in-wsl-ubuntu20-04/2852)._