# Welcome to the StereoLabs Community

**URL:** <https://community.stereolabs.com/t/welcome-to-the-stereolabs-community/7>\
**Category:** Site Feedback\
**Tags:** welcome\
**Created:** [November 16, 2020, 2:22pm UTC](https://community.stereolabs.com/t/welcome-to-the-stereolabs-community/7 "2020-11-16T14:22:34Z")\
**Posts on this page:** 3\
**Page:** 1

<div class="post-metadata">

**Author:** ![system](https://community.stereolabs.com/uploads/default/original/2X/7/703c26fe16845a046a5c896e226e5f728ea313a0.svg) [@system](https://community.stereolabs.com/u/system)\
**Post date:** [November 16, 2020, 2:22pm UTC](https://community.stereolabs.com/t/welcome-to-the-stereolabs-community/7/1 "2020-11-16T14:22:34Z")

</div>

Welcome to the official [StereoLabs](https://www.stereolabs.com/) Community Forum, the best place to connect, learn, and exchange ideas about the [ZED camera family](https://www.stereolabs.com/products/), the [ZED SDK](https://www.stereolabs.com/developers/), and the entire [Stereolabs](https://www.stereolabs.com/) product ecosystem.

Whether you are an existing user or considering joining the community, we encourage you to create an account, ask your questions, and share the awesome projects you are building with our technology.

This forum is now the preferred channel for **technical questions** , so that solutions can be shared with everyone and the whole community benefits from the collective knowledge.

For **administrative, shipping, or commercial matters** , please reach out to our support team directly at [support@stereolabs.com](mailto:support@stereolabs.com).

Wondering whether to post your technical question here, on GitHub, or somewhere else? The answer is simple: it belongs right here!

We look forward to your contributions; happy building!

---

<div class="post-metadata">

**Author:** ![karinawilson](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/k/49beb7/32.png) [@karinawilson](https://community.stereolabs.com/u/karinawilson)\
**Post date:** [July 27, 2026, 3:53pm UTC](https://community.stereolabs.com/t/welcome-to-the-stereolabs-community/7/2 "2026-07-27T15:53:38Z")

</div>

I’m running a 2-camera ZED2 Fusion setup (serial numbers 25827852 and 29882646) to capture a fused 3D point cloud of a test article, and I’m running into persistent “ghosting” — objects in the fused cloud appear doubled/offset rather than as a single coherent shape, indicating an extrinsic calibration problem between the two cameras.

**What I’ve tried:**

- **ZED360 (body-tracking walk-around calibration):** An initial calibration attempt produced a reasonably well-aligned result (independently cross-checked via ICP point cloud registration). A subsequent recalibration attempt on the same physical rig — which was not intentionally moved — produced a substantially different pose (rotation shifted from ~17° to ~6.5°, and one translation component flipped sign), and the resulting fused cloud showed clear doubling.

- **OpenCV checkerboard-based stereo calibration** (using each camera’s factory rectified intrinsics, solving only the extrinsic pose).

- **ArUco marker-based calibration** (single static 160mm marker, pose solved independently per camera via `solvePnP` and averaged over 60 samples): produced a low sample-to-sample spread (~16mm/1.3°, suggesting a stable per-attempt solve), but subsequent ICP cross-check against the live scene showed very low fitness (~0.06) and continued doubling in the point cloud.

As you can see, I have now conducted multiple methods of calibrating the cameras with little success. I’m hoping others have had success, and could provide me tips, along with the support team, on the best practices for calibration. I have already looked at the documentation pages for how to use ZED360, and followed the steps as exact as I could.

Happy to provide SDK version, camera firmware, log files, or captured data if useful.

Thanks,

Karina

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [July 30, 2026, 1:22pm UTC](https://community.stereolabs.com/t/welcome-to-the-stereolabs-community/7/3 "2026-07-30T13:22:29Z")

</div>

Hi @karinawilson  
Welcome to the [StereoLabs](https://www.stereolabs.com/) community

Thank you for the very detailed report; this level of information makes the analysis much easier.

> objects in the fused cloud appear doubled/offset rather than as a single coherent shape, indicating an extrinsic calibration problem between the two cameras

Before chasing the extrinsics further, there is an important design detail of ZED360 that explains a good part of what you observed. As documented in the [Useful knowledge about the Fusion API Calibration](https://www.stereolabs.com/docs/development/zed-tools/zed-360#useful-knowledge-about-the-fusion-api-calibration) section, the optimizer only estimates the **yaw** of each camera; **pitch and roll are taken from the camera IMU** , and the floor level is estimated only if the ankles of the person are detected during the walk-around. ZED360 minimizes the distance between body keypoints, which are noisy at the centimeter level, so it is designed to produce a calibration good enough for skeleton fusion; it is not a metrology-grade extrinsic solver for point cloud registration.

This has two consequences for your case:

- Two runs on the same rig can converge to different solutions, because the cost function is weakly constrained if the person does not cover the whole shared volume at several depths. The jump you saw from ~17° to ~6.5° with a translation sign flip is typical of an under-constrained optimization, not of a moved rig.
- Any residual pitch/roll error coming from the IMU cannot be corrected by the optimizer, and a fraction of a degree of tilt is enough to produce visible doubling on a target a few meters away.

**Step 1: validate each camera individually before fusing.** Ghosting is not necessarily extrinsic. Open each camera separately in [ZED Depth Viewer](https://www.stereolabs.com/docs/development/zed-tools/zed-depth-viewer) at the working distance and check a flat reference surface for bowing or a distance bias. If one of the two stereo calibrations has drifted (impact, strong thermal cycling, glass in front of the lens), no extrinsic transform will ever align the two clouds, and ICP fitness will stay low. You can restore the factory calibration from [ZED Explorer](https://www.stereolabs.com/docs/development/zed-tools/zed-explorer#calibration-parameters), and use [ZED Calibration](https://www.stereolabs.com/docs/development/zed-tools/zed-calibration) only if you have a specific reason to override the factory data. Also use `DEPTH_MODE::NEURAL_PLUS` for this kind of geometric work, see [Depth Modes](https://www.stereolabs.com/docs/development/zed-sdk/modules/depth-sensing/depth-modes), and set a conservative `confidence_threshold` so that unreliable edge points do not look like a second surface. One more thing worth testing: set `InitParameters::camera_disable_self_calib = true` on both cameras, so the self-calibration performed at each `open()` cannot slightly change the stereo geometry between your calibration session and your capture session.

**Step 2: check the convention used to inject your own extrinsics.** This is the most frequent cause of a “stable solve, wrong result”. As described in the [Fusion configuration files](https://www.stereolabs.com/docs/development/zed-sdk/modules/fusion#configuration-files) section, the pose stored in the JSON must be expressed in meters and in `COORDINATE_SYSTEM::IMAGE`; the SDK read/write helpers handle the conversion to the coordinate system you requested in `InitParameters`. If you parse the JSON yourself and apply the pose to clouds retrieved in `RIGHT_HANDED_Y_UP`, you get exactly the kind of axis permutation and sign flip you are describing. The [Coordinate Frames](https://www.stereolabs.com/docs/development/zed-sdk/modules/positional-tracking/coordinate-frames) page has the reference conventions.

**Step 3: on the marker approach.** A 16 mm / 1.3° sample-to-sample spread is repeatability, not accuracy; a single 160 mm marker seen from a few meters gives a poorly conditioned rotation estimate and is subject to planar pose ambiguity, so the bias can easily be an order of magnitude larger than the spread. A ChArUco board, or several markers spread over the working volume, will constrain the solution much better. Please also check that you are feeding `solvePnP` with the **rectified** intrinsics and zero distortion (`camera_configuration.calibration_parameters`, not `..._raw`), since you are working on rectified images.

**Practical path that usually works for a static scene like yours:** use ZED360 only to get a coarse initialization, then refine with ICP on the static test article itself, and write the refined pose back into the Fusion JSON. With a coarse init available, the ICP `max_correspondence_distance` should be a few centimeters, not meters; a fitness of 0.06 usually means the initial guess is far off, the units differ (millimeters against meters), or the two clouds barely overlap. Also make sure both clouds are cropped to the shared volume before running ICP, otherwise the non-overlapping background dominates the correspondence count.

Finally, please keep in mind that two ZED 2 cameras on USB are not hardware synchronized. This is not an issue for a static article, but it does add noise to the calibration walk-around; walking slowly, as recommended in the ZED360 procedure, is important. If you plan to grow this rig, the [ZED X](https://www.stereolabs.com/products/zed-x) family on GMSL2 supports hardware synchronized capture through the ZED Link capture cards, which removes that error source entirely ([store page](https://store.stereolabs.com/products/zed-x-stereo-camera)).

If you can share the ZED SDK version, the camera firmware versions, the ZED360 JSON file, and two short SVO2 recordings of the scene (one per camera), we can check the geometry on our side and tell you whether the residual error is extrinsic or per-camera depth.