# Using Two ZED X One Monocular Cameras for Custom 2 m Baseline Stereo – Calibration, SDK Support & Environmental Specs

**URL:** <https://community.stereolabs.com/t/using-two-zed-x-one-monocular-cameras-for-custom-2-m-baseline-stereo-calibration-sdk-support-environmental-specs/10631>\
**Category:** ZED X\
**Created:** [January 13, 2026, 3:34pm UTC](https://community.stereolabs.com/t/using-two-zed-x-one-monocular-cameras-for-custom-2-m-baseline-stereo-calibration-sdk-support-environmental-specs/10631 "2026-01-13T15:34:03Z")\
**Posts on this page:** 9\
**Page:** 1

<div class="post-metadata">

**Author:** ![NivC](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/n/ecae2f/32.png) [@NivC](https://community.stereolabs.com/u/NivC)\
**Post date:** [January 13, 2026, 3:34pm UTC](https://community.stereolabs.com/t/using-two-zed-x-one-monocular-cameras-for-custom-2-m-baseline-stereo-calibration-sdk-support-environmental-specs/10631/1 "2026-01-13T15:34:03Z")

</div>

Hello [Stereolabs](https://www.stereolabs.com/) team,

I’m evaluating the **ZED X One monocular camera family** for a custom stereo-vision setup and would appreciate clarification on a few technical points before moving forward.

### **Project Overview**

- I plan to use **two ZED X One monocular cameras** to build a **custom stereo pair** with a **baseline of ~2 meters** , aiming to improve depth accuracy at long range.

- Target platform: **NVIDIA Jetson Orin Nano**

- Environment: **open sea / outdoor**

- Target object size: approx. **1-2 m wide × 4–5 m long (boat-sized object)**

- Detection & tracking range: **up to 100 m**

- Most critical depth accuracy: **below 50 m**

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [January 14, 2026, 9:27am UTC](https://community.stereolabs.com/t/using-two-zed-x-one-monocular-cameras-for-custom-2-m-baseline-stereo-calibration-sdk-support-environmental-specs/10631/2 "2026-01-14T09:27:27Z")

</div>

Hi @NivC

> [@NivC](#):
>
> **1. Calibration**  
> Do you provide calibration tools, code, or guidelines for using **two independent ZED X One cameras** with a **large custom baseline (~2 m)**, and can this be integrated into the ZED SDK?

We provide [this tool](https://github.com/stereolabs/zed-opencv-calibration), which can be used for the baseline you described too.  
I recommend using a big checkerboard, 100 or 150 mm square, for example.

> [@NivC](#):
>
> **2. SDK & Jetson support**  
> Is using **two ZED X One cameras via ZED Link + GMSL2** on a **Jetson Orin Nano** fully supported and stable in the SDK?

Yes, with the ZED SDK v5.1, you can natively create a stereo rig from 2x ZED X One cameras.  
You can use the stereo\_reprojection\_viewer tool as an example:

> <https://github.com/stereolabs/zed-opencv-calibration/blob/main/stereo_reprojection_viewer/src/main.cpp#L340-L416>

> [@NivC](#):
>
> Is IP69K limited only to the **ZED X One S (Light) wide lens**?

Yes

> [@NivC](#):
>
> What are the IP ratings for the **narrow lens** and other models like **ZED X One GS**?

It has no IP-rating certification

> [@NivC](#):
>
> **4. GMSL2 cables/connectors**  
> Do the **GMSL2 cables and connectors** also have an ingress protection rating?

Yes, they are protected against water ingress too.

> [@NivC](#):
>
> **5. Sensor variants**  
> Are **monochrome or IR camera variants** available (or planned) for the ZED X One monocular lineup?

The ZED SDK allows you to retrieve monochrome images, but we have no plans to release cameras with monochrome CMOS sensors.  
Regarding IR, you can get the “no lens” variant and add optics with no included IR filters.

---

<div class="post-metadata">

**Author:** ![NivC](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/n/ecae2f/32.png) [@NivC](https://community.stereolabs.com/u/NivC)\
**Post date:** [January 15, 2026, 9:12am UTC](https://community.stereolabs.com/t/using-two-zed-x-one-monocular-cameras-for-custom-2-m-baseline-stereo-calibration-sdk-support-environmental-specs/10631/3 "2026-01-15T09:12:38Z")

</div>

> What are the IP ratings for the **narrow lens** and other models like **ZED X One GS**?

You mentioned that the narrow lens version currently has no IP-rating certification. Is it possible to custom order an IP69K-rated version of the ZED X One S (narrow lens)? If not, is IP69K certification planned for this model or any other ZED X One variants in the near future?

> “You can get the “no lens” variant and add optics with no included IR filters.”

Regarding IR: I understand that the “no lens” variant allows the use of optics without integrated IR-cut filters. My goal is to detect object (boat) at night at distances of up to ~30 m. Is this achievable with the standard wide or narrow lens configurations of the ZED X One cameras?

If not, do you offer or recommend any lenses without IR-cut filters that are known to work well with the ZED X One?

I’m also interested in using two cameras for stereo vision, along with an additional camera on the same system (three cameras total). Given that I’m using an **NVIDIA Jetson Orin Nano** , what type of **link**  **connectivity** would I need to support this setup?

I’m interested in purchasing ZED X One cameras and would be happy to discuss my requirements in more detail. Is it possible to arrange a short call or continue the discussion via email?

Best regards,  
**Niv**

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [January 15, 2026, 1:42pm UTC](https://community.stereolabs.com/t/using-two-zed-x-one-monocular-cameras-for-custom-2-m-baseline-stereo-calibration-sdk-support-environmental-specs/10631/4 "2026-01-15T13:42:55Z")

</div>

> [@NivC](#):
>
> Is it possible to custom order an IP69K-rated version of the ZED X One S (narrow lens)?

The ZED X One S is available in Fisheye, Wide,Narrow, and No Lens configuration:

 ![image](https://community.stereolabs.com/uploads/default/original/2X/1/15694fa6243362557b0b444dfa3f34b269075b5f.png)

> [@NivC](#):
>
> My goal is to detect object (boat) at night at distances of up to ~30 m. Is this achievable with the standard wide or narrow lens configurations of the ZED X One cameras?

This is possible only if you use visible light solutions. You cannot use our optics solutions with IR lighting systems.

> [@NivC](#):
>
> If not, do you offer or recommend any lenses without IR-cut filters that are known to work well with the ZED X One?

We do not have this information.

> [@NivC](#):
>
> I’m also interested in using two cameras for stereo vision, along with an additional camera on the same system (three cameras total). Given that I’m using an **NVIDIA Jetson Orin Nano** , what type of **link**  **connectivity** would I need to support this setup?

You must use a ZED Link Duo capture card that allows you to connect up to 4 cameras:

> **[ZED Link Duo on Orin Nano - Stereolabs](https://www.stereolabs.com/docs/embedded/zed-link/dual-jetson-orin-nano-devkit-setup)**
>
> This tutorial will help you set up the ZED Link Duo GMSL2 capture card, and use the Stereolabs GMSL2 cameras with the NVIDIA® Jetson™ Orin Nano Developer Kits.

> [@NivC](#):
>
> I’m interested in purchasing ZED X One cameras and would be happy to discuss my requirements in more detail. Is it possible to arrange a short call or continue the discussion via email?

We provide unlimited support to all our customers. At this time, we don’t offer assistance through meetings or phone calls, as focusing on online support allows us to respond faster and in greater detail.

If you have details **that cannot be publicly discussed** , please write an email to [support@stereolabs.com](mailto:support@stereolabs.com) to discuss them privately with our support team.

---

<div class="post-metadata">

**Author:** ![NivC](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/n/ecae2f/32.png) [@NivC](https://community.stereolabs.com/u/NivC)\
**Post date:** [January 15, 2026, 2:03pm UTC](https://community.stereolabs.com/t/using-two-zed-x-one-monocular-cameras-for-custom-2-m-baseline-stereo-calibration-sdk-support-environmental-specs/10631/5 "2026-01-15T14:03:48Z")

</div>

Thanks for the quick response

> The ZED X One S is available in Fisheye, Wide,Narrow, and No Lens configuration:

 ![15694fa6243362557b0b444dfa3f34b269075b5f](https://community.stereolabs.com/uploads/default/original/2X/c/c7b8311ed0374553a38a7511d895cc90ee03e2b2.png)

So, to confirm—are **all ZED X One S lens variants** (Fisheye, Wide, Narrow, and No Lens) rated **IP69K**?

Based on the description, I initially understood that the **IP69K rating applied only to the Wide lens variant** by the line in the image (highlighted in yellow).

Could you please clarify?

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [January 15, 2026, 2:46pm UTC](https://community.stereolabs.com/t/using-two-zed-x-one-monocular-cameras-for-custom-2-m-baseline-stereo-calibration-sdk-support-environmental-specs/10631/6 "2026-01-15T14:46:43Z")

</div>

> [@NivC](#):
>
> So, to confirm—are **all ZED X One S lens variants** (Fisheye, Wide, Narrow, and No Lens) rated **IP69K**?

~~Only the model with the included lenses, because they are assembled to guarantee the rating~~  
We cannot certify custom optics solutions to be IP69 K-rated.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [January 15, 2026, 2:48pm UTC](https://community.stereolabs.com/t/using-two-zed-x-one-monocular-cameras-for-custom-2-m-baseline-stereo-calibration-sdk-support-environmental-specs/10631/7 "2026-01-15T14:48:45Z")

</div>

> [@NivC](#):
>
> Based on the description, I initially understood that the **IP69K rating applied only to the Wide lens variant** by the line in the image (highlighted in yellow).

I must agree with you:  
 ![image](https://community.stereolabs.com/uploads/default/original/2X/b/b97c75d26cb237336b9b60b5cb2b7b907c28bd75.png)

This information comes from the [datasheet](https://cdn.sanity.io/files/s18ewfw4/staging/5617ab0ab4a1c509c7eba63a64c1e145b7c8df82.pdf/ZED%20X%20One%20S%20-%20datasheet-11-12-25.pdf) of the camera..

---

<div class="post-metadata">

**Author:** ![NivC](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/n/ecae2f/32.png) [@NivC](https://community.stereolabs.com/u/NivC)\
**Post date:** [January 15, 2026, 2:54pm UTC](https://community.stereolabs.com/t/using-two-zed-x-one-monocular-cameras-for-custom-2-m-baseline-stereo-calibration-sdk-support-environmental-specs/10631/8 "2026-01-15T14:54:13Z")

</div>

I want to purchase pair of the narrow lens Zed X One S, but I need to know if it IP69K, I would appreciate if you can double check if it stands for that requirement.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [January 15, 2026, 2:55pm UTC](https://community.stereolabs.com/t/using-two-zed-x-one-monocular-cameras-for-custom-2-m-baseline-stereo-calibration-sdk-support-environmental-specs/10631/9 "2026-01-15T14:55:10Z")

</div>

I confirm that only the ZED X One S with Wide optics are IP69K certified.