# Using sync-in port as external trigger for ZED box mina ZEDx camera over GSML2

**URL:** <https://community.stereolabs.com/t/using-sync-in-port-as-external-trigger-for-zed-box-mina-zedx-camera-over-gsml2/10719>\
**Category:** ZED Mini\
**Tags:** jetson\
**Created:** [January 29, 2026, 3:18pm UTC](https://community.stereolabs.com/t/using-sync-in-port-as-external-trigger-for-zed-box-mina-zedx-camera-over-gsml2/10719 "2026-01-29T15:18:37Z")\
**Posts on this page:** 7\
**Page:** 1

<div class="post-metadata">

**Author:** ![Olvert77](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/o/dec6dc/32.png) [@Olvert77](https://community.stereolabs.com/u/Olvert77)\
**Post date:** [January 29, 2026, 3:18pm UTC](https://community.stereolabs.com/t/using-sync-in-port-as-external-trigger-for-zed-box-mina-zedx-camera-over-gsml2/10719/1 "2026-01-29T15:18:37Z")

</div>

I have a setup with a ZED Box Mini and 2 ZEDX cameras connected over GSML2.  
I have connected an external trigger to the sync-in port which i for test control with a testapplication.

However the cameras are not leaving free-running mode? My SDK version is v5.0.0 and Ubuntu 22.04.5’  
Help is very appreciated!

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [January 29, 2026, 3:33pm UTC](https://community.stereolabs.com/t/using-sync-in-port-as-external-trigger-for-zed-box-mina-zedx-camera-over-gsml2/10719/2 "2026-01-29T15:33:26Z")

</div>

Hi @Olvert77  
Welcome to the [StereoLabs](https://www.stereolabs.com/) community.

> [@Olvert77](#):
>
> My SDK version is v5.0.0 and Ubuntu 22.04.5’

You must install the latest [ZED SDK v5.1.2](https://www.stereolabs.com/developers/release), the latest [ZED X Driver v1.3.2](https://www.stereolabs.com/developers/drivers), and follow this guide to set the ZED Box Orin in master trigger mode:

> **[SYNC-OUT - ZED Box Mini Connectivity - Stereolabs](https://www.stereolabs.com/docs/embedded/zed-box-mini/connectivity#sync-out)**
>
> The synchronization-output connector is used as a frame-sync trigger output to synchronize image acquisition on multiple GMSL2 cameras connected to different ZED Box Minis. | Connection Ports # Front side # Power connector Ethernet connector Power...

You must also set up PTP to make sure that the ZED Box Mini and the slave clocks are synchronized, in the case the slave runs a Linux based OS.

---

<div class="post-metadata">

**Author:** ![Olvert77](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/o/dec6dc/32.png) [@Olvert77](https://community.stereolabs.com/u/Olvert77)\
**Post date:** [January 29, 2026, 3:49pm UTC](https://community.stereolabs.com/t/using-sync-in-port-as-external-trigger-for-zed-box-mina-zedx-camera-over-gsml2/10719/3 "2026-01-29T15:49:39Z")

</div>

Thanks for the response!

However the documentation makes me a bit confused. Is it even possible to operate in the way I want? I simply want to capture a frame when my trigger goes high … like if I had an external button. The document makes me worry I can only sync a number of devices to a common given fps?

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [January 29, 2026, 3:58pm UTC](https://community.stereolabs.com/t/using-sync-in-port-as-external-trigger-for-zed-box-mina-zedx-camera-over-gsml2/10719/4 "2026-01-29T15:58:09Z")

</div>

> [@Olvert77](#):
>
> I simply want to capture a frame when my trigger goes high

This is not yet allowed.

> [@Olvert77](#):
>
> The document makes me worry I can only sync a number of devices to a common given fps?

Yes, this is correct. The `slave mode` allows you to trigger capture only at supported frequencies:  
15 Hz, 30 Hz, 60 Hz, and 120 Hz (only in SVGA mode).

---

<div class="post-metadata">

**Author:** ![Olvert77](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/o/dec6dc/32.png) [@Olvert77](https://community.stereolabs.com/u/Olvert77)\
**Post date:** [January 29, 2026, 4:40pm UTC](https://community.stereolabs.com/t/using-sync-in-port-as-external-trigger-for-zed-box-mina-zedx-camera-over-gsml2/10719/5 "2026-01-29T16:40:27Z")

</div>

Ok, then I’ll try to go the other way around and let the cameras trig the rest of my system.

I see the sync-out aligning with the fps now. Can you please confirm that the frames are captured on the rising-edge?

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [January 29, 2026, 4:59pm UTC](https://community.stereolabs.com/t/using-sync-in-port-as-external-trigger-for-zed-box-mina-zedx-camera-over-gsml2/10719/6 "2026-01-29T16:59:28Z")

</div>

> [@Olvert77](#):
>
> Can you please confirm that the frames are captured on the rising-edge?

Yes, they are captured on the rising edge

---

<div class="post-metadata">

**Author:** ![hamdan11](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/h/ce7236/32.png) [@hamdan11](https://community.stereolabs.com/u/hamdan11)\
**Post date:** [April 15, 2026, 8:32am UTC](https://community.stereolabs.com/t/using-sync-in-port-as-external-trigger-for-zed-box-mina-zedx-camera-over-gsml2/10719/7 "2026-04-15T08:32:44Z")

</div>

hi .. i have a doubt….so the camera when in master mode generates signals (30 signals) per sec if its at 30 fps??also i have connected a strobing controller to the sync out pin so practically when the camera runs in free mode while being configured as master with sync\_mode=0 then it should cnstantly send 30 signals every sec ryt?? also when i turn off the explorer will the signals be stopped or turn off the daemon ..??