# Unity ZEDView doesn't show the live footage when using stream input

**URL:** <https://community.stereolabs.com/t/unity-zedview-doesnt-show-the-live-footage-when-using-stream-input/11704>\
**Category:** Unity\
**Created:** [September 8, 2026, 1:45am UTC](https://community.stereolabs.com/t/unity-zedview-doesnt-show-the-live-footage-when-using-stream-input/11704 "2026-09-08T01:45:23Z")\
**Posts on this page:** 5\
**Page:** 1

<div class="post-metadata">

**Author:** ![punnlert](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/b38774/32.png) [@punnlert](https://community.stereolabs.com/u/punnlert)\
**Post date:** [September 8, 2026, 1:45am UTC](https://community.stereolabs.com/t/unity-zedview-doesnt-show-the-live-footage-when-using-stream-input/11704/1 "2026-09-08T01:45:23Z")

</div>

I followed the instruction from [Body Tracking | StereoLabs](https://docs.stereolabs.com/docs/integrations/unity/body-tracking) to set up a body tracking scene. The only [Stereolabs](https://www.stereolabs.com/)’ camera I have is the ZED X so I use a Jetson Orin Nano to connect with it and streamed the input over the network. But when I run the scene, the small window that is suppose to show the live view just showed a brief loading icon and then turned grey.

I would also like to note that the tracking mannequin was mimicking my movement perfectly and I tested the stream separately with this script [zed-sdk/camera streaming/receiver/cpp at master · stereolabs/zed-sdk · GitHub](https://github.com/stereolabs/zed-sdk/tree/master/camera%20streaming/receiver/cpp) and it also receives the video perfectly. I checked the URP pipeline and made sure that all materials has been converted.

My ZED SDK version is 5.4.1 on both Jetson Orin Nano and the machine that run Unity. I stream the content using ZED Explorer.

Does anybody have a suggestion on how I should proceed?

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [September 8, 2026, 9:54am UTC](https://community.stereolabs.com/t/unity-zedview-doesnt-show-the-live-footage-when-using-stream-input/11704/2 "2026-09-08T09:54:42Z")

</div>

Hi @punnlert, thanks for the detailed report, it really helps.

> [@punnlert](#):
>
> the small window that is suppose to show the live view just showed a brief loading icon and then turned grey.

> [@punnlert](#):
>
> I would also like to note that the tracking mannequin was mimicking my movement perfectly

These two facts together are very informative. The body tracking data path and the image display path in the Unity plugin are independent: skeletons come from the SDK as data structures, while the image is copied GPU-side into a Unity texture, drawn on the `Frame` quad under `ZED_Rig_Mono -> Camera_Left`, rendered into the `ZEDView` render texture, and finally displayed by the `Virtual Canvas` prefab. Since the avatar is animated correctly, the camera is open and the stream is being received; the problem is almost certainly in the image texture/rendering chain, not in the streaming input. Your C++ receiver test confirms this too.

Here is what I suggest checking, in order:

**1. Unity Console at startup**  
Please look for errors or warnings right after the loading icon disappears (shader/material errors, texture creation or registration failures). That log is usually enough to identify the exact cause.

**2. Graphics API**  
The image sharing between the ZED SDK and Unity requires Direct3D11 on Windows. Go to `Edit -> Project Settings -> Player -> Other Settings`, uncheck **Auto Graphics API for Windows** , and make sure **Direct3D11** is first in the list. If you are on a laptop with hybrid graphics, also force Unity to run on the NVIDIA GPU from the NVIDIA Control Panel; the SDK runs on the discrete GPU and the texture copy fails silently if Unity renders on the integrated one.

**3. URP materials**  
Even when the Render Pipeline Converter reports success, the ZED frame material is a frequent exception. Select `ZED_Rig_Mono -> Camera_Left -> Frame` and verify that the assigned material is the `_URP` variant, as described in the note at the bottom of our [Getting Started with Unity page](https://docs.stereolabs.com/docs/integrations/unity). Do the same for the quad of the `Virtual Canvas` prefab.

**4. Render texture wiring**  
As per the [Body Tracking tutorial](https://docs.stereolabs.com/docs/integrations/unity/body-tracking), `Camera_Left` must have `ZEDView` as **Target Texture** , and the `Virtual Canvas` must display that same render texture. Also check that the `Virtual View Camera` has a higher depth than `Camera_Left`, and that no other camera in the scene is overriding the output.

**5. Isolate the render pipeline from the input**  
Two quick tests that will tell us a lot:

- Record an SVO on the Jetson, copy it to the Unity machine, and use SVO input in `ZEDManager`. If the view is still grey, the issue is in the project rendering setup and not in the streaming.
- Open the stock Body Tracking sample scene shipped with the plugin (Samples tab in the Package Manager) and run it with your stream. If the image appears there, we can compare the two scenes.

**6. Version match**  
Could you confirm your Unity version and the version of the [ZED Unity plugin](https://github.com/stereolabs/zed-unity) you installed? The plugin must be the release matching ZED SDK 5.4, which you can double check on the [Developer Center](https://www.stereolabs.com/developers/release/).

For reference, streaming from a Jetson to a desktop is a fully supported workflow, so your ZED X on a Jetson Orin Nano is a valid setup here: [Developing with ZED X on a PC](https://docs.stereolabs.com/docs/products/cameras/zedx/development-on-pc) and [Local Network Streaming](https://docs.stereolabs.com/docs/development/zed-sdk/modules/camera/local-network-streaming). If at some point you only need the avatar animation and not the video passthrough, [ZED Live Link for Unity](https://docs.stereolabs.com/docs/integrations/live-link/live-link-for-unity) is an alternative that sends body tracking data over UDP; note that it does not carry the video stream, so it would not replace the live view you are looking for. If instead you plan to extend the tracked volume later, adding a second [ZED X](https://store.stereolabs.com/en-fr/products/zed-x-stereo-camera) and using our Fusion module with [ZED360](https://docs.stereolabs.com/docs/development/zed-tools/zed-360) gives noticeably more robust skeletons in occluded scenes.

Please post the Console log and the outcome of the SVO test, and we will narrow it down from there.

Best,  
Walter

---

<div class="post-metadata">

**Author:** ![punnlert](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/b38774/32.png) [@punnlert](https://community.stereolabs.com/u/punnlert)\
**Post date:** [September 11, 2026, 6:01am UTC](https://community.stereolabs.com/t/unity-zedview-doesnt-show-the-live-footage-when-using-stream-input/11704/3 "2026-09-11T06:01:37Z")

</div>

Hello,

Thank you for taking your time to write a detailed troubleshoot. I tried all of the solution.

**1. Unity Console at startup**

This is the screenshot of the console after startup and the ZEDView went blank

 ![Screenshot from 2026-09-11 14-50-43](https://community.stereolabs.com/uploads/default/original/2X/8/89d31d7f177e55eb846a9235760ecee81353d543.png)

**2. Graphics API**

I’m on a linux laptop and using NVIDIA GPU. I’m not sure how to force Unity to run on the NVIDIA GPU. But I unchecked the **Auto Graphics API for Windows.**

**3. URP materials**

I did this but still no image shows.

**4. Render texture wiring**

I was using the sample scene for this. I checked and the Camera\_Left has ZEDView as Target Texture (In this version, it’s called output texture in this version)

**5. Isolate the render pipeline from the input**

I use SVO as an input and it didn’t show anything. I also tried stock sample scene but it also not working.

**6. Version match**

the ZED Unity plugin is 5.4.0 and my ZED SDK is the latest 5.4.1

Best,  
Punn

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [September 11, 2026, 8:01am UTC](https://community.stereolabs.com/t/unity-zedview-doesnt-show-the-live-footage-when-using-stream-input/11704/4 "2026-09-11T08:01:42Z")

</div>

> [@punnlert](#):
>
> **2. Graphics API**
> 
> I’m on a linux laptop and using NVIDIA GPU. I’m not sure how to force Unity to run on the NVIDIA GPU. But I unchecked the **Auto Graphics API for Windows.**

Please check this:  
[https://support.stereolabs.com/hc/en-us/articles/8422008229143-How-can-I-solve-ZED-SDK-OpenGL-issues-under-Ubuntu](https://support.stereolabs.com/hc/en-us/articles/8422008229143-How-can-I-solve-ZED-SDK-OpenGL-issues-under-Ubuntu)

---

<div class="post-metadata">

**Author:** ![punnlert](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/b38774/32.png) [@punnlert](https://community.stereolabs.com/u/punnlert)\
**Post date:** [September 14, 2026, 2:47am UTC](https://community.stereolabs.com/t/unity-zedview-doesnt-show-the-live-footage-when-using-stream-input/11704/5 "2026-09-14T02:47:02Z")

</div>

This solves the problem completely, thank you!