Unidefined symbol launching python program

I figured out the problem. This is because StereoLabs released SDK 5.0.2 and the matching Python API. The problem is that StereoLabs doesn’t maintain ABI compatibility between patch releases, and the Python API is not versioned at the patch release level.

So in our case we have an install_zed.sh shell script that downloads SDK version 5.0.1 and then runs /usr/local/zed/get_python_api.py. But the api install script pulls version “5.0”, which has been updated to be compatible with 5.0.2 and is not backwards compatible with 5.0.1.

StereoLabs either needs to start versioning the Python API with patch versions so the SDK can install the correct version, or needs to maintain ABI compatibility between patch releases.