# Unable to boot ZED Box Orin NX | NVIDIA logo -\>black screen-\> continuously blinking \_

**URL:** <https://community.stereolabs.com/t/unable-to-boot-zed-box-orin-nx-nvidia-logo-black-screen-continuously-blinking/11760>\
**Category:** ZED Box\
**Created:** [September 28, 2026, 12:40pm UTC](https://community.stereolabs.com/t/unable-to-boot-zed-box-orin-nx-nvidia-logo-black-screen-continuously-blinking/11760 "2026-09-28T12:40:04Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![ashutosh.sahu](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/5f9b8f/32.png) [@ashutosh.sahu](https://community.stereolabs.com/u/ashutosh.sahu)\
**Post date:** [September 28, 2026, 12:40pm UTC](https://community.stereolabs.com/t/unable-to-boot-zed-box-orin-nx-nvidia-logo-black-screen-continuously-blinking/11760/1 "2026-09-28T12:40:04Z")

</div>

Hello,

I have a **ZED Box Orin NX 16GB running JetPack 6.2 / L4T 36.4.3.**

The device stopped booting. The current behavior during boot is:

**NVIDIA logo → black screen → continuously blinking \_**

During this blinking stage, the power LED remains green. I have tried to do ssh, but it did not work.

I have performed the troubleshooting/recovery procedures described in your documentation My observations are:

- UEFI is accessible and functioning.

- The Orin NX 16GB and 16197 MB RAM are detected in UEFI.

- The internal NVMe SSD is detected by UEFI.

- I created the official JetPack 6.2 recovery USB using [zedbox\_all\_usb\_flash\_6.2.sh](http://zedbox_all_usb_flash_6.2.sh "http://zedbox\_all\_usb\_flash\_6.2.sh/").

- The recovery USB is detected by UEFI.

- Running EFI\BOOT\BOOTAA64.efi manually starts and it displays the following:

The system then hangs with a blinking \_.

I have also tried the live-USB Force Recovery procedure using the USB-A port.

However: lsusb -d ‘0955:’ , never detects the expected Orin NX 16GB recovery device: 0955:7323.

The Micro-USB OTG port also does not enumerate as /dev/ttyACM0 on an Ubuntu 22.04 host. The same host USB port successfully detects other USB devices.

I also noticed that the UEFI RTC had reset to: 01/01/1970

I corrected the date/time, but the boot problem remained.

The device also becomes noticeably warm during these recovery attempts.

The most important point: **I have important data on the internal NVMe and do not want to erase/reflash it before attempting data recovery.**

**Could you please advise whether this indicates a hardware/bootloader issue and provide the recommended procedure for backing up the internal NVMe data before any reflash/recovery? How should I get the ZED Box working again?**

I can provide photographs of the UEFI screens, recovery boot output, serial/USB tests, and the recovery USB configuration if required.

Thank you.

 ![shared image (3)](https://community.stereolabs.com/uploads/default/original/2X/e/ea5b99d3f81e12fdedcc802c7f6467f92e2aefb2.jpeg)

 ![Media (20)](https://community.stereolabs.com/uploads/default/original/2X/8/8079cc4d2e04d347bf9f7a5d8a9c919157104c32.jpeg)

---

<div class="post-metadata">

**Author:** ![pylon-sync-bot](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/dbc845/32.png) [@pylon-sync-bot](https://community.stereolabs.com/u/pylon-sync-bot)\
**Post date:** [October 9, 2026, 10:15am UTC](https://community.stereolabs.com/t/unable-to-boot-zed-box-orin-nx-nvidia-logo-black-screen-continuously-blinking/11760/2 "2026-10-09T10:15:12Z")

</div>

Hi,

Your data on the NVMe should be safe: nothing below erases or reflashes it. This looks like an issue we’ve seen recently. A Linux package update can break one of the drivers our board relies on, so it’s unlikely to be a hardware problem.

1. Press Esc repeatedly at the NVIDIA splash screen to open UEFI setup, then go to Device Manager \> NVIDIA Configuration \> L4T Configuration. Set L4T Boot Mode to Kernel Partition, check that OS chain A status is Normal, then F10 and Y.

1. Reboot. The box will start in a degraded mode (no camera drivers). If a first boot setup screen shows up, just create a temporary user.

1. You should be able to read your NVMe from there, so feel free to copy anything important to a USB drive first.

1. Run `sudo dpkg --configure -a`

1. Reboot, go back to L4T Configuration and set L4T Boot Mode back to ExtLinux (F10, Y).

If it still shows a black screen after that, let me know and I’ll send you the next step.

Best,

Tristan Leduc

StereoLabs Support