# Synchronized Depth and Stereo RGB Topics/Images

**URL:** <https://community.stereolabs.com/t/synchronized-depth-and-stereo-rgb-topics-images/9588>\
**Category:** Software\
**Tags:** sdk, ros2\
**Created:** [August 3, 2025, 6:24pm UTC](https://community.stereolabs.com/t/synchronized-depth-and-stereo-rgb-topics-images/9588 "2025-08-03T18:24:56Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![jdcast](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/j/5f8ce5/32.png) [@jdcast](https://community.stereolabs.com/u/jdcast)\
**Post date:** [August 3, 2025, 6:24pm UTC](https://community.stereolabs.com/t/synchronized-depth-and-stereo-rgb-topics-images/9588/1 "2025-08-03T18:24:56Z")

</div>

I’m using multiple zed camera systems with gsml2. One utilizes two zed x mini cameras. Another uses a stereo pair of zed x one cameras (potentially more than two in the future). I’ve been referencing this [thread](https://community.stereolabs.com/t/zedx-synchronization-advantages/3521) and this [thread](https://community.stereolabs.com/t/zed-x-hardware-synchronization/7433).

For each of these systems, I’m trying to understand whether the depth and rgb images produced by the ZED SDK should be synchronized when they are emitted and how close those timestamps should be expected to be. I’m considering the following two scenarios:

1. Depth and rgb image topics coming from the zed\_wrapper (either live or via svo2 file replay)
2. Depth and rgb images via the ZED\_Depth\_Viewer.

Regarding the ZED\_Depth\_Viewer, I notice that when I use two zed x one cameras configured in a stereo pair, and then view them in ZED\_Depth\_Viewer, the depth image says it publishes at one frame frame rate (e.g. 9-10hz) while the images publish at another (e.g. 15hz).

Ultimately, for the systems I’ve mentioned, should I expect depth and rgb images/topics to be synchronized in the zed\_wrapper and the ZED\_Depth\_Viewer?  
If so, how close should their timestamps be in the two cases above?

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [August 4, 2025, 1:30pm UTC](https://community.stereolabs.com/t/synchronized-depth-and-stereo-rgb-topics-images/9588/2 "2025-08-04T13:30:42Z")

</div>

> [@jdcast](#):
>
> Regarding the ZED\_Depth\_Viewer, I notice that when I use two zed x one cameras configured in a stereo pair, and then view them in ZED\_Depth\_Viewer, the depth image says it publishes at one frame frame rate (e.g. 9-10hz) while the images publish at another (e.g. 15hz).

ZED Depth Viewer shows the grab rate (15 Hz) and the depth processing rate (9/10 Hz), but this does not mean that they are published at different rates, they are always synchronized and published at the depth rate.

> [@jdcast](#):
>
> If so, how close should their timestamps be in the two cases above?

Two frames to be synchronized must have a timestamp difference minor than the grab period = 1/grab\_rate.