# Sync multi cameras

**URL:** <https://community.stereolabs.com/t/sync-multi-cameras/10249>\
**Category:** ZED Mini\
**Tags:** jetson\
**Created:** [October 29, 2025, 11:00am UTC](https://community.stereolabs.com/t/sync-multi-cameras/10249 "2025-10-29T11:00:32Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![wangchunyi120](https://community.stereolabs.com/user_avatar/community.stereolabs.com/wangchunyi120/32/5024_2.png) [@wangchunyi120](https://community.stereolabs.com/u/wangchunyi120)\
**Post date:** [October 29, 2025, 11:00am UTC](https://community.stereolabs.com/t/sync-multi-cameras/10249/1 "2025-10-29T11:00:32Z")

</div>

Hello there,

I have two ZEDX MINI cameras and a Orin AGX and a capture card quad; and I want to sync these two cameras .

I read all documents and SDK Readmes, I am still confused about the sync method.

Here is my questions:

1、How can I use a Trigger signal to trigger the two cameras? I read this page,[ZED Link Mono GPIO Triggering - Stereolabs](https://www.stereolabs.com/docs/embedded/zed-link/zed-link-mono-triggering), But it says the function is not available now? When Can I use this mode? When it can be used, Can I randomly set the trigger signal? Like 1-30fps continuously adjustable?

2、If I use the sync method like this page shows :[GitHub - stereolabs/zed-multi-camera: ZED SDK sample with multiple ZEDs](https://github.com/stereolabs/zed-multi-camera/blob/master), what is the laggest latency between the two cameras?

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [November 4, 2025, 6:52pm UTC](https://community.stereolabs.com/t/sync-multi-cameras/10249/2 "2025-11-04T18:52:03Z")

</div>

Hi @wangchunyi120  
All the cameras that are connected to the same 4-wire GMSL2 port are natively hardware synchronized. You must not enable synchronization.

On the ZED Link Quad, you must enable synchronization only if you connect cameras to the two different 4-wire ports.  
Read more here:

> **[ZED Link Quad on AGX Orin - Stereolabs](https://www.stereolabs.com/docs/embedded/zed-link/quad-jetson-orin-agx-devkit-setup#enable-full-8-camera-onboard-synchronization)**
>
> This tutorial will help you set up the ZED Link Quad GMSL2 capture card, and use the Stereolabs GMSL2 cameras with the NVIDIA® Jetson™ Orin AGX Developer Kits.

The synchronization accuracy is 15 µsec