# Simulated ZED X IMU data missing from SVO2 recordings in Isaac Sim

**URL:** <https://community.stereolabs.com/t/simulated-zed-x-imu-data-missing-from-svo2-recordings-in-isaac-sim/11829>\
**Category:** Software\
**Tags:** sdk\
**Created:** [October 30, 2026, 5:27pm UTC](https://community.stereolabs.com/t/simulated-zed-x-imu-data-missing-from-svo2-recordings-in-isaac-sim/11829 "2026-10-30T17:27:36Z")\
**Posts on this page:** 5\
**Page:** 1

<div class="post-metadata">

**Author:** ![mani](https://community.stereolabs.com/user_avatar/community.stereolabs.com/mani/32/6558_2.png) [@mani](https://community.stereolabs.com/u/mani)\
**Post date:** [October 30, 2026, 5:27pm UTC](https://community.stereolabs.com/t/simulated-zed-x-imu-data-missing-from-svo2-recordings-in-isaac-sim/11829/1 "2026-10-30T17:27:36Z")

</div>

I am working on a visual odometry (VO) and visual-inertial odometry (VIO) evaluation project using a simulated ZED X camera in NVIDIA Isaac Sim, integrated with the ZED ROS 2 Wrapper.

My goal is to record one SVO2 dataset containing both stereo images and simulated IMU measurements, and then replay the same dataset twice:

- VO: `pos_tracking_mode: GEN_1`, `imu_fusion: false`
- VIO: `pos_tracking_mode: GEN_1`, `imu_fusion: true`

I would like to compare both estimated trajectories against Isaac Sim ground truth under identical sensor inputs.

**Environment:**

- Camera: Simulated ZED X
- ZED SDK: 5.5.0
- ROS 2: Jazzy
- Simulator: NVIDIA Isaac Sim
- Integration: ZED Isaac Sim extension + ZED ROS 2 Wrapper
- SVO format: SVO2
- Camera resolution: 960 × 600
- Camera frame rate: 30 FPS

**What works:**

I can successfully run positional tracking in Isaac Sim with:

```auto
pos_tracking:
    pos_tracking_enabled: true
    pos_tracking_mode: 'GEN_1'
    imu_fusion: true

sensors:
    sensors_image_sync: false
    sensors_pub_rate: 100.0
    publish_imu: true

```

The ZED Wrapper publishes both odometry and IMU measurements.

For example, a ROS 2 bag recorded during one simulation run contains:

```auto
Duration: 6.83 seconds

/clock 206 messages
/zed/ground_truth/pose 204 messages
/zed/zed_node/odom 183 messages
/zed/zed_node/imu/data 145 messages

```

Therefore, simulated IMU measurements are available through the ROS 2 interface, and live positional tracking works with IMU fusion enabled using GEN\_1.

**The problem:**

When I record an SVO2 file from the simulated camera using the ZED ROS 2 Wrapper’s `/zed/zed_node/start_svo_rec` service, the resulting file contains stereo frames but no IMU measurements.

Running:

```auto
ZED_SVO_Editor -inf recordings/T_GEN1_IMU_test.svo2

```

produces:

```auto
[ZED][WARNING] [Init]
No inertial data was found in this SVO.
Certain modules may operate with reduced accuracy as a result.

SVO Infos: SVO v 2
Image Size: [960 x 600]
Framerate: 30
Number of Frames: 207
Camera model: ZED X
ZED SDK version: 5.5.0

```

I also tested recording directly through the ROS 2 service, without using my Python recording script:

```auto
ros2 service call /zed/zed_node/start_svo_rec \
  zed_msgs/srv/StartSvoRec \
  "{svo_filename: '/path/to/test.svo2', compression_mode: 5}"

```

The resulting SVO2 file again contained stereo images but no inertial data.

During SVO playback with IMU fusion enabled, the SDK reports that no IMU data is available in the source.

**My questions:**

1. Does the ZED Isaac Sim integration currently support recording simulated IMU measurements into SVO2 files?
2. If supported, is there any additional SDK configuration, Isaac Sim extension setting, or recording option required to include IMU data?
3. Why can the ZED ROS 2 Wrapper publish simulated IMU measurements during live operation, while the same measurements are missing from the SVO2 recording?
4. Is this a known limitation or issue with the simulated camera stream or ZED SDK 5.5.0?
5. Is there a recommended workflow for recording a simulated stereo + IMU dataset once and then evaluating the native ZED SDK VO and VIO algorithms on that exact same dataset?

I have read the [Stereolabs](https://www.stereolabs.com/) documentation explaining that SVO2 files can store IMU measurements and that positional tracking can be enabled during playback even when it was disabled during recording.

I would like to know whether this functionality is also supported when the source is a simulated ZED X camera in Isaac Sim rather than a physical ZED camera.

Thank you very much for your help!

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [October 30, 2026, 5:37pm UTC](https://community.stereolabs.com/t/simulated-zed-x-imu-data-missing-from-svo2-recordings-in-isaac-sim/11829/2 "2026-10-30T17:37:22Z")

</div>

Hi @mani,  
Welcome to the [StereoLabs](https://www.stereolabs.com/) community and thank you for the detailed report.

> [@mani](#):
>
> 1. Does the ZED Isaac Sim integration currently support recording simulated IMU measurements into SVO2 files?

Yes. IMU data received from the Isaac Sim stream is expected to be stored in SVO2 recordings of that stream; the [ZED Isaac Sim extension v5.3.1 release notes](https://github.com/stereolabs/zed-isaac-sim/releases/tag/v5.3.1) explicitly compare the IMU orientation returned live and from SVOs recorded from the stream.

> [@mani](#):
>
> 1. If supported, is there any additional SDK configuration, Isaac Sim extension setting, or recording option required to include IMU data?

No additional setting is required. On the Isaac Sim side, the camera IMU must provide readings (`Rigid Body Enabled` ticked and `Imu_Sensor` enabled), and this seems to be already the case since the wrapper publishes IMU data.

> [@mani](#):
>
> 1. Why can the ZED ROS 2 Wrapper publish simulated IMU measurements during live operation, while the same measurements are missing from the SVO2 recording?
> 2. Is this a known limitation or issue with the simulated camera stream or ZED SDK 5.5.0?

This is not a known limitation, so we must isolate where the inertial data is lost. Can you please share:

- the Isaac Sim and ZED Isaac Sim extension versions
- the ZED ROS 2 Wrapper version or commit
- a short SVO2 file showing the problem

It would also help to know whether an SVO2 recorded directly with the ZED SDK from the same stream (`InitParameters.set_from_stream` plus `enable_recording`) contains inertial data; this tells us whether the issue is in the wrapper or upstream.

I also recommend upgrading to the latest [ZED SDK v5.5.1](https://www.stereolabs.com/developers/release) and to the extension v5.3.1. The latter fixes GEN\_1 positional tracking with IMU fusion inverting the camera pitch, both in streams and in SVOs recorded from them, which would directly affect your VIO evaluation.

> [@mani](#):
>
> 1. Is there a recommended workflow for recording a simulated stereo + IMU dataset once and then evaluating the native ZED SDK VO and VIO algorithms on that exact same dataset?

Your workflow is correct: record a single SVO2, then replay it twice with the ZED ROS 2 Wrapper using the `svo_path` launch argument, changing only `pos_tracking.imu_fusion`. Keep `svo.svo_realtime: false` (default) so that every frame is processed in both runs and the two trajectories are comparable.

---

<div class="post-metadata">

**Author:** ![mani](https://community.stereolabs.com/user_avatar/community.stereolabs.com/mani/32/6558_2.png) [@mani](https://community.stereolabs.com/u/mani)\
**Post date:** [November 3, 2026, 6:47am UTC](https://community.stereolabs.com/t/simulated-zed-x-imu-data-missing-from-svo2-recordings-in-isaac-sim/11829/3 "2026-11-03T06:47:39Z")

</div>

Hello,

Thank you for your previous suggestions.

I have completed several additional tests to investigate why simulated ZED X IMU data is missing from SVO2 recordings.

My setup is:

- NVIDIA Isaac Sim 6.1.0

- ZED Isaac Sim extension 5.2.1

- ZED SDK 5.5.0

- ZED ROS 2 wrapper 5.5.0

- ROS 2 Jazzy

I confirmed that the simulated IMU sensor is enabled and that the parent robot `base_link` has Rigid Body enabled. The ZED OmniGraph camera node uses the default streaming port, transport mode BOTH, camera model ZED\_X, and 30 FPS.

I also bypassed the ROS 2 wrapper’s recording service and recorded an SVO2 file directly through the ZED Python SDK using `sl.Camera.open()` and `enable_recording()`.

Unfortunately, the resulting SVO2 still contains no IMU data. `ZED_SVO_Editor -inf` reports:

`No inertial data was found in this SVO.`

Additional SDK tests showed the following:

- `get_sensors_data(TIME_REFERENCE.IMAGE)`: SUCCESS, with changing IMU values and timestamps.

- `get_sensors_data(TIME_REFERENCE.CURRENT)`: INVALID FUNCTION PARAMETERS.

- `get_sensors_data_batch()`: INVALID FUNCTION PARAMETERS.

- I tested both local IPC and network streaming connections, with the same results.

- The SDK logs `Backward compatibility required` when connecting to the simulated stream.

This suggests that IMU data is available through image-synchronized sensor access, but the other sensor retrieval methods are not functioning with this simulated stream.

Could you please clarify:

1. Is this behavior expected with ZED Isaac Sim extension 5.2.1 and ZED SDK 5.5.0?

2. Could it explain why IMU data is not stored in SVO2 recordings?

3. Is there a configuration change or targeted fix that would allow us to resolve this issue without upgrading the entire Isaac Sim extension?

I would prefer to preserve the existing working simulation setup if possible.

Thank you for your help.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [November 4, 2026, 10:16am UTC](https://community.stereolabs.com/t/simulated-zed-x-imu-data-missing-from-svo2-recordings-in-isaac-sim/11829/4 "2026-11-04T10:16:57Z")

</div>

The fix should be available with the ZED SDK v5.6 that will be released in a few days.

Can you please send me an SVO to [support@stereolabs.com](mailto:support@stereolabs.com) so we can validate the fix with it?  
Please cite this discussion in the email

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [November 6, 2026, 2:42pm UTC](https://community.stereolabs.com/t/simulated-zed-x-imu-data-missing-from-svo2-recordings-in-isaac-sim/11829/5 "2026-11-06T14:42:36Z")

</div>

Hi @mani  
Thank you for the SVO file that you shared.  
I confirm that the IMU data is available when using the ZED SDK v5.6 that will be released before the end of the next week.

**NOTE:** when recording an SVO with simulated data, the behavior is the same as the old SVO v1. The IMU is not generated/recorded at high frequency, but at the same frequency of frame recording.