# Sharing a Solution: ZED Camera Python API Issue with Microsoft Store Python

**URL:** <https://community.stereolabs.com/t/sharing-a-solution-zed-camera-python-api-issue-with-microsoft-store-python/9373>\
**Category:** Software\
**Tags:** python, zed-sdk\
**Created:** [July 13, 2025, 4:09am UTC](https://community.stereolabs.com/t/sharing-a-solution-zed-camera-python-api-issue-with-microsoft-store-python/9373 "2025-07-13T04:09:53Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![seungjuchoi](https://community.stereolabs.com/user_avatar/community.stereolabs.com/seungjuchoi/32/3108_2.png) [@seungjuchoi](https://community.stereolabs.com/u/seungjuchoi)\
**Post date:** [July 13, 2025, 4:09am UTC](https://community.stereolabs.com/t/sharing-a-solution-zed-camera-python-api-issue-with-microsoft-store-python/9373/1 "2025-07-13T04:09:53Z")

</div>

Hi everyone,

I’d like to share a solution I discovered after spending a significant amount of time troubleshooting a persistent issue with the ZED camera Python API. I hope this helps others facing similar problems. For reference, here’s the official installation guide:

> **[Install the ZED Python API - Stereolabs](https://www.stereolabs.com/docs/app-development/python/install)**
>
> This section explains how to use the ZED SDK in Python 3 on Windows and Linux platforms.

**Background**

I was preparing for large-scale data collection using ZED cameras as labels, and it was critical to get everything running on a specific laptop. However, I encountered a problem where the skeleton (body tracking) would not appear in our data collection program—only the video feed was visible.

To narrow down the issue, I ran the official sample programs and consistently encountered errors. When this error occurred, the model would fail to download, and only RGB output would appear—no skeleton detection.

 ![image](https://community.stereolabs.com/uploads/default/original/2X/7/7092c7e18f90a1c25049ec62275efef1352bfdc8.png)

Relevant ticket: [Cudnn not found and AI Models not optimized](https://community.stereolabs.com/t/cudnn-not-found-and-ai-models-not-optimized/1694)

This issue wasn’t limited to body tracking; it caused broader problems with the SDK as well.

**Troubleshooting Attempts**

I tried the following combinations in an attempt to resolve the issue:

- ZED SDK versions: 4.0.8, 4.1.4, 4.2.5, 5.0.1
- CUDA versions: 11.8, 12.1, 12.8
- Various cuDNN installations

Despite these efforts, the problem persisted.

**Key Discovery**

By chance, I heard that things worked with Python 3.8.10, so I gave it a try—and it worked! Upon further investigation, I realized the crucial factor: **do not use the Python version from the Microsoft Store**.

**Solution**

- Avoid installing Python via the Microsoft Store.
- Instead, download and install Python directly from the official website ([python.org](http://python.org)) or use a package manager like uv, pyenv, or conda.

**Problematic Scenario**

- Installing Python 3.10 from the Microsoft Store results in version 3.10.11.
- Running the ZED SDK sample with this version consistently triggers the described errors.

I personally use uv, and pinning to Python 3.10.11 connects immediately. However, the issue is reproducible even without uv. I started using uv to quickly resolve the problem with 100% reliability.

**Summary**

If you’re experiencing issues with ZED SDK and Python—especially with skeleton/body tracking—check your Python installation source. Avoid the Microsoft Store version and use a direct download or a reliable package manager instead. Adding this note to the official documentation could help many others avoid similar headaches.

Hope this saves someone else some time!