# Sender/Receiver example fails on Jetson Orin Nano w/ZED SDK 5.4.1

**URL:** <https://community.stereolabs.com/t/sender-receiver-example-fails-on-jetson-orin-nano-w-zed-sdk-5-4-1/11715>\
**Category:** Python\
**Tags:** sdk, jetson\
**Created:** [September 14, 2026, 5:06pm UTC](https://community.stereolabs.com/t/sender-receiver-example-fails-on-jetson-orin-nano-w-zed-sdk-5-4-1/11715 "2026-09-14T17:06:08Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![cata](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/c/ecb155/32.png) [@cata](https://community.stereolabs.com/u/cata)\
**Post date:** [September 14, 2026, 5:06pm UTC](https://community.stereolabs.com/t/sender-receiver-example-fails-on-jetson-orin-nano-w-zed-sdk-5-4-1/11715/1 "2026-09-14T17:06:09Z")

</div>

Hi!  
I’m trying to setup the single streamer /receiver example from **ZED SDK 5.4.1** on a **Jetson Orin Nano Developer Kit 8GB** using a ZED X paired with a ZED Link Duo capture card.

However, I’m facing some problems.  
Even though I can ping the machine and the stream starts successfully:

```bash
ubuntu@ubuntu:/usr/local/zed/samples/camera streaming/receiver/python$ ping 192.168.1.103

PING 192.168.1.103 (192.168.1.103) 56(84) bytes of data.

64 bytes from 192.168.1.103: icmp_seq=1 ttl=64 time=0.410 ms

64 bytes from 192.168.1.103: icmp_seq=2 ttl=64 time=0.293 ms

^C

--- 192.168.1.103 ping statistics ---

2 packets transmitted, 2 received, 0% packet loss, time 1039ms

rtt min/avg/max/mdev = 0.293/0.351/0.410/0.058 ms

ubuntu@ubuntu:/usr/local/zed/samples/camera streaming/single_sender/python$ python3 streaming_sender.py 
[Sample] Using default resolution
[2026-09-14 12:08:50 UTC][ZED][INFO] Logging level INFO
[2026-09-14 12:08:51 UTC][ZED][INFO] Using GMSL input... Switched to default resolution HD1200
[2026-09-14 12:08:51 UTC][ZED][INFO] [Init] Camera FW version: 2001
[2026-09-14 12:08:51 UTC][ZED][INFO] [Init] Video mode: HD1200@30
[2026-09-14 12:08:51 UTC][ZED][INFO] [Init] Serial Number: S/N 40081464
[2026-09-14 12:08:51 UTC][ZED][INFO] [Init] Depth mode selected: NEURAL. Ensure this mode matches your application's performance and accuracy requirements. See https://www.stereolabs.com/docs/depth-sensing/depth-modes for help.
Streaming on port 30000
[ZED][Streaming] Use Transport layer mode : 0

```

On the receiver side i get:  
`ubuntu@ubuntu:/usr/local/zed/samples/camera streaming/receiver/python$ python streaming_receiver.py --ip_address 192.168.1.103:30000`  
`[2026-09-14 12:25:11 UTC][ZED][INFO] Logging level INFO`  
`[Streaming] Warning: Failed to retrieve camera settings from sender`  
`[Streaming] Error: Stream Opening returned TIMEOUT (5000 ms)`  
`[Streaming] Incorrect metadata size. Expecting: 2904 got -1. Skipping.`  
`[2026-09-14 12:25:18 UTC][ZED][ERROR] FAILURE in sl::ERROR_CODE sl:` 📷`:open(sl::InitParameters)`  
`Camera Open : FAILURE. Exit program.`

This communication error remain even if I use ZED Explorer as receiver, both in the same or a different machine.

NOTE: ZED Diagnostic shows no problem, everything is fine and all checks are passed

---

<div class="post-metadata">

**Author:** ![IKEDA](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/i/dec6dc/32.png) [@IKEDA](https://community.stereolabs.com/u/IKEDA)\
**Post date:** [November 4, 2026, 10:17am UTC](https://community.stereolabs.com/t/sender-receiver-example-fails-on-jetson-orin-nano-w-zed-sdk-5-4-1/11715/2 "2026-11-04T10:17:34Z")

</div>

````auto
We are seeing exactly the same issue with ZED SDK 5.5.1.

Setup: ZED Box Mini (Jetson Orin Nano 4GB, L4T 36.4.4 / JetPack 6.2.1),
ZED X Nano (GMSL2), receiver on an x86 PC with SDK 5.5.1.

Sender (official C++ single_sender sample, unmodified):

```
[ZED][Streaming] Use Transport layer mode : 0
[ZED_SDK][Encoding] H265 hardware encoder not available, falling back to H264 CPU encoding
[Sample] Streaming on port 30000
```

"[Streaming] Streaming is now running...." is never printed. The receiver log is
identical to yours (Failed to retrieve camera settings / TIMEOUT 5000 ms /
Incorrect metadata size 2904 got -1).

What we checked:
- A receiver on the ZED Box itself (127.0.0.1) fails the same way, so it is not a
  network or receiver-side problem.
- Python sample, C++ sample and ZED Studio all behave the same.
- HD1200 / SVGA, 15 / 30 fps, H265 (auto fallback) / H264: same result.
- Only one libsl_zed.so on the system; calibration file is present.
- The sender binds UDP 30000/30001, but incoming requests stay unread in the
  socket receive queue.
- Note on the attached logs: the clocks are not synchronized (no NTP on the
  ZED Box, about 90 s ahead of the PC), and the PC log timestamps are labeled
  UTC but are actually local time (JST, UTC+9). Since the loopback test on the
  Box itself fails the same way, the clock offset should not be related.

It looks like the streaming server never finishes starting after the fallback to
the CPU encoder. Stereolabs team, could you confirm whether CPU-encoded
streaming is supported on Orin Nano with SDK 5.4.1 / 5.5.1, and if there is a
workaround?

Screenshot and logs attached.

````

 ![Screenshot_20261104_085620_masked](https://community.stereolabs.com/uploads/default/original/2X/3/3f88c51709062e04fc1d41ad6331b42efaa03cd6.png)

[receiver\_20261104\_085544.log](https://community.stereolabs.com/uploads/short-url/i7I78SmY7fHzrea84gStyOjKjw6.log) (394 Bytes)

[sender\_20261103\_235544.log](https://community.stereolabs.com/uploads/short-url/hERpUd5g6j2mjp4VNqbDATk8Jrb.log) (932 Bytes)