# \[ROS2 Wrapper\] 4 ZED2i cameras same device in docker container

**URL:** <https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246>\
**Category:** ROS2\
**Tags:** multi-camera, ros, docker, jetson\
**Created:** [March 14, 2023, 12:58pm UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246 "2023-03-14T12:58:22Z")\
**Posts on this page:** 20\
**Page:** 1

<div class="post-metadata">

**Author:** ![otstanteplz](https://community.stereolabs.com/user_avatar/community.stereolabs.com/otstanteplz/32/1080_2.png) [@otstanteplz](https://community.stereolabs.com/u/otstanteplz)\
**Post date:** [March 14, 2023, 12:58pm UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/1 "2023-03-14T12:58:22Z")

</div>

Hi,

I have 4 ZED2i connected on the device via USB3.0 separate controllers, but when i`m trying to launch them i see that only 2 got recognized. If i remove serial numbers from launch file, i steal see only 2 cameras, but with that appears warning that says LOW USB BANDWIDTH. Can you help me to connect all 4 of them?

---

<div class="post-metadata">

**Author:** ![pixml](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/bbce88/32.png) [@pixml](https://community.stereolabs.com/u/pixml)\
**Post date:** [March 14, 2023, 1:19pm UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/2 "2023-03-14T13:19:08Z")

</div>

Hi all! I’ll add some info to previous post.  
So, i’ve already asked about usb bandwidth [here](https://community.stereolabs.com/t/motherboard-selection/2112), and now we have 2 different PCIe expansion cards. Each has 2 ZED2i cameras, so, as i understand - it shouldnt be usn brandwidth issue  
We tried to run in different modes (VGA@15, 720@15), but all 4 are not running at the same time.  
If we have serial numbers in launch file - we see log1.txt, if we remove them - we can see log2.txt  
[log2.txt](https://community.stereolabs.com/uploads/short-url/22ows5FQMN7k4xzsGaP9mISlHnP.txt) (118.6 KB)  
[log1.txt](https://community.stereolabs.com/uploads/short-url/ksBBuf0rMKnEJX4zLtRjRa5gndS.txt) (94.3 KB)  
Moreover, when I just access cameras via python - all cameras are available  
But as soon as we start testing inside ros&docker, they turn off one by one (python sdk does not see them, but “v4l2-ctl --list-devices” show them

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [March 14, 2023, 4:02pm UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/3 "2023-03-14T16:02:20Z")

</div>

Hi @pixml and @otstanteplz  
do the camera connect if you try to start the 4 nodes separately?  
We do not suggest connecting 2 cameras to the same USB3 channel? Are the 4 cameras connected to 4 different channels?  
Can you post the output of the command `$ lsusb -t -v`?

---

<div class="post-metadata">

**Author:** ![pixml](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/bbce88/32.png) [@pixml](https://community.stereolabs.com/u/pixml)\
**Post date:** [March 14, 2023, 7:58pm UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/4 "2023-03-14T19:58:56Z")

</div>

Thanks for quick response!  
About 4 nodes separately @otstanteplz will answer tomorrow.  
If I understand you correctly, usb3 channel is equal to usb controller, so we have 2 PCI Expansion cards == we have 2 controllers/channels  
First PCI Expansion card connected with 1 and 2 Zed2i cameras, and second connected to 3 and 4 Zed2i cameras  
We understand that it would be better to have a controller for each camera, but in the [previously we discussed](https://community.stereolabs.com/t/motherboard-selection/2112/4) that the 2 cameras per expansion card should work…  
Output of` lsusb -t -v`

> /: Bus 10.Port 1: Dev 1, Class=root\_hub, Driver=xhci\_hcd/4p, 5000M  
> ID 1d6b:0003 Linux Foundation 3.0 root hub  
> |\_\_ Port 2: Dev 2, If 0, Class=Hub, Driver=hub/1p, 5000M  
> ID 2109:0211 VIA Labs, Inc.  
> |\_\_ Port 1: Dev 4, If 0, Class=Hub, Driver=hub/1p, 5000M  
> ID 2109:0211 VIA Labs, Inc.  
> |\_\_ Port 1: Dev 6, If 1, Class=Video, Driver=uvcvideo, 5000M  
> ID 2b03:f880  
> |\_\_ Port 1: Dev 6, If 0, Class=Video, Driver=uvcvideo, 5000M  
> ID 2b03:f880  
> |\_\_ Port 4: Dev 3, If 0, Class=Hub, Driver=hub/1p, 5000M  
> ID 2109:0211 VIA Labs, Inc.  
> |\_\_ Port 1: Dev 5, If 0, Class=Video, Driver=uvcvideo, 5000M  
> ID 2b03:f880  
> |\_\_ Port 1: Dev 5, If 1, Class=Video, Driver=uvcvideo, 5000M  
> ID 2b03:f880  
> /: Bus 09.Port 1: Dev 1, Class=root\_hub, Driver=xhci\_hcd/4p, 480M  
> ID 1d6b:0002 Linux Foundation 2.0 root hub  
> |\_\_ Port 1: Dev 2, If 0, Class=Video, Driver=uvcvideo, 480M  
> ID 0ac8:3500 Z-Star Microelectronics Corp.  
> |\_\_ Port 1: Dev 2, If 1, Class=Video, Driver=uvcvideo, 480M  
> ID 0ac8:3500 Z-Star Microelectronics Corp.  
> |\_\_ Port 1: Dev 2, If 2, Class=Audio, Driver=snd-usb-audio, 480M  
> ID 0ac8:3500 Z-Star Microelectronics Corp.  
> |\_\_ Port 1: Dev 2, If 3, Class=Audio, Driver=snd-usb-audio, 480M  
> ID 0ac8:3500 Z-Star Microelectronics Corp.  
> |\_\_ Port 2: Dev 3, If 0, Class=Hub, Driver=hub/4p, 480M  
> ID 2109:2211 VIA Labs, Inc.  
> |\_\_ Port 1: Dev 8, If 0, Class=Hub, Driver=hub/4p, 480M  
> ID 2109:2211 VIA Labs, Inc.  
> |\_\_ Port 1: Dev 9, If 0, Class=Hub, Driver=hub/2p, 480M  
> ID 0424:2512 Microchip Technology, Inc. (formerly SMSC) USB 2.0 Hub  
> |\_\_ Port 2: Dev 11, If 0, Class=Human Interface Device, Driver=, 12M  
> ID 2b03:f881  
> |\_\_ Port 4: Dev 4, If 0, Class=Hub, Driver=hub/4p, 480M  
> ID 2109:2211 VIA Labs, Inc.  
> |\_\_ Port 1: Dev 5, If 0, Class=Hub, Driver=hub/2p, 480M  
> ID 0424:2512 Microchip Technology, Inc. (formerly SMSC) USB 2.0 Hub  
> |\_\_ Port 2: Dev 7, If 0, Class=Human Interface Device, Driver=, 12M  
> ID 2b03:f881  
> /: Bus 08.Port 1: Dev 1, Class=root\_hub, Driver=xhci\_hcd/4p, 5000M  
> ID 1d6b:0003 Linux Foundation 3.0 root hub  
> |\_\_ Port 1: Dev 2, If 0, Class=Hub, Driver=hub/1p, 5000M  
> ID 2109:0211 VIA Labs, Inc.  
> |\_\_ Port 1: Dev 4, If 0, Class=Video, Driver=uvcvideo, 5000M  
> ID 2b03:f880  
> |\_\_ Port 1: Dev 4, If 1, Class=Video, Driver=uvcvideo, 5000M  
> ID 2b03:f880  
> |\_\_ Port 3: Dev 3, If 0, Class=Hub, Driver=hub/1p, 5000M  
> ID 2109:0211 VIA Labs, Inc.  
> |\_\_ Port 1: Dev 5, If 0, Class=Video, Driver=uvcvideo, 5000M  
> ID 2b03:f880  
> |\_\_ Port 1: Dev 5, If 1, Class=Video, Driver=uvcvideo, 5000M  
> ID 2b03:f880  
> /: Bus 07.Port 1: Dev 1, Class=root\_hub, Driver=xhci\_hcd/1p, 480M  
> ID 1d6b:0002 Linux Foundation 2.0 root hub  
> |\_\_ Port 1: Dev 2, If 0, Class=Hub, Driver=hub/4p, 480M  
> ID 2109:3431 VIA Labs, Inc. Hub  
> |\_\_ Port 1: Dev 3, If 0, Class=Hub, Driver=hub/4p, 480M  
> ID 2109:2211 VIA Labs, Inc.  
> |\_\_ Port 1: Dev 5, If 0, Class=Hub, Driver=hub/2p, 480M  
> ID 0424:2512 Microchip Technology, Inc. (formerly SMSC) USB 2.0 Hub  
> |\_\_ Port 2: Dev 6, If 0, Class=Human Interface Device, Driver=usbhid, 12M  
> ID 2b03:f881  
> |\_\_ Port 3: Dev 4, If 0, Class=Hub, Driver=hub/4p, 480M  
> ID 2109:2211 VIA Labs, Inc.  
> |\_\_ Port 1: Dev 7, If 0, Class=Hub, Driver=hub/2p, 480M  
> ID 0424:2512 Microchip Technology, Inc. (formerly SMSC) USB 2.0 Hub  
> |\_\_ Port 2: Dev 8, If 0, Class=Human Interface Device, Driver=, 12M  
> ID 2b03:f881  
> /: Bus 06.Port 1: Dev 1, Class=root\_hub, Driver=xhci\_hcd/4p, 10000M  
> ID 1d6b:0003 Linux Foundation 3.0 root hub  
> /: Bus 05.Port 1: Dev 1, Class=root\_hub, Driver=xhci\_hcd/2p, 480M  
> ID 1d6b:0002 Linux Foundation 2.0 root hub  
> /: Bus 04.Port 1: Dev 1, Class=root\_hub, Driver=xhci\_hcd/2p, 5000M  
> ID 1d6b:0003 Linux Foundation 3.0 root hub  
> /: Bus 03.Port 1: Dev 1, Class=root\_hub, Driver=xhci\_hcd/10p, 480M  
> ID 1d6b:0002 Linux Foundation 2.0 root hub  
> |\_\_ Port 1: Dev 2, If 0, Class=Human Interface Device, Driver=usbhid, 12M  
> ID 062a:4101 MosArt Semiconductor Corp. Wireless Keyboard/Mouse  
> |\_\_ Port 1: Dev 2, If 1, Class=Human Interface Device, Driver=usbhid, 12M  
> ID 062a:4101 MosArt Semiconductor Corp. Wireless Keyboard/Mouse  
> |\_\_ Port 8: Dev 3, If 0, Class=Vendor Specific Class, Driver=pl2303, 12M  
> ID 067b:2303 Prolific Technology, Inc. PL2303 Serial Port  
> |\_\_ Port 10: Dev 4, If 0, Class=Mass Storage, Driver=ums-realtek, 480M  
> ID 0bda:0153 Realtek Semiconductor Corp. 3-in-1 (SD/SDHC/SDXC) Card Reader  
> /: Bus 02.Port 1: Dev 1, Class=root\_hub, Driver=ehci-pci/2p, 480M  
> ID 1d6b:0002 Linux Foundation 2.0 root hub  
> |\_\_ Port 1: Dev 2, If 0, Class=Hub, Driver=hub/6p, 480M  
> ID 8087:8000 Intel Corp.  
> /: Bus 01.Port 1: Dev 1, Class=root\_hub, Driver=ehci-pci/2p, 480M  
> ID 1d6b:0002 Linux Foundation 2.0 root hub  
> |\_\_ Port 1: Dev 2, If 0, Class=Hub, Driver=hub/4p, 480M  
> ID 8087:8008 Intel Corp.

---

<div class="post-metadata">

**Author:** ![otstanteplz](https://community.stereolabs.com/user_avatar/community.stereolabs.com/otstanteplz/32/1080_2.png) [@otstanteplz](https://community.stereolabs.com/u/otstanteplz)\
**Post date:** [March 15, 2023, 7:08am UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/5 "2023-03-15T07:08:28Z")

</div>

Hi, I tried run them separately, launch order doesn’t matter, it always one camera with same serial number that doesn’t work. I tried run this serial number first, but result is still the same

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [March 15, 2023, 8:27am UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/6 "2023-03-15T08:27:34Z")

</div>

According to the device tree the 4 cameras are all connected to the Bus 10, one on the Port 4, the remaining 3 to the Port 1.  
Are you using hubs?

---

<div class="post-metadata">

**Author:** ![pixml](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/bbce88/32.png) [@pixml](https://community.stereolabs.com/u/pixml)\
**Post date:** [March 15, 2023, 9:03am UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/7 "2023-03-15T09:03:47Z")

</div>

Well, I’m not very good at hardware, but as i understand:

1. 4 cameras are all connected to the Bus 10, but two of them connected to the Port4, two of them connected to the Port2  
 ![Снимок экрана 2023-03-15 в 12.59.20](https://community.stereolabs.com/uploads/default/original/2X/8/8138cefad03bc3790e05d72272f287ffbbe921c6.png)
2. We don’t use usb hubs, we use 2 PCI Expansion cards (this is [first](https://lanberg.pl/en/produkt/PCE-US3-004#img1), second is the same, but with 3.0 ports)

---

<div class="post-metadata">

**Author:** ![pixml](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/bbce88/32.png) [@pixml](https://community.stereolabs.com/u/pixml)\
**Post date:** [March 15, 2023, 9:51am UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/8 "2023-03-15T09:51:20Z")

</div>

I think i was wrong a bit  
I see same tree on bus 8:

 ![Снимок экрана 2023-03-15 в 13.48.51](https://community.stereolabs.com/uploads/default/original/2X/1/15e7a73b414f166c4a954331ce376661ce88a612.png)

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [March 15, 2023, 9:59am UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/9 "2023-03-15T09:59:19Z")

</div>

Yes, this seems correct, the problem is that 2x ZED 2i connected to the same bus channel can conflict.

Have you tried this configuration outside the docker container?

---

<div class="post-metadata">

**Author:** ![pixml](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/bbce88/32.png) [@pixml](https://community.stereolabs.com/u/pixml)\
**Post date:** [March 15, 2023, 10:01am UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/10 "2023-03-15T10:01:57Z")

</div>

So, i’m not sure, but it looks like this is not about ZED cameras, because `lsusb -d 2b03: -v` shows another info  
[log\_lsusb2b03.txt](https://community.stereolabs.com/uploads/short-url/4zZF4fVrwwdLUSuj40Miv9mv2Pu.txt) (73.5 KB)

And one more interesting thing  
If we pull out the unworked zed camera from usb port and then plug it back in same usb port, this zed camera can work, but then any other zed2i camera can turn off (even from another bus)

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [March 15, 2023, 10:07am UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/11 "2023-03-15T10:07:17Z")

</div>

The ZED 2i when connected to the USB port creates two devices:

- `2b03:f880` → UVC video module (USB3)
- `2b03:f881` → HID sensors data module (USB2)

The fact that when you connect one camera another one stops to work make me think that this is also a power issue.

@adujardin[already suggested](https://community.stereolabs.com/t/motherboard-selection/2112/4) to be sure that the expansion cards are correctly powered. Is the power configuration correct?

---

<div class="post-metadata">

**Author:** ![pixml](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/bbce88/32.png) [@pixml](https://community.stereolabs.com/u/pixml)\
**Post date:** [March 15, 2023, 10:12am UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/12 "2023-03-15T10:12:42Z")

</div>

We don’t use ROS inside docker, but i think we can try  
I will describe what a typical situation looks like:

1. We connected 4 cameras
2. We checked that we see them through Zed Explorer and python `sl.Camera.get_device_list()`
3. We are starting to test our ROS pipeline
4. In ROS only two or three cameras turn on
5. We stop ROS, look at the cameras through Zed Explorer or python and see only 2 or 3 cameras
6. Loop repeat

Yes, the cards must be powered, but I will ask our engineers to check again

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [March 15, 2023, 10:48am UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/13 "2023-03-15T10:48:59Z")

</div>

> [@pixml](#):
>
> We don’t use ROS inside docker, but i think we can try

@pixml the title of this thread is `4 ZED2i cameras same device in docker container`… please change it if it’s not correct

---

<div class="post-metadata">

**Author:** ![pixml](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/bbce88/32.png) [@pixml](https://community.stereolabs.com/u/pixml)\
**Post date:** [March 15, 2023, 11:09am UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/14 "2023-03-15T11:09:00Z")

</div>

Oh, my mistake, sorry  
I meant we don’t use ROS **outside** of docker, but we can try (as you suggested)

---

<div class="post-metadata">

**Author:** ![otstanteplz](https://community.stereolabs.com/user_avatar/community.stereolabs.com/otstanteplz/32/1080_2.png) [@otstanteplz](https://community.stereolabs.com/u/otstanteplz)\
**Post date:** [March 15, 2023, 8:32pm UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/15 "2023-03-15T20:32:51Z")

</div>

Upd I tried to run zed cameras separetly via default launch file and than run my own launch file which starts other nodes and this worked out, but when i trying to run all zeds via one launch file i’m facing issue with one camera missing.  
I’m attaching my launch file where i trying to launch all 4 cameras  
i don’t have enough permissions to attach files, so here link to gist [multiple\_zed2i.launch.py · GitHub](https://gist.github.com/otstanteplz/e2bc53cf91956d280a10a7f4499c69b5)

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [March 16, 2023, 5:56am UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/16 "2023-03-16T05:56:06Z")

</div>

Can you try to remove this line?

> <https://gist.github.com/otstanteplz/e2bc53cf91956d280a10a7f4499c69b5#file-multiple_zed2i-launch-py-L32>

The camera id is assigned by the OS, if camera id and serial number do not match you can have issues.

---

<div class="post-metadata">

**Author:** ![otstanteplz](https://community.stereolabs.com/user_avatar/community.stereolabs.com/otstanteplz/32/1080_2.png) [@otstanteplz](https://community.stereolabs.com/u/otstanteplz)\
**Post date:** [March 16, 2023, 7:07am UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/17 "2023-03-16T07:07:05Z")

</div>

Thank you, it worked like a charm  
Upd @Myzhar It workerd one time, when i tried launch second time after a while, the issue came back  
ZED Explorer stopped recognizing camera and suggesting to plug cam to another usb port, it goes away after turning off the power from this cam

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [March 16, 2023, 8:35am UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/18 "2023-03-16T08:35:54Z")

</div>

It is possible that for power issues the cameras are excluded by the USB3 controller.  
You can recover them by using the `sl::reboot` command with the S/N as the parameter.

A tip that you could use is to add a little delay (e.g. 1 second) between the different camera openings.

A curiosity, have you tried the launch file of our multi-camera tutorial?

> **[zed-ros2-examples/tutorials/zed\_multi\_camera at master ·...](https://github.com/stereolabs/zed-ros2-examples/tree/master/tutorials/zed_multi_camera)**
>
> master/tutorials/zed\_multi\_camera

---

<div class="post-metadata">

**Author:** ![otstanteplz](https://community.stereolabs.com/user_avatar/community.stereolabs.com/otstanteplz/32/1080_2.png) [@otstanteplz](https://community.stereolabs.com/u/otstanteplz)\
**Post date:** [March 16, 2023, 9:20am UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/19 "2023-03-16T09:20:07Z")

</div>

No, i have not tried yours launch, but i defently will and let you know the results

---

<div class="post-metadata">

**Author:** ![otstanteplz](https://community.stereolabs.com/user_avatar/community.stereolabs.com/otstanteplz/32/1080_2.png) [@otstanteplz](https://community.stereolabs.com/u/otstanteplz)\
**Post date:** [March 16, 2023, 1:10pm UTC](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246/20 "2023-03-16T13:10:41Z")

</div>

@Myzhar I tried your launch and the problem persists. But the reboot command helped, the only thing is that I can’t run it inside the container, i always getting FAILURE, but outside it works fine. The main idea, that i will reboot all my serials and then launch all nodes (it works if i reboot them outside of container). Can you help me with that? i tried to look in source code to understand why reboot returns FAILURE but cant find anything except this part [zed-python-api/sl\_c.pxd at master · stereolabs/zed-python-api · GitHub](https://github.com/stereolabs/zed-python-api/blob/master/src/pyzed/sl_c.pxd#L1427)

[Next page](https://community.stereolabs.com/t/ros2-wrapper-4-zed2i-cameras-same-device-in-docker-container/2246.md?page=2)