# ROS2 Humble ZED multi container dies frequently, Jetson AGX Orin 64gb, L4T 36.4.7, ZED SDK 5.1.1, 3 ZEDx Mini via Quad Capture Card   

**URL:** <https://community.stereolabs.com/t/ros2-humble-zed-multi-container-dies-frequently-jetson-agx-orin-64gb-l4t-36-4-7-zed-sdk-5-1-1-3-zedx-mini-via-quad-capture-card/10374>\
**Category:** Software\
**Tags:** jetson, ros2\
**Created:** [November 20, 2025, 4:43pm UTC](https://community.stereolabs.com/t/ros2-humble-zed-multi-container-dies-frequently-jetson-agx-orin-64gb-l4t-36-4-7-zed-sdk-5-1-1-3-zedx-mini-via-quad-capture-card/10374 "2025-11-20T16:43:48Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![Maximilian](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/m/d6d6ee/32.png) [@Maximilian](https://community.stereolabs.com/u/Maximilian)\
**Post date:** [November 20, 2025, 4:43pm UTC](https://community.stereolabs.com/t/ros2-humble-zed-multi-container-dies-frequently-jetson-agx-orin-64gb-l4t-36-4-7-zed-sdk-5-1-1-3-zedx-mini-via-quad-capture-card/10374/1 "2025-11-20T16:43:49Z")

</div>

Hi there,

Yesterday I flashed our Jetson and installed the newest NVIDIA Jetson Linux version 36.4.7 (Jetpack 6.2.1) with the newest ZED SDK 5.1.1. I am using ROS2 Humble and do ros2 launch zed\_multi\_camera zed\_multi\_camera.launch.py with corresponding arguments. Unfortunately, I frequently obtain the following error at the end of the launch / as soon as I subscribe to one of the published topics:

[ERROR] [component\_container\_isolated-1]: process has died [pid 16260, exit code -6, cmd ‘/opt/ros/humble/lib/rclcpp\_components/component\_container\_isolated --ros-args --log-level info --ros-args -r \_\_node:=zed\_multi\_container -r \_\_ns:=/zed\_multi’].

Thanks for your help!

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [November 20, 2025, 5:21pm UTC](https://community.stereolabs.com/t/ros2-humble-zed-multi-container-dies-frequently-jetson-agx-orin-64gb-l4t-36-4-7-zed-sdk-5-1-1-3-zedx-mini-via-quad-capture-card/10374/2 "2025-11-20T17:21:14Z")

</div>

Hi @Maximilian  
Welcome to the [Stereolabs](https://www.stereolabs.com/) community.

Please send me the content of the `common_stereo.yaml` parameter file

---

<div class="post-metadata">

**Author:** ![Maximilian](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/m/d6d6ee/32.png) [@Maximilian](https://community.stereolabs.com/u/Maximilian)\
**Post date:** [November 20, 2025, 5:35pm UTC](https://community.stereolabs.com/t/ros2-humble-zed-multi-container-dies-frequently-jetson-agx-orin-64gb-l4t-36-4-7-zed-sdk-5-1-1-3-zedx-mini-via-quad-capture-card/10374/3 "2025-11-20T17:35:01Z")

</div>

Hi Myzhar,

Thanks for your quick reply! Here is the content of my common\_stereo.yaml:

# config/common\_stereo.yaml

# Common parameters to [Stereolabs](https://www.stereolabs.com/) ZED Stereo cameras

* * *

/\*\*:  
ros\_\_parameters:  
use\_sim\_time: false # Set to `true` only if there is a publisher for the simulated clock to the `/clock` topic. Normally used in simulation mode.

```
    simulation:
        sim_enabled: false # Set to `true` to enable the simulation mode and connect to a simulation server
        sim_address: '127.0.0.1' # The connection address of the simulation server. See the documentation of the supported simulation plugins for more information.
        sim_port: 30000 # The connection port of the simulation server. See the documentation of the supported simulation plugins for more information.

    svo:
        use_svo_timestamps: true # Use the SVO timestamps to publish data. If false, data will be published at the system time.
        publish_svo_clock: false # [overwritten by launch file options] When use_svo_timestamps is true allows to publish the SVO clock to the `/clock` topic. This is useful for synchronous rosbag playback.
        svo_loop: false # Enable loop mode when using an SVO as input source. NOTE: ignored if SVO timestamping is used
        svo_realtime: false # if true the SVO will be played trying to respect the original framerate eventually skipping frames, otherwise every frame will be processed respecting the `pub_frame_rate` setting
        play_from_frame: 0 # Start playing the SVO from a specific frame
        replay_rate: 1.0 # Replay rate for the SVO when not used in realtime mode (between [0.10-5.0])

    general:
        camera_timeout_sec: 5
        camera_max_reconnect: 5
        camera_flip: false
        self_calib: true # Enable the self-calibration process at camera opening. See https://www.stereolabs.com/docs/api/structsl_1_1InitParameters.html#affeaa06cfc1d849e311e484ceb8edcc5
        serial_number: 0 # overwritten by launch file
        pub_resolution: 'NATIVE' # The resolution used for image and depth map publishing. 'NATIVE' to use the same `general.grab_resolution` - `CUSTOM` to apply the `general.pub_downscale_factor` downscale factory to reduce bandwidth in transmission
        pub_downscale_factor: 2.0 # rescale factor used to rescale image before publishing when 'pub_resolution' is 'CUSTOM'
        pub_frame_rate: 30.0 # [DYNAMIC] Frequency of publishing of visual images and depth data (not the Point Cloud, see 'depth.point_cloud_freq'). This value must be equal or less than the camera framerate.
        enable_image_validity_check: 1 # [SDK5 required] Sets the image validity check. If set to 1, the SDK will check if the frames are valid before processing.
        gpu_id: -1
        optional_opencv_calibration_file: '' # Optional path where the ZED SDK can find a file containing the calibration information of the camera computed by OpenCV. Read the ZED SDK documentation for more information: https://www.stereolabs.com/docs/api/structsl_1_1InitParameters.html#a9eab2753374ef3baec1d31960859ba19
        async_image_retrieval: false # If set to true will camera image retrieve at a framerate different from \ref grab() application framerate. This is useful for recording SVO or sending camera stream at different rate than application.
        publish_status: true # Advertise the status topics that are published only if a node subscribes to them
        # Other parameters are defined, according to the camera model, in the 'zed.yaml', 'zedm.yaml', 'zed2.yaml', 'zed2i.yaml'
        # 'zedx.yaml', 'zedxmini.yaml', 'virtual.yaml' files

    video:
        saturation: 4 # [DYNAMIC]
        sharpness: 4 # [DYNAMIC]
        gamma: 8 # [DYNAMIC]
        auto_exposure_gain: true # [DYNAMIC]
        exposure: 80 # [DYNAMIC]
        gain: 80 # [DYNAMIC]
        auto_whitebalance: true # [DYNAMIC]
        whitebalance_temperature: 42 # [DYNAMIC] - [28,65] x100 - works only if `auto_whitebalance` is false
        publish_rgb: true # Advertise the RGB image topics that are published only if a node subscribes to them
        publish_left_right: false # Advertise the left and right image topics that are published only if a node subscribes to them
        publish_raw: false # Advertise the raw image topics that are published only if a node subscribes to them
        publish_gray: false # Advertise the gray image topics that are published only if a node subscribes to them
        publish_stereo: false # Advertise the stereo image topic that is published only if a node subscribes to it
        # Other parameters are defined, according to the camera model, in the 'zed.yaml', 'zedm.yaml', 'zed2.yaml', 'zed2i.yaml'
        # 'zedx.yaml', 'zedxmini.yaml', 'virtual.yaml' files

    sensors:
        publish_imu_tf: false # [overwritten by launch file options] enable/disable the IMU TF broadcasting
        sensors_image_sync: false # Synchronize Sensors messages with latest published video/depth message
        sensors_pub_rate: 100. # frequency of publishing of sensors data. MAX: 400. - MIN: grab rate
        publish_imu: false # Advertise the IMU topic that is published only if a node subscribes to it
        publish_imu_raw: false # Advertise the raw IMU topic that is published only if a node subscribes to it
        publish_cam_imu_transf: false # Advertise the CAMERA-IMU transformation topic that is published only if a node subscribes to it
        publish_mag: false # Advertise the magnetometer topic that is published only if a node subscribes to it
        publish_baro: false # Advertise the barometer topic that is published only if a node subscribes to it
        publish_temp: false # Advertise the temperature topics that are published only if a node subscribes to them

    region_of_interest:
        automatic_roi: false # Enable the automatic ROI generation to automatically detect part of the robot in the FoV and remove them from the processing. Note: if enabled the value of `manual_polygon` is ignored
        depth_far_threshold_meters: 2.5 # Filtering how far object in the ROI should be considered, this is useful for a vehicle for instance
        image_height_ratio_cutoff: 0.5 # By default consider only the lower half of the image, can be useful to filter out the sky
        #manual_polygon: '[]' # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
        #manual_polygon: '[[0.25,0.33],[0.75,0.33],[0.75,0.5],[0.5,0.75],[0.25,0.5]]' # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
        #manual_polygon: '[[0.25,0.25],[0.75,0.25],[0.75,0.75],[0.25,0.75]]' # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
        #manual_polygon: '[[0.5,0.25],[0.75,0.5],[0.5,0.75],[0.25,0.5]]' # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
        apply_to_depth: true # Apply ROI to depth processing
        apply_to_positional_tracking: true # Apply ROI to positional tracking processing
        apply_to_object_detection: true # Apply ROI to object detection processing
        apply_to_body_tracking: true # Apply ROI to body tracking processing
        apply_to_spatial_mapping: true # Apply ROI to spatial mapping processing
        publish_roi_mask: false # Advertise the ROI mask image topic that is published only if a node subscribes to it

    depth:
        depth_mode: 'NEURAL' # Matches the ZED SDK setting: 'NONE', 'PERFORMANCE', 'QUALITY', 'ULTRA', 'NEURAL', 'NEURAL_PLUS' - Note: if 'NONE' all the modules that requires depth extraction are disabled by default (Pos. Tracking, Obj. Detection, Mapping, ...)
        depth_stabilization: 20 # Forces positional tracking to start if major than 0 - Range: [0,100]
        openni_depth_mode: false # 'false': 32bit float [meters], 'true': 16bit unsigned int [millimeters]
        point_cloud_freq: 30.0 # [DYNAMIC] Frequency of the pointcloud publishing. This value must be equal or less than the camera framerate.
        point_cloud_res: 'COMPACT' # The resolution used for point cloud publishing - 'COMPACT'-Standard resolution. Optimizes processing and bandwidth, 'REDUCED'-Half resolution. Low processing and bandwidth requirements
        depth_confidence: 95 # [DYNAMIC]
        depth_texture_conf: 100 # [DYNAMIC]
        remove_saturated_areas: true # [DYNAMIC]
        publish_depth_map: true # Advertise the depth map topics that are published only if a node subscribes to them
        publish_depth_info: false # Advertise the depth info topic that is published only if a node subscribes to it
        publish_point_cloud: false # Advertise the point cloud topic that is published only if a node subscribes to it
        publish_depth_confidence: true # Advertise the depth confidence topic that is published only if a node subscribes to it
        publish_disparity: false # Advertise the disparity topic that is published only if a node subscribes to it
        # Other parameters are defined, according to the camera model, in the 'zed.yaml', 'zedm.yaml', 'zed2.yaml', 'zed2i.yaml'
        # 'zedx.yaml', 'zedxmini.yaml', 'virtual.yaml' files

    pos_tracking:
        pos_tracking_enabled: false # True to enable positional tracking from start
        pos_tracking_mode: 'GEN_3' # Matches the ZED SDK setting: 'GEN_1', 'GEN_2', 'GEN_3'
        imu_fusion: false # enable/disable IMU fusion. When set to false, only the optical odometry will be used.
        publish_tf: false # [overwritten by launch file options] publish `odom -> camera_link` TF
        publish_map_tf: false # [overwritten by launch file options] publish `map -> odom` TF
        map_frame: 'map'
        odometry_frame: 'odom'
        area_memory: true # Enable to detect loop closure
        area_file_path: '' # Path to the area memory file for relocalization and loop closure in a previously explored environment. 
        save_area_memory_on_closing: false # Save Area memory before closing the camera if `area_file_path` is not empty. You can also use the `save_area_memory` service to save the area memory at any time.
        reset_odom_with_loop_closure: true # Re-initialize odometry to the last valid pose when loop closure happens (reset camera odometry drift)
        publish_3d_landmarks: false # Publish 3D landmarks used by the positional tracking algorithm
        publish_lm_skip_frame: 5 # Publish the landmarks every X frames to reduce bandwidth. Set to 0 to publish all landmarks
        depth_min_range: 0.0 # Set this value for removing fixed zones of the robot in the FoV of the camerafrom the visual odometry evaluation
        set_as_static: false # If 'true' the camera will be static and not move in the environment
        set_gravity_as_origin: true # If 'true' align the positional tracking world to imu gravity measurement. Keep the yaw from the user initial pose.
        floor_alignment: false # Enable to automatically calculate camera/floor offset
        initial_base_pose: [0.0, 0.0, 0.0, 0.0, 0.0, 0.0] # Initial position of the `camera_link` frame in the map -> [X, Y, Z, R, P, Y]
        path_pub_rate: 2.0 # [DYNAMIC] - Camera trajectory publishing frequency
        path_max_count: -1 # use '-1' for unlimited path size
        two_d_mode: false # Force navigation on a plane. If true the Z value will be fixed to 'fixed_z_value', roll and pitch to zero
        fixed_z_value: 0.0 # Value to be used for Z coordinate if `two_d_mode` is true
        transform_time_offset: 0.0 # The value added to the timestamp of `map->odom` and `odom->camera_link` transform being generated
        reset_pose_with_svo_loop: true # Reset the camera pose the `initial_base_pose` when the SVO loop is enabled and the SVO playback reaches the end of the file.
        publish_odom_pose: true # Advertise the odometry and pose topics that are published only if a node subscribes to them
        publish_pose_cov: false # Advertise the pose with covariance topic that is published only if a node subscribes to it
        publish_cam_path: false # Advertise the camera odometry and pose path topics that are published only if a node subscribes to them

    gnss_fusion:
        gnss_fusion_enabled: false # fuse 'sensor_msg/NavSatFix' message information into pose data
        gnss_fix_topic: '/fix' # Name of the GNSS topic of type NavSatFix to subscribe [Default: '/gps/fix']
        gnss_zero_altitude: false # Set to `true` to ignore GNSS altitude information
        h_covariance_mul: 1.0 # Multiplier factor to be applied to horizontal covariance of the received fix (plane X/Y)
        v_covariance_mul: 1.0 # Multiplier factor to be applied to vertical covariance of the received fix (Z axis)
        publish_utm_tf: true # Publish `utm` -> `map` TF
        broadcast_utm_transform_as_parent_frame: false # if 'true' publish `utm` -> `map` TF, otherwise `map` -> `utm`
        enable_reinitialization: false # determines whether reinitialization should be performed between GNSS and VIO fusion when a significant disparity is detected between GNSS data and the current fusion data. It becomes particularly crucial during prolonged GNSS signal loss scenarios.
        enable_rolling_calibration: true # If this parameter is set to true, the fusion algorithm will used a rough VIO / GNSS calibration at first and then refine it. This allow you to quickly get a fused position.
        enable_translation_uncertainty_target: false # When this parameter is enabled (set to true), the calibration process between GNSS and VIO accounts for the uncertainty in the determined translation, thereby facilitating the calibration termination. The maximum allowable uncertainty is controlled by the 'target_translation_uncertainty' parameter.
        gnss_vio_reinit_threshold: 5.0 # determines the threshold for GNSS/VIO reinitialization. If the fused position deviates beyond out of the region defined by the product of the GNSS covariance and the gnss_vio_reinit_threshold, a reinitialization will be triggered.
        target_translation_uncertainty: 0.1 # defines the target translation uncertainty at which the calibration process between GNSS and VIO concludes. By default, the threshold is set at 10 centimeters.
        target_yaw_uncertainty: 0.1 # defines the target yaw uncertainty at which the calibration process between GNSS and VIO concludes. The unit of this parameter is in radian. By default, the threshold is set at 0.1 radians.

    mapping:
        mapping_enabled: false # True to enable mapping t # Pand fused point cloud pubblication
        resolution: 0.05 # maps resolution in meters [min: 0.01f - max: 0.2f]
        max_mapping_range: 5.0 # maximum depth range while mapping in meters (-1 for automatic calculation) [2.0, 20.0]
        fused_pointcloud_freq: 1.0 # frequency of the publishing of the fused colored point cloud
        clicked_point_topic: '/clicked_point' # Topic published by Rviz when a point of the cloud is clicked. Used for plane detection
        pd_max_distance_threshold: 0.15 # Plane detection: controls the spread of plane by checking the position difference.
        pd_normal_similarity_threshold: 15.0 # Plane detection: controls the spread of plane by checking the angle difference.
        publish_det_plane: false # Advertise the plane detection topics that is published only if a node subscribes to it

    object_detection:
        od_enabled: false # True to enable Object Detection
        enable_tracking: true # Whether the object detection system includes object tracking capabilities across a sequence of images.
        detection_model: 'MULTI_CLASS_BOX_FAST' # 'MULTI_CLASS_BOX_FAST', 'MULTI_CLASS_BOX_MEDIUM', 'MULTI_CLASS_BOX_ACCURATE', 'PERSON_HEAD_BOX_FAST', 'PERSON_HEAD_BOX_ACCURATE', 'CUSTOM_YOLOLIKE_BOX_OBJECTS'
        max_range: 20.0 # [m] Upper depth range for detections.The value cannot be greater than 'depth.max_depth'
        filtering_mode: 'NMS3D' # Filtering mode that should be applied to raw detections: 'NONE', 'NMS3D', 'NMS3D_PER_CLASS'
        prediction_timeout: 2.0 # During this time [sec], the object will have OK state even if it is not detected. Set this parameter to 0 to disable SDK predictions
        allow_reduced_precision_inference: false # Allow inference to run at a lower precision to improve runtime and memory usage
        # Other parameters are defined in the 'object_detection.yaml' and 'custom_object_detection.yaml' files

    body_tracking:
        bt_enabled: false # True to enable Body Tracking
        model: 'HUMAN_BODY_MEDIUM' # 'HUMAN_BODY_FAST', 'HUMAN_BODY_MEDIUM', 'HUMAN_BODY_ACCURATE'
        body_format: 'BODY_38' # 'BODY_18','BODY_34','BODY_38'
        allow_reduced_precision_inference: false # Allow inference to run at a lower precision to improve runtime and memory usage
        max_range: 15.0 # [m] Defines a upper depth range for detections
        body_kp_selection: 'FULL' # 'FULL', 'UPPER_BODY'
        enable_body_fitting: false # Defines if the body fitting will be applied
        enable_tracking: true # Defines if the object detection will track objects across images flow
        prediction_timeout_s: 0.5 # During this time [sec], the skeleton will have OK state even if it is not detected. Set this parameter to 0 to disable SDK predictions
        confidence_threshold: 50.0 # [DYNAMIC] - Minimum value of the detection confidence of skeleton key points [0,99]
        minimum_keypoints_threshold: 5 # [DYNAMIC] - Minimum number of skeleton key points to be detected for a valid skeleton

    stream_server:
        stream_enabled: false # enable the streaming server when the camera is open
        codec: 'H264' # different encoding types for image streaming: 'H264', 'H265'
        port: 30000 # Port used for streaming. Port must be an even number. Any odd number will be rejected.
        bitrate: 12500 # [1000 - 60000] Streaming bitrate (in Kbits/s) used for streaming. See https://www.stereolabs.com/docs/api/structsl_1_1StreamingParameters.html#a873ba9440e3e9786eb1476a3bfa536d0
        gop_size: -1 # [max 256] The GOP size determines the maximum distance between IDR/I-frames. Very high GOP size will result in slightly more efficient compression, especially on static scenes. But latency will increase.
        adaptative_bitrate: false # Bitrate will be adjusted depending the number of packet dropped during streaming. If activated, the bitrate can vary between [bitrate/4, bitrate].
        chunk_size: 16084 # [1024 - 65000] Stream buffers are divided into X number of chunks where each chunk is chunk_size bytes long. You can lower chunk_size value if network generates a lot of packet lost: this will generates more chunk for a single image, but each chunk sent will be lighter to avoid inside-chunk corruption. Increasing this value can decrease latency.
        target_framerate: 0 # Framerate for the streaming output. This framerate must be below or equal to the camera framerate. Allowed framerates are 15, 30, 60 or 100 if possible. Any other values will be discarded and camera FPS will be taken.

    advanced: # WARNING: do not modify unless you are confident of what you are doing
        # Reference documentation: https://man7.org/linux/man-pages/man7/sched.7.html
        thread_sched_policy: 'SCHED_BATCH' # 'SCHED_OTHER', 'SCHED_BATCH', 'SCHED_FIFO', 'SCHED_RR' - NOTE: 'SCHED_FIFO' and 'SCHED_RR' require 'sudo'
        thread_grab_priority: 50 # ONLY with 'SCHED_FIFO' and 'SCHED_RR' - [1 (LOW) z-> 99 (HIGH)] - NOTE: 'sudo' required
        thread_sensor_priority: 70 # ONLY with 'SCHED_FIFO' and 'SCHED_RR' - [1 (LOW) z-> 99 (HIGH)] - NOTE: 'sudo' required
        thread_pointcloud_priority: 60 # ONLY with 'SCHED_FIFO' and 'SCHED_RR' - [1 (LOW) z-> 99 (HIGH)] - NOTE: 'sudo' required

    debug:
        sdk_verbose: 1 # Set the verbose level of the ZED SDK
        sdk_verbose_log_file: '' # Path to the file where the ZED SDK will log its messages. If empty, no file will be created. The log level can be set using the `sdk_verbose` parameter.
        use_pub_timestamps: false # Use the current ROS time for the message timestamp instead of the camera timestamp. This is useful to test data communication latency.
        debug_common: false
        debug_sim: false
        debug_video_depth: false
        debug_camera_controls: false
        debug_point_cloud: false
        debug_positional_tracking: false
        debug_gnss: false
        debug_sensors: false
        debug_mapping: false
        debug_terrain_mapping: false
        debug_object_detection: false
        debug_body_tracking: false
        debug_roi: false
        debug_streaming: false
        debug_advanced: false
        debug_nitros: false
        disable_nitros: false # If available, disable NITROS usage for debugging and testing purposes

```

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [November 21, 2025, 1:11pm UTC](https://community.stereolabs.com/t/ros2-humble-zed-multi-container-dies-frequently-jetson-agx-orin-64gb-l4t-36-4-7-zed-sdk-5-1-1-3-zedx-mini-via-quad-capture-card/10374/4 "2025-11-21T13:11:19Z")

</div>

> [@Maximilian](#):
>
> `pos_tracking_mode: 'GEN_3'`

This, together with the ZED SDK v5.1.1, is the possible cause of the issue.  
Please upgrade to ZED SDK v5.1.2 if you want to use `GEN_3`; otherwise, use `GEN_1` or `GEN_2`.