# Recording Parameters in Unreal Engine

**URL:** <https://community.stereolabs.com/t/recording-parameters-in-unreal-engine/10787>\
**Category:** Unreal Engine\
**Tags:** svo, sdk\
**Created:** [February 11, 2026, 2:05pm UTC](https://community.stereolabs.com/t/recording-parameters-in-unreal-engine/10787 "2026-02-11T14:05:38Z")\
**Posts on this page:** 3\
**Page:** 1

<div class="post-metadata">

**Author:** ![julian15](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/j/a6a055/32.png) [@julian15](https://community.stereolabs.com/u/julian15)\
**Post date:** [February 11, 2026, 2:05pm UTC](https://community.stereolabs.com/t/recording-parameters-in-unreal-engine/10787/1 "2026-02-11T14:05:39Z")

</div>

Hi,

I’m trying to build an app in Unreal Engine using the ZED SDK that performs body tracking. There’s a Virtual Canvas that shows the camera’s live RGB feed. I’ve set up a replay system that records the body tracking data. Afterwards, a new avatar is spawned and replicates the same movements.

Now I want the RGB video to be shown again in the Virtual Canvas as well. This means I would somehow need to save the frames beforehand or directly record a video and then play it back. I’ve tried using the recording parameters in the ZED\_Initializer, but I couldn’t get it working.

Any help would be much appreciated!

Best regards,  
Julian

---

<div class="post-metadata">

**Author:** ![BenjaminV](https://community.stereolabs.com/user_avatar/community.stereolabs.com/benjaminv/32/3863_2.png) [@BenjaminV](https://community.stereolabs.com/u/BenjaminV)\
**Post date:** [February 16, 2026, 8:03am UTC](https://community.stereolabs.com/t/recording-parameters-in-unreal-engine/10787/2 "2026-02-16T08:03:08Z")

</div>

Hi,

You have two possibilities:

- First, you use the recording module of the ZED SDK ([Video Recording - Stereolabs](https://www.stereolabs.com/docs/video/recording)) to record a “SVO” file, which can be used later as input in the SDK if you want to replay the whole scene.
- Or, Only save the rgb images alongside the Body tracking data. Then, do not use the ZED SDK but save the images as png file on disk. The image is retrieved from the camera is available here ([zed-UE5/Plugins/Stereolabs/Source/ZED/Public/Core/ZEDCamera.h at main · stereolabs/zed-UE5 · GitHub](https://github.com/stereolabs/zed-UE5/blob/main/Plugins/Stereolabs/Source/ZED/Public/Core/ZEDCamera.h#L226)) as a Texture. Then, you can save this texture on disk.

---

<div class="post-metadata">

**Author:** ![julian15](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/j/a6a055/32.png) [@julian15](https://community.stereolabs.com/u/julian15)\
**Post date:** [February 19, 2026, 9:42am UTC](https://community.stereolabs.com/t/recording-parameters-in-unreal-engine/10787/3 "2026-02-19T09:42:22Z")

</div>

Hey,

thanks for helping, I will try that!