# Recommended Jetson model for 2× ZED 2i real-time depth and tracking

**URL:** <https://community.stereolabs.com/t/recommended-jetson-model-for-2x-zed-2i-real-time-depth-and-tracking/11487>\
**Category:** Hardware\
**Tags:** jetson\
**Created:** [June 30, 2026, 8:00am UTC](https://community.stereolabs.com/t/recommended-jetson-model-for-2x-zed-2i-real-time-depth-and-tracking/11487 "2026-06-30T08:00:00Z")\
**Posts on this page:** 3\
**Page:** 1

<div class="post-metadata">

**Author:** ![stilrmy](https://community.stereolabs.com/user_avatar/community.stereolabs.com/stilrmy/32/6359_2.png) [@stilrmy](https://community.stereolabs.com/u/stilrmy)\
**Post date:** [June 30, 2026, 8:00am UTC](https://community.stereolabs.com/t/recommended-jetson-model-for-2x-zed-2i-real-time-depth-and-tracking/11487/1 "2026-06-30T08:00:00Z")

</div>

Hello [Stereolabs](https://www.stereolabs.com/) team,

We are planning to use **two ZED 2i cameras** on a quadruped robot and would like to confirm which Jetson model is sufficient for reliable real-time operation.

Our expected setup is:

- **2× ZED 2i** connected to one Jetson via USB 3.0

- Real-time camera capture and depth estimation

- Possible object/human tracking on the Jetson

- Main use case: robot following and object tracking

- Priority: stable frame rate and low latency, not maximum image resolution

The expected camera settings are likely:

- **HD720 @ 30 FPS or 60 FPS**

- Depth mode: **NEURAL\_LIGHT** or **NEURAL**

- We do not need full-rate offline recording, but stable real-time operation is important.

We are considering the following Jetson models:

- Jetson Orin NX 16GB

- Jetson AGX Orin 32GB

- Jetson AGX Orin 64GB

- Jetson AGX Thor, if it provides a meaningful benefit for this setup

Could you please advise:

1. Is **Jetson Orin NX 16GB** sufficient for running **2× ZED 2i** with real-time depth estimation and object/human tracking?

2. In what cases would you recommend upgrading to **AGX Orin 32GB or 64GB**?

3. Would **Jetson AGX Thor** provide a meaningful practical benefit for this two-camera setup, or would it be unnecessary overkill?

4. What resolution, FPS, and depth mode would you recommend for stable dual-ZED operation?

5. Are there any USB bandwidth or USB controller limitations we should consider when using **two ZED 2i cameras** on one Jetson?

6. Which JetPack and ZED SDK versions do you recommend for this setup?

7. Do you have any confirmed successful configuration or benchmark for **2× ZED 2i on Orin NX 16GB, AGX Orin, or AGX Thor**?

Thank you.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [June 30, 2026, 4:47pm UTC](https://community.stereolabs.com/t/recommended-jetson-model-for-2x-zed-2i-real-time-depth-and-tracking/11487/2 "2026-06-30T16:47:29Z")

</div>

Hi @stilrmy  
Welcome to the [StereoLabs](https://www.stereolabs.com/) community.

Thank you for the detailed description; it makes it much easier to give you precise guidance.

> [@stilrmy](#):
>
> Is **Jetson Orin NX 16GB** sufficient for running **2× ZED 2i** with real-time depth estimation and object/human tracking?

For your stated priority (stable frame rate and low latency over maximum resolution), the Orin NX 16GB is a reasonable starting point, but it will be tight once you add object/body tracking on top of dual-camera depth. Our published Neural depth benchmarks give a good reference; note they were measured on ZED X, but they illustrate the relative GPU cost well. With `NEURAL_LIGHT`, two cameras at 30 FPS consume roughly 23% GPU; with `NEURAL`, two cameras reach roughly 50% GPU. Object or body tracking adds a further AI inference load to the same GPU, so on the Orin NX 16GB you should plan to run `NEURAL_LIGHT` and keep one tracking module active, not several in parallel. You can review the full tables here: [Depth Modes | StereoLabs](https://docs.stereolabs.com/docs/development/zed-sdk/modules/depth-sensing/depth-modes)

> [@stilrmy](#):
>
> In what cases would you recommend upgrading to **AGX Orin 32GB or 64GB**?

The AGX Orin 32GB is the safer choice if you want headroom to run `NEURAL` depth on both cameras while keeping object detection and body tracking active simultaneously, or if you anticipate moving to higher FPS or adding more processing on the same unit. The 64GB variant is mainly justified when you run large additional AI workloads (your own detection networks, mapping, planning) alongside the ZED SDK. For a strict dual-ZED-2i depth plus tracking pipeline, 32GB is generally enough; the extra RAM of the 64GB is rarely the bottleneck before GPU compute is.

> [@stilrmy](#):
>
> Would **Jetson AGX Thor** provide a meaningful practical benefit for this two-camera setup, or would it be unnecessary overkill?

For a two-camera ZED 2i setup with `NEURAL_LIGHT` or `NEURAL`, Thor is overkill. It becomes meaningful only if you plan to scale to more cameras, run `NEURAL_PLUS`, or host heavy concurrent AI models. I would not recommend it for this specific configuration.

> [@stilrmy](#):
>
> What resolution, FPS, and depth mode would you recommend for stable dual-ZED operation?

Given your “following and tracking” use case, where mid-range obstacle and subject perception matters more than fine detail, I recommend HD720 @ 30 FPS with `NEURAL_LIGHT`. This mode is the fastest and is explicitly designed for multi-camera setups, with an ideal depth range of 0.3 to 5 m, which suits robot following well. If you later find you need better object detail or longer range and you have spare GPU budget (typically on AGX Orin), `NEURAL` extends the ideal range to about 0.3 to 9 m. I would avoid `NEURAL_PLUS` for a two-camera real-time pipeline; it is the slowest mode and is not well suited to multi-camera operation.

> [@stilrmy](#):
>
> Are there any USB bandwidth or USB controller limitations we should consider when using **two ZED 2i cameras** on one Jetson?

This is an important point for dual ZED 2i. Each ZED 2i requires a full USB 3.0 (5 Gbps) bandwidth allocation for uncompressed stereo video. The key constraint is not just the number of ports but the number of independent USB host controllers. If both cameras share a single USB 3.0 controller through an internal hub, you can saturate the available bandwidth and see frame drops. On Jetson, verify that the two cameras enumerate on separate USB host controllers (`lsusb -t` is your friend here), and prefer direct ports over hubs. Also use quality cables; marginal cables are a frequent cause of intermittent green frames or drops at HD720/HD1080.

> [@stilrmy](#):
>
> Which JetPack and ZED SDK versions do you recommend for this setup?

I recommend pairing the latest ZED SDK 5.x with the JetPack version officially listed as supported for it on our download page, rather than the newest JetPack available. You can always confirm the exact supported JetPack/L4T combination here before flashing: [ZED SDK 5.4 - Download | Stereolabs](https://www.stereolabs.com/developers/release/)

> [@stilrmy](#):
>
> Do you have any confirmed successful configuration or benchmark for **2× ZED 2i on Orin NX 16GB, AGX Orin, or AGX Thor**?

The performance figures above are our official multi-camera benchmarks, measured with the ZED SDK multi-camera example on Orin AGX, Orin NX 16, Orin NX 8, and Nano. They are based on ZED X rather than ZED 2i, so treat them as a strong relative indicator of GPU cost per depth mode rather than an exact ZED 2i number. The reference code is here: [zed-sdk/depth sensing/multi camera at master · stereolabs/zed-sdk · GitHub](https://github.com/stereolabs/zed-sdk/tree/master/depth%20sensing/multi%20camera)

For product details and specifications, the ZED 2i page is here: [ZED 2 - AI Stereo Camera | Stereolabs](https://www.stereolabs.com/products/zed-2) and you can find it in the store at [https://store.stereolabs.com/](https://store.stereolabs.com/)

To summarize: for a robust 2x ZED 2i following-and-tracking robot, AGX Orin 32GB with HD720 @ 30 FPS and `NEURAL_LIGHT` is the configuration I would recommend for comfortable headroom; the Orin NX 16GB can work if you stay strictly on `NEURAL_LIGHT` and limit concurrent tracking modules.

Could you let me know which tracking you intend to run (object detection, body tracking, or both, and whether on the ZED SDK or your own network)? That determines how much GPU budget remains for depth and will let me refine the recommendation.

---

<div class="post-metadata">

**Author:** ![stilrmy](https://community.stereolabs.com/user_avatar/community.stereolabs.com/stilrmy/32/6359_2.png) [@stilrmy](https://community.stereolabs.com/u/stilrmy)\
**Post date:** [July 1, 2026, 1:37am UTC](https://community.stereolabs.com/t/recommended-jetson-model-for-2x-zed-2i-real-time-depth-and-tracking/11487/3 "2026-07-01T01:37:09Z")

</div>

Thank you for the reply! We are going to run the object detection on the cameras. Considering the future support for other projects, we might go with the AGX Orin 64 GB. Thank you very much for the information!