# Questions if Zed 2i is Right

**URL:** <https://community.stereolabs.com/t/questions-if-zed-2i-is-right/11259>\
**Category:** Software\
**Tags:** zed-gstreamer, python, jetson\
**Created:** [April 30, 2026, 2:58pm UTC](https://community.stereolabs.com/t/questions-if-zed-2i-is-right/11259 "2026-04-30T14:58:26Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![T.Peace](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/t/e480ec/32.png) [@T.Peace](https://community.stereolabs.com/u/T.Peace)\
**Post date:** [April 30, 2026, 2:58pm UTC](https://community.stereolabs.com/t/questions-if-zed-2i-is-right/11259/1 "2026-04-30T14:58:26Z")

</div>

I have a few questions regarding the zed 2i stereo camera.

Are each of the cameras individually addressable, or is it a unified video stream? I would like to get each camera individually.

My use case is to have it on a small rc boat. I see that it has an IP66 rating. How well would that do on the water? The goal is not to submerge it, but there is a high probability of getting wet, and always a small risk of being submerged.

My vision system uses gstreamer and deepstream, and I see that there is a gstreamer plugin for the camera. How well does it work? Is it also possible to interact through v4l2?

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [May 4, 2026, 1:12pm UTC](https://community.stereolabs.com/t/questions-if-zed-2i-is-right/11259/2 "2026-05-04T13:12:54Z")

</div>

Hi @T.Peace

> [@T.Peace](#):
>
> Are each of the cameras individually addressable, or is it a unified video stream? I would like to get each camera individually.

You can retrieve the streams separately by using the [ZED SDK API](https://www.stereolabs.com/docs/api).

> [@T.Peace](#):
>
> My use case is to have it on a small rc boat. I see that it has an IP66 rating. How well would that do on the water? The goal is not to submerge it, but there is a high probability of getting wet, and always a small risk of being submerged.

IP66 means **Ingress Protection 66** , per IEC 60529. The two digits break down as:

**First digit (6) — Solid particle protection:** Dust-tight. Complete protection against contact with internal components and no ingress of dust whatsoever.

**Second digit (6) — Liquid ingress protection:** Protection against powerful water jets. Water projected in powerful jets (12.5 mm nozzle) from any direction shall have no harmful effects. Test conditions are typically 100 liters/min at 100 kPa pressure from 3 meters distance for at least 3 minutes.

In practice, an IP66-rated enclosure can handle direct high-pressure washdowns (e.g., industrial cleaning) and operate in dusty outdoor environments without issues — but it is _not_ rated for immersion. For submersion, you’d need a second digit of 7 (temporary, up to 1 m) or 8 (continuous).

> [@T.Peace](#):
>
> My vision system uses gstreamer and deepstream, and I see that there is a gstreamer plugin for the camera. How well does it work? Is it also possible to interact through v4l2?

We provide GStreamer elements to use our cameras:  
GitHub: [GitHub - stereolabs/zed-gstreamer: Package of GStreamer elements to interface with ZED Cameras · GitHub](https://github.com/stereolabs/zed-gstreamer)  
Documentation: [Getting Started with GStreamer and ZED - Stereolabs](https://www.stereolabs.com/docs/gstreamer)