# Questions for remote streaming

**URL:** <https://community.stereolabs.com/t/questions-for-remote-streaming/1899>\
**Category:** ROS1\
**Tags:** streaming\
**Created:** [December 9, 2022, 1:19pm UTC](https://community.stereolabs.com/t/questions-for-remote-streaming/1899 "2022-12-09T13:19:20Z")\
**Posts on this page:** 5\
**Page:** 1

<div class="post-metadata">

**Author:** ![madjxatw](https://community.stereolabs.com/user_avatar/community.stereolabs.com/madjxatw/32/898_2.png) [@madjxatw](https://community.stereolabs.com/u/madjxatw)\
**Post date:** [December 9, 2022, 1:19pm UTC](https://community.stereolabs.com/t/questions-for-remote-streaming/1899/1 "2022-12-09T13:19:20Z")

</div>

I have a use case where a robot needs to do some cv stuff with zed meanwhile stream the images to a remote machine for monitoring purpose. My first attempt is to use the remote streaming feature from the SDK but found the ros node subscribing nothing once I first enable the streaming mode in another non-ros process. Similarly, when the zed ros node starts first, I couldn’t get the steaming work.

Now I notice that the ros wrapper has a service named `start_remote_stream`, I yet have no time this week to do further test on it, but want to get a quick answer whether executing a call to the remote streaming service would stop other stuff such as subscribing to image topics from working.

Another thing that I want to confirm is if it’s possible to receive the streaming on remote machine without SDK installed by using a video player that supports protocol like rtp? SDK and even CUDA requirement reduces the deployment flexibility for a simple monitoring end.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [December 10, 2022, 11:57am UTC](https://community.stereolabs.com/t/questions-for-remote-streaming/1899/2 "2022-12-10T11:57:26Z")

</div>

Hi @madjxatw  
welcome to the [Stereolabs](https://www.stereolabs.com/) community.

> [@madjxatw](#):
>
> Now I notice that the ros wrapper has a service named `start_remote_stream`, I yet have no time this week to do further test on it, but want to get a quick answer whether executing a call to the remote streaming service would stop other stuff such as subscribing to image topics from working.

No, the streaming service runs in parallel without affecting the node behaviors.

> [@madjxatw](#):
>
> Another thing that I want to confirm is if it’s possible to receive the streaming on remote machine without SDK installed by using a video player that supports protocol like rtp? SDK and even CUDA requirement reduces the deployment flexibility for a simple monitoring end.

No, the ZED SDK is required to process this kind of stream.

For remote monitoring you can use a ROS node that subscribes to ZED image topics and sends them using standard protocols, for example: [video\_stream\_opencv - ROS Wiki](http://wiki.ros.org/video_stream_opencv)

---

<div class="post-metadata">

**Author:** ![madjxatw](https://community.stereolabs.com/user_avatar/community.stereolabs.com/madjxatw/32/898_2.png) [@madjxatw](https://community.stereolabs.com/u/madjxatw)\
**Post date:** [December 10, 2022, 1:13pm UTC](https://community.stereolabs.com/t/questions-for-remote-streaming/1899/3 "2022-12-10T13:13:41Z")

</div>

Hi @Myzhar  
Thank you for the useful info! As my understanding, the video\_stream\_opencv package is used to take a video stream as input and publish it in an ROS image topic, which means that I have to install ROS on the remote monitoring end. I have no plan to introduce ROS on the remote side for the sake of simplicity and flexibility.

My current approach is subscribing to a ZED image topic and sending the images over UDP for lower network latency. However, considering the bandwidth and the size limit of a single UDP packet, I would prefer to use RTSP instead. This requires redirecting the subscribed images to an RTSP server, is there any easy-to-reach solution that you can advice?

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [December 11, 2022, 1:55pm UTC](https://community.stereolabs.com/t/questions-for-remote-streaming/1899/4 "2022-12-11T13:55:34Z")

</div>

@madjxatw this is what you are searching for:

> **[GitHub - CircusMonkey/ros\_rtsp: ROS node to subscribe to an image and serve...](https://github.com/CircusMonkey/ros_rtsp)**
>
> ROS node to subscribe to an image and serve it up as a RTSP video feed. - GitHub - CircusMonkey/ros\_rtsp: ROS node to subscribe to an image and serve it up as a RTSP video feed.

---

<div class="post-metadata">

**Author:** ![odin3](https://community.stereolabs.com/user_avatar/community.stereolabs.com/odin3/32/861_2.png) [@odin3](https://community.stereolabs.com/u/odin3)\
**Post date:** [December 13, 2022, 9:04am UTC](https://community.stereolabs.com/t/questions-for-remote-streaming/1899/5 "2022-12-13T09:04:33Z")

</div>

mmm this could be a solution to stream rtsp video from the jetson xavier nx with low latency? My goal is to onboard the zed camera on a robot and be able to control it without relying on a cuda graphics card.