# Python zed sdk , grab to slow

**URL:** <https://community.stereolabs.com/t/python-zed-sdk-grab-to-slow/11190>\
**Category:** Python\
**Tags:** sdk, jetson, depth\
**Created:** [April 15, 2026, 7:30am UTC](https://community.stereolabs.com/t/python-zed-sdk-grab-to-slow/11190 "2026-04-15T07:30:39Z")\
**Posts on this page:** 3\
**Page:** 1

<div class="post-metadata">

**Author:** ![timsaya](https://community.stereolabs.com/user_avatar/community.stereolabs.com/timsaya/32/6084_2.png) [@timsaya](https://community.stereolabs.com/u/timsaya)\
**Post date:** [April 15, 2026, 7:30am UTC](https://community.stereolabs.com/t/python-zed-sdk-grab-to-slow/11190/1 "2026-04-15T07:30:40Z")

</div>

I am using a ZED X Mini with a Jetson development board, and I am using the Python ZED SDK.

I use `zed.grab()` to acquire RGB images, depth visualization (`depth_vis`), and raw floating-point depth data.

I found that at SVGA resolution, a single **retrieve\_measure`()`** call takes about 20–25 ms. Is this normal?

At HD1080 resolution, it takes even longer, making it difficult to achieve a 30 FPS capture rate.

Is this expected behavior?

Strictly speaking, it is `retrieve_measure` to slow

---

<div class="post-metadata">

**Author:** ![mattrouss](https://community.stereolabs.com/user_avatar/community.stereolabs.com/mattrouss/32/2452_2.png) [@mattrouss](https://community.stereolabs.com/u/mattrouss)\
**Post date:** [April 15, 2026, 10:14am UTC](https://community.stereolabs.com/t/python-zed-sdk-grab-to-slow/11190/2 "2026-04-15T10:14:55Z")

</div>

Hello @timsaya,

As the majority of ZED SDK algorithms are computed in the grab() method, the latency of the grab() call depends on the following:

- resolution / frame rate selected
- which depth mode is enabled (NEURAL, NEURAL\_PLUS, etc)
- if there are other algorithms (positional tracking, object detection, etc) enabled
- the compute unit used (embedded Jetson computer or x86 PC with a big GPU)
- the power mode used for Jetson devices (recommended is MAXN for the fastest compute)

Which jetson platform are you using?

---

<div class="post-metadata">

**Author:** ![timsaya](https://community.stereolabs.com/user_avatar/community.stereolabs.com/timsaya/32/6084_2.png) [@timsaya](https://community.stereolabs.com/u/timsaya)\
**Post date:** [April 15, 2026, 12:31pm UTC](https://community.stereolabs.com/t/python-zed-sdk-grab-to-slow/11190/3 "2026-04-15T12:31:36Z")

</div>

_Jetson Orin NX_ 8GB

Is 20–30 ms expected? Is it possible to get it down to 10 ms on C++ SDK ?