# Point Cloud Alignment Issue in Multi-Camera Fusion with ZED2i (ZED360 + Fusion API)

**URL:** <https://community.stereolabs.com/t/point-cloud-alignment-issue-in-multi-camera-fusion-with-zed2i-zed360-fusion-api/9493>\
**Category:** C++\
**Tags:** multi-camera, calibration, depth\
**Created:** [July 22, 2025, 3:32pm UTC](https://community.stereolabs.com/t/point-cloud-alignment-issue-in-multi-camera-fusion-with-zed2i-zed360-fusion-api/9493 "2025-07-22T15:32:57Z")\
**Posts on this page:** 5\
**Page:** 1

<div class="post-metadata">

**Author:** ![priyamgupta](https://community.stereolabs.com/user_avatar/community.stereolabs.com/priyamgupta/32/4618_2.png) [@priyamgupta](https://community.stereolabs.com/u/priyamgupta)\
**Post date:** [July 22, 2025, 3:32pm UTC](https://community.stereolabs.com/t/point-cloud-alignment-issue-in-multi-camera-fusion-with-zed2i-zed360-fusion-api/9493/1 "2025-07-22T15:32:58Z")

</div>

Hi,

I’m working on a multi-camera setup using **two ZED2i cameras**. My goal is to **fuse the point cloud data** from both cameras into a single, well-aligned cloud so I can **calculate the volume of an object** placed within the shared space.

Here’s what I’m doing:

1. **Calibration:**

- I used **ZED360** for calibration.
- **Flip mode:** Auto
- **Depth mode:** Neural (instead of Ultra)
- Both cameras are connected **locally via USB 3.0** on the same machine.

1. **Fusion code:**

- I’m using the **body tracking fusion sample** from the official ZED SDK GitHub:  
[zed-sdk/body tracking/multi-camera/cpp at master · stereolabs/zed-sdk · GitHub](https://github.com/stereolabs/zed-sdk/tree/master/body%20tracking/multi-camera/cpp)
- Resolution: **1080p @ 30 FPS** on both cameras.
- Depth mode: \*\*NEURAL\_PLUS

**Problem:**  
The point clouds from the two cameras are **not aligning correctly** after fusion. The fused cloud seems **disjointed or misaligned** , making volume estimation unreliable.

I’ve attached an image showing the issue (see below).

* * *

**Questions:**

- Is this the **correct approach** for creating a unified point cloud for volume estimation?
- Could this issue be caused by:
  - Improper calibration?
  - USB bandwidth limits?
  - Using Neural instead of Ultra depth mode?
  - Camera placement or orientation?

- Are there **additional steps or settings** I should be using to improve the accuracy of fusion?

Any suggestions or troubleshooting tips would be appreciated!

 ![1](https://community.stereolabs.com/uploads/default/original/2X/9/9b095ed6f3e6ce4b88a4c83a718fe5f86f56bffd.jpeg)

In the above image you can see that the box made by tape should match or align but it is not.

---

<div class="post-metadata">

**Author:** ![priyamgupta](https://community.stereolabs.com/user_avatar/community.stereolabs.com/priyamgupta/32/4618_2.png) [@priyamgupta](https://community.stereolabs.com/u/priyamgupta)\
**Post date:** [July 22, 2025, 3:34pm UTC](https://community.stereolabs.com/t/point-cloud-alignment-issue-in-multi-camera-fusion-with-zed2i-zed360-fusion-api/9493/2 "2025-07-22T15:34:15Z")

</div>

[zed2i\_zed2i\_new19.json](https://community.stereolabs.com/uploads/short-url/4Wkwkt4Eci3Q4PDhRFj1sD45wYB.json) (1.5 KB)  
[ClientPublisher.cpp](https://community.stereolabs.com/uploads/short-url/9z8xqrjzATg0hDn1j2dmu3AGsnx.cpp) (3.3 KB)  
[main.cpp](https://community.stereolabs.com/uploads/short-url/5IOhKtxp8eO403bKgpyUumG98wH.cpp) (8.1 KB)

these are the code files which I am using for the reference.

---

<div class="post-metadata">

**Author:** ![BenjaminV](https://community.stereolabs.com/user_avatar/community.stereolabs.com/benjaminv/32/3863_2.png) [@BenjaminV](https://community.stereolabs.com/u/BenjaminV)\
**Post date:** [July 23, 2025, 6:55am UTC](https://community.stereolabs.com/t/point-cloud-alignment-issue-in-multi-camera-fusion-with-zed2i-zed360-fusion-api/9493/3 "2025-07-23T06:55:27Z")

</div>

Hi,

During the calibration, make sure to cover the whole area slowly.

If you still can not get an acceptable calibration, you can use this sample : [zed-aruco/multi-camera at master · stereolabs/zed-aruco · GitHub](https://github.com/stereolabs/zed-aruco/tree/master/multi-camera) to calibrate using aruco markers

---

<div class="post-metadata">

**Author:** ![priyamgupta](https://community.stereolabs.com/user_avatar/community.stereolabs.com/priyamgupta/32/4618_2.png) [@priyamgupta](https://community.stereolabs.com/u/priyamgupta)\
**Post date:** [July 23, 2025, 9:34am UTC](https://community.stereolabs.com/t/point-cloud-alignment-issue-in-multi-camera-fusion-with-zed2i-zed360-fusion-api/9493/4 "2025-07-23T09:34:02Z")

</div>

Yes, I tried this today but the calibration is still not perfect.  
I’ve attached three images: two from the individual cameras and the third showing the fused point cloud result. I’m using a 6x6 ArUco marker (ID = 5) with a marker length of 200 mm.

 ![Screenshot from 2025-07-23 11-31-16](https://community.stereolabs.com/uploads/default/original/2X/8/89ab235ace2c781c0d1a8af085b25e1c66455b43.jpeg)  
 ![Screenshot from 2025-07-23 11-25-46](https://community.stereolabs.com/uploads/default/original/2X/d/dbe44efe7a8aae0fd74f741c1147856ad6c58cdf.jpeg)  
 ![Screenshot from 2025-07-23 11-25-12](https://community.stereolabs.com/uploads/default/original/2X/f/faacc882063d84704557cff3b99dbc43159df7bb.jpeg)

The main issue now seems to be with the **depth alignment** — the floor plane is not aligning properly along the Z-axis between the two cameras. The fused point cloud shows noticeable misalignment in elevation.

 ![Screenshot from 2025-07-23 11-30-06](https://community.stereolabs.com/uploads/default/original/2X/e/e30de0c6e5c7cb8b2aa88f1946d54996009b225a.jpeg)  
 ![Screenshot from 2025-07-23 11-24-31](https://community.stereolabs.com/uploads/default/original/2X/2/2a56e258d1446f13eacb0cbcce08f4cbf34efe48.png)  
Is there any way to improve the Z-axis calibration accuracy? Should I be using a marker board or multiple markers instead of just one?  
Also the alignment issues are still there.

---

<div class="post-metadata">

**Author:** ![BenjaminV](https://community.stereolabs.com/user_avatar/community.stereolabs.com/benjaminv/32/3863_2.png) [@BenjaminV](https://community.stereolabs.com/u/BenjaminV)\
**Post date:** [July 23, 2025, 11:24am UTC](https://community.stereolabs.com/t/point-cloud-alignment-issue-in-multi-camera-fusion-with-zed2i-zed360-fusion-api/9493/5 "2025-07-23T11:24:30Z")

</div>

You can try to use a bigger Aruco.  
Using multiple markers can help; however, this is not supported in the current version of the code I shared. You will need to implement it yourself.