# Playback of SVO recording with external data

**URL:** <https://community.stereolabs.com/t/playback-of-svo-recording-with-external-data/11721>\
**Category:** Python\
**Tags:** svo, python\
**Created:** [September 15, 2026, 7:52pm UTC](https://community.stereolabs.com/t/playback-of-svo-recording-with-external-data/11721 "2026-09-15T19:52:43Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![mminervini](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/m/f05b48/32.png) [@mminervini](https://community.stereolabs.com/u/mminervini)\
**Post date:** [September 15, 2026, 7:52pm UTC](https://community.stereolabs.com/t/playback-of-svo-recording-with-external-data/11721/1 "2026-09-15T19:52:43Z")

</div>

Dear [StereoLabs](https://www.stereolabs.com/) support,

I followed the examples for [recording](https://github.com/stereolabs/zed-sdk/blob/master/recording/recording/external_data/python/svo_recording.py) and [playback](https://github.com/stereolabs/zed-sdk/blob/master/recording/playback/external_data/python/svo_playback.py) SVO files with external data using the Python API.

Recording works well and for each frame I write some data with `sl.TIME_REFERENCE.IMAGE` timestamp, however when I play back frames I get out of sync data.  
For the first frame in the video, `retrieve_svo_data` fails, then from the second frame on, `retrieve_svo_data` works, but I don’t get the data I was expecting:

- Frame 0: failure
- Frame 1: success, but got data of frame 0
- Frame 2: success, but got data of frame 1
- …

The [API reference](https://www.stereolabs.com/docs/api/python/classpyzed_1_1sl_1_1Camera.html#ab9cf1ff3d124a18d43505bb480ce2d83) of `retrieve_svo_data` is not clear on how the timestamp range is treated, in particular if it is considered an open or closed interval. Playing with the timestamps I realised that in order to get the expected data (i.e. data 0 for frame 0, data 1 for frame 1, etc.) I had to add 1 nanosecond to both `ts_begin` and `ts_end`.

This workaround of adding 1 ns got me where I wanted, but it doesn’t look very clean.  
Retrieving the data that was saved for a frame looks like a major use case of this API, so I was wandering if got it wrong and there is a better way to accomplish this task.

I’m on Orin NX with Jetpack 6.2.1 and ZED SDK 5.4.1.

Thanks in advance,  
Massimo