# Opening and closing two, or more cameras will leave the SDK in a dirty state

**URL:** <https://community.stereolabs.com/t/opening-and-closing-two-or-more-cameras-will-leave-the-sdk-in-a-dirty-state/11757>\
**Category:** C++\
**Tags:** sdk, jetson\
**Created:** [September 28, 2026, 12:39pm UTC](https://community.stereolabs.com/t/opening-and-closing-two-or-more-cameras-will-leave-the-sdk-in-a-dirty-state/11757 "2026-09-28T12:39:40Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![jtonu](https://community.stereolabs.com/user_avatar/community.stereolabs.com/jtonu/32/6511_2.png) [@jtonu](https://community.stereolabs.com/u/jtonu)\
**Post date:** [September 28, 2026, 12:39pm UTC](https://community.stereolabs.com/t/opening-and-closing-two-or-more-cameras-will-leave-the-sdk-in-a-dirty-state/11757/1 "2026-09-28T12:39:40Z")

</div>

On Jetson Orin NX with ZED SDK 5.5.0, a C++ client opens two ZED X One GS cameras sequentially and calls only `grab()`. The first process exits cleanly; reopening the same binary in the same boot can stall both `grab()` calls and abort during SDK/Argus recovery with `malloc(): unaligned tcache chunk detected`.

Reproduction:

1. Start two ZED X One GS cameras after a boot with no other camera client running.
2. Verify both workers joined and both `close()` calls returned `SUCCESS`, and the process exited normally. 3. Run the identical command again in the same boot. First reopen aborted spontaneously. In some camera configurations a second reopen is required, so repeat once more if needed.

````auto
malloc(): unaligned tcache chunk detected
Program received signal SIGABRT

Abort/recovery thread:
  __GI___ libc_malloc(bytes=48)
  libnvargus_socketclient.so
  sl::ArgusCamera::open(...)
  sl::ArgusCamera::reboot(bool)
  sl::ArgusCamera::control()

Blocked capture threads include:
  sl::ArgusCamera::readSingle(...)
  sl::GMSLInput::waitForNewFrame(int)
  sl::CameraOne::grab(...)
```

````

Environment:

```auto
Linux tonu-jetson 6.8.12-1021-tegra-wg #2 SMP PREEMPT Fri Sep 4 15:35:30 EEST 2026 aarch64 aarch64 aarch64 GNU/Linux
# R39 (release), REVISION: 2.1, GCID: 46758480, BOARD: generic, EABI: aarch64, DATE: Fri Aug 7 05:54:22 AM UTC 2026
# KERNEL_VARIANT: oot
TARGET_USERSPACE_LIB_DIR=nvidia
TARGET_USERSPACE_LIB_DIR_PATH=usr/lib/aarch64-linux-gnu/nvidia
f4d08c76ee844977358da3cb738e8c5daae15c70a83aa25e46ff76ae76e731b7 /usr/local/zed/lib/libsl_zed.so
f63be44ea6bdad92ed00d19c23c9ff30ea2dc4d9847e93b562d4aa1c486687b4 /usr/lib/aarch64-linux-gnu/nvidia/libnvargus_socketclient.so
e091c2e97a83123a7d5e7d482c2f69e41eecfac97b44fcbd129560561beffb4b /usr/sbin/nvargus-daemon

```

Code:

```auto
#include <sl/CameraOne.hpp>
#include <thread>

int main() {
    sl::CameraOne a, b;
    sl::InitParametersOne p;
    p.camera_resolution = sl::RESOLUTION::SVGA;
    p.camera_fps = 15;

    p.input.setFromCameraID(0);
    if (a.open(p) != sl::ERROR_CODE::SUCCESS) return 1;

    p.input.setFromCameraID(1);
    if (b.open(p) != sl::ERROR_CODE::SUCCESS) return 2;

    auto grab = [](sl::CameraOne* camera) {
        for (int i = 0; i < 360; ++i)
            camera->grab();
    };

    std::thread ta(grab, &a);
    std::thread tb(grab, &b);

    ta.join();
    tb.join();

    a.close();
    b.close();
}

```

All ~ 20 trials contained CSI/V4L2-related errors during camera discovery/setup. About a few failing trials contain a second occurrence burst after the automatic `nvargus-daemon` stop/start. Because the initial burst also occurs in most passing trials, the messages are relevant evidence but are not proof that CSI caused the heap corruption.

```auto
2026-09-23T15:51:52.624312+03:00 ... (NvCamV4l2) Error 0x000a000e: V4L2Device not available ... findDevice(), line 261
2026-09-23T15:51:52.624369+03:00 ... (NvOdmDevice) Error 0x000a000e: ... V4L2SensorViCsi.cpp, function initialize(), line 114
2026-09-23T15:51:52.624369+03:00 ... SCF: Error 0x00000004: Sensor could not be opened ... getSourceFromGuid(), line 726
2026-09-23T15:51:53.242440+03:00 ... (fusa) Error: BadValue nullptr in string in: fusaCsiStreamHandler.cpp 185
2026-09-23T15:52:12.199903+03:00 ... systemd[1]: Stopping nvargus-daemon.service - Argus daemon...
2026-09-23T15:52:13.246223+03:00 ... (NvCamV4l2) Error 0x000a000e: V4L2Device not available ... findDevice(), line 261
2026-09-23T15:52:13.246223+03:00 ... (NvOdmDevice) Error 0x000a000e: ... V4L2SensorViCsi.cpp, function initialize(), line 114
2026-09-23T15:52:13.246223+03:00 ... SCF: Error 0x00000004: Sensor could not be opened ... getSourceFromGuid(), line 726
2026-09-23T15:52:15.725266+03:00 ... (fusa) Error: BadValue nullptr in string in: fusaCsiStreamHandler.cpp 185

```

This may share the underlying defect reported in topic 11720, but it is not a confirmed duplicate. Evidence demonstrates an unsanitized SDK 5.5.0 same-boot reopen crash with heap corruption and CSI/Argus recovery errors. Please merge or cross-reference the cases if engineering confirms a common root cause.

---

<div class="post-metadata">

**Author:** ![pylon-sync-bot](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/dbc845/32.png) [@pylon-sync-bot](https://community.stereolabs.com/u/pylon-sync-bot)\
**Post date:** [September 30, 2026, 10:21am UTC](https://community.stereolabs.com/t/opening-and-closing-two-or-more-cameras-will-leave-the-sdk-in-a-dirty-state/11757/2 "2026-09-30T10:21:29Z")

</div>

Hi,&nbsp;

Our engineering teams are looking into your issue to identify a potential cause. We will let you know once we have updates on it.&nbsp;

Regards,&nbsp;

Tristan Leduc&nbsp;

StereoLabs Support