# New SDK 5.4.1 GMSL2 timestamping

**URL:** <https://community.stereolabs.com/t/new-sdk-5-4-1-gmsl2-timestamping/11570>\
**Category:** Software\
**Tags:** sdk\
**Created:** [July 25, 2026, 7:41am UTC](https://community.stereolabs.com/t/new-sdk-5-4-1-gmsl2-timestamping/11570 "2026-07-25T07:41:42Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![beniaminopozzan](https://community.stereolabs.com/user_avatar/community.stereolabs.com/beniaminopozzan/32/3586_2.png) [@beniaminopozzan](https://community.stereolabs.com/u/beniaminopozzan)\
**Post date:** [July 25, 2026, 7:41am UTC](https://community.stereolabs.com/t/new-sdk-5-4-1-gmsl2-timestamping/11570/1 "2026-07-25T07:41:42Z")

</div>

Hello,

The release notes for ZEDSDK 5.4.1 state

> Improved image timestamp accuracy on GMSL cameras (ZED X / ZED X One families): the frame timestamp is now captured in hardware instead of sampled in software, reducing timestamp jitter by ~10× and making it immune to CPU load. Enabled by default; set ZED\_SDK\_DISABLE\_HW\_TSC\_SOF=1 to restore the previous software-sampled timestamps.

First of all, this is great news!

- would it be possible to have a more in depth description of the changes and differences between the old and new timestamping mechanisms?
- is a minimum version for the GMSL2 driver required?

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [July 29, 2026, 4:00pm UTC](https://community.stereolabs.com/t/new-sdk-5-4-1-gmsl2-timestamping/11570/2 "2026-07-29T16:00:22Z")

</div>

Hi @beniaminopozzan  
thank you, I am glad the change is useful for your pipeline.

> would it be possible to have a more in depth description of the changes and differences between the old and new timestamping mechanisms?

What changed is _where_ and _when_ the timestamp is sampled, not the clock domain it is expressed in.

**Old behavior (software sampling):** the SDK capture thread read the selected clock at the moment the frame buffer was handed over to user space. That value therefore included the whole capture and delivery latency of the pipeline, plus the scheduling jitter of the capture thread itself; under heavy CPU load, thread wake-up delays translated directly into timestamp jitter.

**New behavior (hardware Start of Frame):** the SDK now uses the Start of Frame timestamp latched by the Tegra capture hardware (TSC counter) and propagated with the frame metadata by the GMSL2 driver, then converted into the active `TIMESTAMP_CLOCK` domain. The value is generated by hardware at the beginning of the frame, so it no longer depends on when the buffer reaches the application; this is where the ~10x jitter reduction and the immunity to CPU load come from.

Practical consequences worth checking in your application:

- the absolute values are now earlier than before, and the residual offset with respect to the real acquisition instant is nearly constant; if you were compensating the old delay with a fixed offset, that offset must be re-tuned or removed;
- inter-camera consistency improves in multi-camera rigs, because all the ports of the same capture card share the same hardware counter; this benefits Fusion and the association with external sensors (LiDAR, GNSS, robot IMU);
- the clock selector is orthogonal to this change: `SYSTEM_CLOCK` is still the default. If you correlate the image timestamps with a free-running hardware counter, or with a device that is not time-disciplined by the host, consider `sl::TIMESTAMP_CLOCK::MONOTONIC_RAW_CLOCK`, introduced in v5.4: [ZED SDK 5.4 - Download | Stereolabs](https://www.stereolabs.com/developers/release/5.4)
- `ZED_SDK_DISABLE_HW_TSC_SOF=1` restores exactly the previous software-sampled behavior, which makes an A/B comparison on your own setup easy.

> is a minimum version for the GMSL2 driver required?

The hardware Start of Frame timestamp is delivered by the GMSL2 driver, so an up to date ZED X Driver is required. I recommend installing the latest driver available for your platform, v1.4.2 is the latest now: [Stereolabs ZED X GMSL2 Drivers | Stereolabs](https://www.stereolabs.com/developers/drivers) (installation steps: [Install the ZED Link driver | StereoLabs](https://www.stereolabs.com/docs/embedded/zed-link/install-the-drivers)).