# Multi - Camera Incorrect FPS and Dropped frames

**URL:** <https://community.stereolabs.com/t/multi-camera-incorrect-fps-and-dropped-frames/10984>\
**Category:** Software\
**Tags:** sdk, jetson\
**Created:** [March 8, 2026, 11:46pm UTC](https://community.stereolabs.com/t/multi-camera-incorrect-fps-and-dropped-frames/10984 "2026-03-08T23:46:56Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![dhutchinson](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/d/77aa72/32.png) [@dhutchinson](https://community.stereolabs.com/u/dhutchinson)\
**Post date:** [March 8, 2026, 11:46pm UTC](https://community.stereolabs.com/t/multi-camera-incorrect-fps-and-dropped-frames/10984/1 "2026-03-08T23:46:57Z")

</div>

I have a ZED Box Orin NX 16GB  
1x ZED X  
1x ZED X Mini

I noticed that If i have 2 cameras running different FPS it causes frame drops:

 ![image](https://community.stereolabs.com/uploads/default/original/2X/c/cc116b3121981ee1c6d7c39278998f7eedc96e91.png)

Occasionally my test app works fine and i can have 1 camera running at 30 FPS while the other at 15FPS with minimal to no frame drops but almost 9 times out of 10 i get this odd scenario where the camera set to 30FPS actually only runs at 15~ FPS its as though its being throttled / blocked internally..

Please find attached my little test sample app:

```c
#include <sl/Camera.hpp>
#include <iostream>
#include <thread>
#include <vector>
#include <atomic>
#include <chrono>

using namespace sl;

static const int FPS[] = {30,15}; //Change to 30,15
std::atomic<bool> running(true);

void runCamera(int id, uint32_t serial)
{
    bool getImage = true;
    bool getObjects = true;
    bool getPoints = true;
    bool getPosition = true;
    bool getSensors = true;

    std::cout << "RUNNING CAMERA " << id << " SN:" << serial << " FPS:" << FPS[id] << std::endl;

    Camera zed;

    InitParameters init;
#ifdef _WIN32
    init.camera_resolution = RESOLUTION::HD720;
    init.input.setFromCameraID(id);
#else
    init.camera_resolution = RESOLUTION::SVGA;
    init.input.setFromCameraID(id);
#endif

    init.depth_mode = DEPTH_MODE::NEURAL_LIGHT;
    init.coordinate_units = UNIT::METER;
    init.camera_fps = FPS[id % 2];
    init.depth_minimum_distance = 0;
    init.depth_maximum_distance = 20;
    init.depth_stabilization = 0;
    
    auto status = zed.open(init);
    std::cout << "Configured FPS: " << zed.getCameraInformation().camera_configuration.fps << std::endl;
    if (status != ERROR_CODE::SUCCESS)
    {
        std::cout << "Failed to open camera: " << status << std::endl;
        return;
    }

    PositionalTrackingParameters tracking;
    tracking.mode = POSITIONAL_TRACKING_MODE::GEN_3;
    tracking.enable_imu_fusion = true;
    tracking.enable_pose_smoothing = false;
    tracking.enable_area_memory = false;
    tracking.set_floor_as_origin = false;
    tracking.set_gravity_as_origin = true;

    zed.enablePositionalTracking(tracking);

    ObjectDetectionParameters obj_params;
    obj_params.detection_model = OBJECT_DETECTION_MODEL::MULTI_CLASS_BOX_FAST;
    obj_params.enable_tracking = true;
    obj_params.enable_segmentation = false;

    zed.enableObjectDetection(obj_params);

    RuntimeParameters runtime;
    runtime.confidence_threshold = 95;
    runtime.measure3D_reference_frame = REFERENCE_FRAME::CAMERA;

    Resolution res(960, 600);

    Mat leftImage;
    Mat pointCloud;

    Pose pose;
    Objects objects;
    SensorsData sensors;

    uint64_t frame = 0;

    auto blockStart = std::chrono::high_resolution_clock::now();
    double grabTimeSum = 0;

    while (running)
    {
        auto grabStart = std::chrono::high_resolution_clock::now();

        auto err = zed.grab(runtime);

        auto grabEnd = std::chrono::high_resolution_clock::now();
        double grabMs =
            std::chrono::duration<double, std::milli>(grabEnd - grabStart).count();

        grabTimeSum += grabMs;

        if (err != ERROR_CODE::SUCCESS)
        {
            std::cout << "Grab failed: " << err << std::endl;
            continue;
        }

        frame++;

        if (getPosition)
            zed.getPosition(pose, REFERENCE_FRAME::CAMERA);

        if (getObjects)
            zed.retrieveObjects(objects);

        if (getImage)
            zed.retrieveImage(leftImage, VIEW::LEFT, MEM::CPU, res);

        if (getPoints)
            zed.retrieveMeasure(pointCloud, MEASURE::XYZ, MEM::CPU, res);

        if (getSensors)
            zed.getSensorsData(sensors, TIME_REFERENCE::CURRENT);

        if (frame % 50 == 0)
        {
            auto now = std::chrono::high_resolution_clock::now();

            double elapsed =
                std::chrono::duration<double>(now - blockStart).count();

            double fps = 50.0 / elapsed;
            double avgGrab = grabTimeSum / 50.0;

            uint32_t dropped = zed.getFrameDroppedCount();

            std::cout
                << "[" << serial << "]-[" << frame << "] "
                << "Dropped: " << dropped
                << " Avg FPS: " << fps
                << " Avg Grab: " << avgGrab << " ms"
                << std::endl;

            blockStart = now;
            grabTimeSum = 0;
        }
    }

    zed.close();
}

int main()
{
    auto devices = Camera::getDeviceList();

    if (devices.empty())
    {
        std::cout << "No ZED cameras detected" << std::endl;
        return 0;
    }

    std::vector<std::thread> cameraThreads;

    for (int i = 0; i < devices.size(); i++)
    {
        auto sn = devices[i].serial_number;

        std::cout << "Found camera: " << sn << std::endl;

        cameraThreads.emplace_back(runCamera, i, sn);

        std::this_thread::sleep_for(std::chrono::milliseconds(500));
    }

    std::cout << "Press ENTER to stop..." << std::endl;
    std::cin.get();

    running = false;

    for (auto &t : cameraThreads)
        t.join();

    return 0;
}

```

Regards,

David

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [March 10, 2026, 11:54am UTC](https://community.stereolabs.com/t/multi-camera-incorrect-fps-and-dropped-frames/10984/2 "2026-03-10T11:54:53Z")

</div>

Hi @dhutchinson  
Are you connecting the two cameras to two different groups?

> **[Multi-camera configurations - Using GMSL with ZED Box Orin - Stereolabs](https://www.stereolabs.com/docs/embedded/zed-box-orin/gmsl#multi-camera-configurations)**
>
> If your ZED Box comes with an embedded capture card, you can use a ZED X or any other GMSL camera.

What version of the ZED SDK and ZED X Driver are you using?  
I recommend you get the latest.