# Motherboard selection

**URL:** <https://community.stereolabs.com/t/motherboard-selection/2112>\
**Category:** Hardware\
**Created:** [February 13, 2023, 9:57am UTC](https://community.stereolabs.com/t/motherboard-selection/2112 "2023-02-13T09:57:24Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![pixml](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/bbce88/32.png) [@pixml](https://community.stereolabs.com/u/pixml)\
**Post date:** [February 13, 2023, 9:57am UTC](https://community.stereolabs.com/t/motherboard-selection/2112/1 "2023-02-13T09:57:24Z")

</div>

Hi there! We are working on an AI system and using 4 ZED2i cameras. Usually everything works well, but sometimes we have troubles with one camera (camera turns off, python sdk doesn’t see it, ZED\_Explorer says “connect to another usb port”). If you replug all cameras to the same usb’s - everything works again for a while.  
We suspect that our weak motherboard is to blame (it didn’t even have usb 3.0 ports and we added them). This is our hardware:

 ![Снимок экрана 2023-02-13 в 13.42.31](https://community.stereolabs.com/uploads/default/original/2X/b/bcbd4d6ee8c215f15825ec4b1ba1e60cc11df72d.png)

Can you recommend hardware for our case (motherboard or motherboard + PCIe expansion cards) to rule out hardware problems?

---

<div class="post-metadata">

**Author:** ![adujardin](https://community.stereolabs.com/user_avatar/community.stereolabs.com/adujardin/32/4125_2.png) [@adujardin](https://community.stereolabs.com/u/adujardin)\
**Post date:** [February 13, 2023, 12:36pm UTC](https://community.stereolabs.com/t/motherboard-selection/2112/2 "2023-02-13T12:36:47Z")

</div>

Hi,

This is a USB bandwidth issue. The ZED2 requires the full bandwidth of 1 USB 3.0 controller when using the full framerate (let’s say HD720@60), so you’ll need 4 separate USB controllers for 4 cameras at full framerate or half that for half the framerate…

I would recommend adding a USB PCI Expansion card. Since this configuration is quite old I think half framerate is acceptable (like HD720@30) so you would need at least 2 PCIe expansion cards if there’s 1 controller per card. Although 4 ZED SDK instances will need quite a lot of computing power to run, depending on the parameters used.

You can check this article for more information [https://support.stereolabs.com/hc/en-us/articles/207635225-How-to-fix-USB-3-0-bandwidth-and-connection-issues](https://support.stereolabs.com/hc/en-us/articles/207635225-How-to-fix-USB-3-0-bandwidth-and-connection-issues)

---

<div class="post-metadata">

**Author:** ![pixml](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/bbce88/32.png) [@pixml](https://community.stereolabs.com/u/pixml)\
**Post date:** [February 15, 2023, 1:51pm UTC](https://community.stereolabs.com/t/motherboard-selection/2112/3 "2023-02-15T13:51:55Z")

</div>

Thanks for quick response!  
I would like to clarify what we are already using PCIe expansion card ([this one](https://lanberg.pl/en/produkt/PCE-US3-004#img1)).  
And since we most often need just pictures, we use either HD720@15 or HD1080@15  
So, should we use more than one PCIe expansion card?

---

<div class="post-metadata">

**Author:** ![adujardin](https://community.stereolabs.com/user_avatar/community.stereolabs.com/adujardin/32/4125_2.png) [@adujardin](https://community.stereolabs.com/u/adujardin)\
**Post date:** [February 16, 2023, 1:25pm UTC](https://community.stereolabs.com/t/motherboard-selection/2112/4 "2023-02-16T13:25:35Z")

</div>

This PCIe expansion card has 1 USB controller, so in theory, HD720@15 should work for 4 cameras. We recommend not starting them all at the same time though, adding a few seconds of delay may reduce detection issues.

However, HD1080@15 is twice the bandwidth of 720@15. So yes, I would recommend adding another PCIe expansion card similar to this one and it should work (with 2 cameras per expansion card). You should also make sure to power the PCIe card as this can also cause issues (through the SATA 15-pin connector on the PCB)