# Is ZED X One S compatible with Holoscan sensor bridge?

**URL:** <https://community.stereolabs.com/t/is-zed-x-one-s-compatible-with-holoscan-sensor-bridge/11847>\
**Category:** ZED X\
**Tags:** jetson\
**Created:** [November 16, 2026, 11:05am UTC](https://community.stereolabs.com/t/is-zed-x-one-s-compatible-with-holoscan-sensor-bridge/11847 "2026-11-16T11:05:33Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![snknitheesh](https://community.stereolabs.com/user_avatar/community.stereolabs.com/snknitheesh/32/4693_2.png) [@snknitheesh](https://community.stereolabs.com/u/snknitheesh)\
**Post date:** [November 16, 2026, 11:05am UTC](https://community.stereolabs.com/t/is-zed-x-one-s-compatible-with-holoscan-sensor-bridge/11847/1 "2026-11-16T11:05:33Z")

</div>

1. Is ZED X One S GMSL version compatible with Holoscan Sensor Bridge that goes into a Thor devkit ?
2. I see the ZED Link Mipi Quad, but is there a ZED Link GMSL Quad ?
3. If not is there any plans for a GMSL to Mipi Deserializer ?

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [November 16, 2026, 5:24pm UTC](https://community.stereolabs.com/t/is-zed-x-one-s-compatible-with-holoscan-sensor-bridge/11847/2 "2026-11-16T17:24:21Z")

</div>

Hi @snknitheesh,

> 1. Is the GMSL version of the ZED X One S compatible with the Holoscan Sensor Bridge connected to a Jetson AGX Thor Developer Kit?

No. With the Holoscan Sensor Bridge on the Jetson AGX Thor Developer Kit, the only supported [StereoLabs](https://www.stereolabs.com/) camera is the [ZED X One Core](https://www.stereolabs.com/store/products/zed-x-one-core). It is a 2.3 MP global shutter MIPI camera, and you can use up to 2 of them through the [ZED Link MIPI Quad](https://www.stereolabs.com/store/products/zed-link-mipi-quad). Setup guide: [ZED Link MIPI Quad on AGX Thor with Holoscan Sensor Bridge](https://docs.stereolabs.com/docs/products/embedded/zed-link-capture-card/mipi/zed-link-mipi-quad/jetson-agx-thor-devkit-setup).

> 1. I see a ZED Link MIPI Quad; is there a ZED Link GMSL Quad?

Yes, the [ZED Link Capture Card Quad](https://www.stereolabs.com/store/products/zed-link-capture-card-quad) exists, but it connects to the Samtec camera connector of the Jetson AGX Orin Developer Kit. The AGX Thor Developer Kit has no CSI/MIPI camera port, so the GMSL2 capture cards cannot be used with it. More details: [Can I use GMSL2 cameras with the NVIDIA Jetson AGX Thor Developer Kit?](https://support.stereolabs.com/articles/8527024569-can-i-use-the-zed-x-gmsl2-cameras-with-the-nvidia-jetson-agx-thor-development-kit)

> 1. If not, are there plans for a GMSL-to-MIPI deserializer?

We cannot share information about future products. To use the [ZED X One S](https://www.stereolabs.com/store/products/zed-x-one-s) with Jetson Thor today, we recommend the ZED Box 2 Max ([T4000](https://www.stereolabs.com/store/products/zed-box-2-max-t4000) or [T5000](https://www.stereolabs.com/store/products/zed-box-2-max-t5000)). It has 8 hardware-synchronized GMSL2 inputs and comes with the ZED SDK preinstalled. Third-party Thor carrier boards are also supported with our [GMSL2 compatibility drivers](https://www.stereolabs.com/developers/drivers).