# Is the ros2 wrapper and streaming mutually exclusive and/or working?

**URL:** <https://community.stereolabs.com/t/is-the-ros2-wrapper-and-streaming-mutually-exclusive-and-or-working/11314>\
**Category:** ROS2\
**Tags:** jetson, streaming, ros2\
**Created:** [May 14, 2026, 12:03am UTC](https://community.stereolabs.com/t/is-the-ros2-wrapper-and-streaming-mutually-exclusive-and-or-working/11314 "2026-05-14T00:03:28Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![TheFujirose](https://community.stereolabs.com/user_avatar/community.stereolabs.com/thefujirose/32/6216_2.png) [@TheFujirose](https://community.stereolabs.com/u/TheFujirose)\
**Post date:** [May 14, 2026, 12:03am UTC](https://community.stereolabs.com/t/is-the-ros2-wrapper-and-streaming-mutually-exclusive-and-or-working/11314/1 "2026-05-14T00:03:28Z")

</div>

I’m trying to figure out if I can both publish video data and at the same time stream data (via RTP) or if they are exclusive, or if it’s currently working; [it’s currently an open issue](https://github.com/stereolabs/zed-ros2-wrapper/issues/28).  
Every time I try it says I have to make a configuration file, but I don’t see anything on that in the [documentation](https://www.stereolabs.com/docs/ros2). My team is trying to build a RTP ingest server that acts as a media relay/distribution hub to distribute our robots feed to multiple shareholders devices while it’s performing. It needs to both use the video feed for object detection and send to that server.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [May 14, 2026, 4:20pm UTC](https://community.stereolabs.com/t/is-the-ros2-wrapper-and-streaming-mutually-exclusive-and-or-working/11314/2 "2026-05-14T16:20:33Z")

</div>

Hi @TheFujirose  
Welcome to the [StereoLabs](https://www.stereolabs.com/) community.

The latest version of the ZED ROS2 Wrapper allows you to start a local ZED SDK streaming server by using the `enable_streaming` or by setting the [stream\_server.stream\_enabled](https://github.com/stereolabs/zed-ros2-wrapper/blob/master/zed_wrapper/config/common_stereo.yaml#L185) to `true`.

On the dual side, you can start a ZED node using a local stream as input source:

```auto
ros2 launch zed_wrapper zed_camera.launch.py camera_model:=zed2i stream_address:=<server_address> stream_port:=<server_port>

```

You cannot use generic RTP streams, but a local stream generated by the ZED SDK:

> **[Local Video Streaming - Stereolabs](https://www.stereolabs.com/docs/video/streaming)**
>
> Using the ZED SDK, you can stream the side-by-side video of a ZED camera over a local IP network (Ethernet or Wifi).

---

<div class="post-metadata">

**Author:** ![TheFujirose](https://community.stereolabs.com/user_avatar/community.stereolabs.com/thefujirose/32/6216_2.png) [@TheFujirose](https://community.stereolabs.com/u/TheFujirose)\
**Post date:** [May 14, 2026, 5:09pm UTC](https://community.stereolabs.com/t/is-the-ros2-wrapper-and-streaming-mutually-exclusive-and-or-working/11314/3 "2026-05-14T17:09:07Z")

</div>

Thank you @Myzhar !

From what you said, I am understanding that the ROS2 Wrapper uses streams only as an input; I apologize that I didn’t realize that.

Thank you, and have a nice day!

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [May 15, 2026, 8:24am UTC](https://community.stereolabs.com/t/is-the-ros2-wrapper-and-streaming-mutually-exclusive-and-or-working/11314/4 "2026-05-15T08:24:45Z")

</div>

> [@TheFujirose](#):
>
> From what you said, I am understanding that the ROS2 Wrapper uses streams only as an input; I apologize that I didn’t realize that.

No, you can also create a Local Stream server:

> [@Myzhar](#):
>
> The latest version of the ZED ROS2 Wrapper allows you to start a local ZED SDK streaming server by using the `enable_streaming` or by setting the [stream\_server.stream\_enabled](https://github.com/stereolabs/zed-ros2-wrapper/blob/master/zed_wrapper/config/common_stereo.yaml#L185) to `true`.

But this is not a “standard RTP stream”, it’s a ZED SDK Local stream:

> **[Local Video Streaming - Stereolabs](https://www.stereolabs.com/docs/video/streaming)**
>
> Using the ZED SDK, you can stream the side-by-side video of a ZED camera over a local IP network (Ethernet or Wifi).